<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 imx8mp gadget mode strange behavior</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/imx8mp-gadget-mode-strange-behavior/m-p/2262809#M30846</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;Processor : imx8mp ( NXP_MIMX8ML8DVNLZAB )&lt;BR /&gt;Kernel version : 6.6.36&lt;BR /&gt;&lt;BR /&gt;We are working on product based on imx8mp processor. In which I observed strange behavior with typeC gadget mode.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I insert USB pendrive in my unit which detected as /dev/sda1, when I connect typec from unit to PC and it detect this pendrive in PC and I can see content of pendrive connected in my unit in the PC. It is working without inserting g_mass_storage.ko (this driver not builtin also)&lt;/LI&gt;&lt;LI&gt;But instead of using pendrive if I use SD card (/dev/mmcblk1p1). Doesn't matter what configuration I use but it's doesn't work.&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Any suggestion or pointers for this problem will be very helpful as we are at very crucial stage of development.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jemish&lt;/P&gt;</description>
    <pubDate>Mon, 15 Dec 2025 11:47:23 GMT</pubDate>
    <dc:creator>jemish_1990</dc:creator>
    <dc:date>2025-12-15T11:47:23Z</dc:date>
    <item>
      <title>imx8mp gadget mode strange behavior</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/imx8mp-gadget-mode-strange-behavior/m-p/2262809#M30846</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;Processor : imx8mp ( NXP_MIMX8ML8DVNLZAB )&lt;BR /&gt;Kernel version : 6.6.36&lt;BR /&gt;&lt;BR /&gt;We are working on product based on imx8mp processor. In which I observed strange behavior with typeC gadget mode.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I insert USB pendrive in my unit which detected as /dev/sda1, when I connect typec from unit to PC and it detect this pendrive in PC and I can see content of pendrive connected in my unit in the PC. It is working without inserting g_mass_storage.ko (this driver not builtin also)&lt;/LI&gt;&lt;LI&gt;But instead of using pendrive if I use SD card (/dev/mmcblk1p1). Doesn't matter what configuration I use but it's doesn't work.&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Any suggestion or pointers for this problem will be very helpful as we are at very crucial stage of development.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jemish&lt;/P&gt;</description>
      <pubDate>Mon, 15 Dec 2025 11:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/imx8mp-gadget-mode-strange-behavior/m-p/2262809#M30846</guid>
      <dc:creator>jemish_1990</dc:creator>
      <dc:date>2025-12-15T11:47:23Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp gadget mode strange behavior</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/imx8mp-gadget-mode-strange-behavior/m-p/2263157#M30849</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/142584"&gt;@jemish_1990&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I don't see such issue on i.MX8MP EVK + 6.6.y.&lt;/P&gt;
&lt;P&gt;The&amp;nbsp;mmcblk1p1&amp;nbsp; can be read on PC with sdcard reader before i insert it on board. Then i insert sdcard and use below command. Then same partition can be mounted in Windows.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;modprobe g_mass_storage file=/dev/mmcblk1p1 removable=1&lt;/LI-CODE&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Tue, 16 Dec 2025 01:39:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/imx8mp-gadget-mode-strange-behavior/m-p/2263157#M30849</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-12-16T01:39:17Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp gadget mode strange behavior</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/imx8mp-gadget-mode-strange-behavior/m-p/2263792#M30851</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788"&gt;@Zhiming_Liu&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for your quick response, I understand issue, it's limitation from our board design.&lt;/P&gt;&lt;P&gt;So we can close this discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jemish&lt;/P&gt;</description>
      <pubDate>Tue, 16 Dec 2025 11:09:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/imx8mp-gadget-mode-strange-behavior/m-p/2263792#M30851</guid>
      <dc:creator>jemish_1990</dc:creator>
      <dc:date>2025-12-16T11:09:59Z</dc:date>
    </item>
  </channel>
</rss>