<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic High-Impedance Buffer in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/High-Impedance-Buffer/m-p/2259495#M30825</link>
    <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I’m working on a small digital logic project and I’m considering using a &lt;A href="https://www.kasuo.com/product/74hct1g126gv-125-datasheet-price-pdf-nxp-usa-inc/" target="_self"&gt;74HCT1G126GV&lt;/A&gt; as a buffer/line driver. The part is a single-channel buffer with 3-state output and a supply range of 2–5.5 V, so it’s ideal for mixed-voltage logic interfaces. The datasheet is here.&lt;/P&gt;&lt;P&gt;My plan is to place the 74HCT1G126 between a microcontroller output and a shared bus or external module. Because the output can be disabled (tri-state), I can avoid bus conflicts when multiple devices share the same lines. It’s also useful for isolating noisy parts of a circuit or for level shifting/helping drive loads that the MCU can’t handle directly.&lt;/P&gt;&lt;P&gt;Before I build, I have a few questions and I’d love your input:&lt;/P&gt;&lt;P&gt;Is it okay to rely on the 74HCT1G126’s 3-state behavior for shared-bus applications, or are there timing or leakage pitfalls I should watch out for? For mixed-voltage interfacing (e.g. 5 V logic driving 3.3 V), how reliable is the HCT buffer in real-life use? Any known gotchas regarding signal integrity or margins? When placing this buffer on a PCB, what layout practices would you recommend (trace routing, decoupling, pull-ups/pull-downs for high-Z)?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
    <pubDate>Wed, 10 Dec 2025 22:06:22 GMT</pubDate>
    <dc:creator>Jordan1x</dc:creator>
    <dc:date>2025-12-10T22:06:22Z</dc:date>
    <item>
      <title>High-Impedance Buffer</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/High-Impedance-Buffer/m-p/2259495#M30825</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I’m working on a small digital logic project and I’m considering using a &lt;A href="https://www.kasuo.com/product/74hct1g126gv-125-datasheet-price-pdf-nxp-usa-inc/" target="_self"&gt;74HCT1G126GV&lt;/A&gt; as a buffer/line driver. The part is a single-channel buffer with 3-state output and a supply range of 2–5.5 V, so it’s ideal for mixed-voltage logic interfaces. The datasheet is here.&lt;/P&gt;&lt;P&gt;My plan is to place the 74HCT1G126 between a microcontroller output and a shared bus or external module. Because the output can be disabled (tri-state), I can avoid bus conflicts when multiple devices share the same lines. It’s also useful for isolating noisy parts of a circuit or for level shifting/helping drive loads that the MCU can’t handle directly.&lt;/P&gt;&lt;P&gt;Before I build, I have a few questions and I’d love your input:&lt;/P&gt;&lt;P&gt;Is it okay to rely on the 74HCT1G126’s 3-state behavior for shared-bus applications, or are there timing or leakage pitfalls I should watch out for? For mixed-voltage interfacing (e.g. 5 V logic driving 3.3 V), how reliable is the HCT buffer in real-life use? Any known gotchas regarding signal integrity or margins? When placing this buffer on a PCB, what layout practices would you recommend (trace routing, decoupling, pull-ups/pull-downs for high-Z)?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Wed, 10 Dec 2025 22:06:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/High-Impedance-Buffer/m-p/2259495#M30825</guid>
      <dc:creator>Jordan1x</dc:creator>
      <dc:date>2025-12-10T22:06:22Z</dc:date>
    </item>
  </channel>
</rss>