<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCAL6416AHF (HWQFN24 package thermal pad connection) in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCAL6416AHF-HWQFN24-package-thermal-pad-connection/m-p/2256494#M30795</link>
    <description>&lt;P&gt;Hi Glenn,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The exposed pad underneath the PCAL6416AHF (HWQFN24) is not internally connected to any pin.&amp;nbsp;It can be left floating, but for better thermal performance it is recommended to connect it to the GND.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BRs, Tomas&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sun, 07 Dec 2025 17:24:16 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2025-12-07T17:24:16Z</dc:date>
    <item>
      <title>PCAL6416AHF (HWQFN24 package thermal pad connection)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCAL6416AHF-HWQFN24-package-thermal-pad-connection/m-p/2256322#M30791</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;QFN24 package "exposed thermal pad" ... there is no information on whether this can / should / shouldn't be connected to GND.&lt;/P&gt;&lt;P&gt;I'm assuming it would be ok, but want to check.&lt;/P&gt;&lt;P&gt;Any issue with connecting the center pad to GND for PCAL6416AHF?&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;-- Glenn&lt;/P&gt;</description>
      <pubDate>Fri, 05 Dec 2025 21:14:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCAL6416AHF-HWQFN24-package-thermal-pad-connection/m-p/2256322#M30791</guid>
      <dc:creator>gwagner613</dc:creator>
      <dc:date>2025-12-05T21:14:58Z</dc:date>
    </item>
    <item>
      <title>Re: PCAL6416AHF (HWQFN24 package thermal pad connection)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCAL6416AHF-HWQFN24-package-thermal-pad-connection/m-p/2256494#M30795</link>
      <description>&lt;P&gt;Hi Glenn,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The exposed pad underneath the PCAL6416AHF (HWQFN24) is not internally connected to any pin.&amp;nbsp;It can be left floating, but for better thermal performance it is recommended to connect it to the GND.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BRs, Tomas&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 07 Dec 2025 17:24:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCAL6416AHF-HWQFN24-package-thermal-pad-connection/m-p/2256494#M30795</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-12-07T17:24:16Z</dc:date>
    </item>
  </channel>
</rss>