<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックS32N55 XSPI timeout during ReadID</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/S32N55-XSPI-timeout-during-ReadID/m-p/2249398#M30706</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to setup a minimal project for the FSS core on the S32N55 to flash the attached s28hs01gt OSPI memory on the S32N55-RDB. Goal is to implement a RAM bootloader to flash the OSPI memory on unprogrammed devices. When trying to read the ID Code with the `Xspi_Ip_ReadId` function, a timeout is reached and the program stalls. This problem also occurs during the `&lt;SPAN&gt;Mem_43_EXFLS_Init&lt;/SPAN&gt;`.&lt;/P&gt;&lt;P&gt;Debugging the examples from the RTD is not helpful, since these require an IVT image in the flash.&lt;/P&gt;&lt;P&gt;The setup is based on the examples from the RTD packages, where the LUTs and memory configuration is shown. I added the initialization of the pins for the OSPI. From the examples it is not clear how the clocks need to be set up.&lt;/P&gt;&lt;P&gt;Does anyone has expirience with this topic and could help to setup this project.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Luis&lt;/P&gt;</description>
    <pubDate>Wed, 26 Nov 2025 13:01:00 GMT</pubDate>
    <dc:creator>waldluis</dc:creator>
    <dc:date>2025-11-26T13:01:00Z</dc:date>
    <item>
      <title>S32N55 XSPI timeout during ReadID</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/S32N55-XSPI-timeout-during-ReadID/m-p/2249398#M30706</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to setup a minimal project for the FSS core on the S32N55 to flash the attached s28hs01gt OSPI memory on the S32N55-RDB. Goal is to implement a RAM bootloader to flash the OSPI memory on unprogrammed devices. When trying to read the ID Code with the `Xspi_Ip_ReadId` function, a timeout is reached and the program stalls. This problem also occurs during the `&lt;SPAN&gt;Mem_43_EXFLS_Init&lt;/SPAN&gt;`.&lt;/P&gt;&lt;P&gt;Debugging the examples from the RTD is not helpful, since these require an IVT image in the flash.&lt;/P&gt;&lt;P&gt;The setup is based on the examples from the RTD packages, where the LUTs and memory configuration is shown. I added the initialization of the pins for the OSPI. From the examples it is not clear how the clocks need to be set up.&lt;/P&gt;&lt;P&gt;Does anyone has expirience with this topic and could help to setup this project.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Luis&lt;/P&gt;</description>
      <pubDate>Wed, 26 Nov 2025 13:01:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/S32N55-XSPI-timeout-during-ReadID/m-p/2249398#M30706</guid>
      <dc:creator>waldluis</dc:creator>
      <dc:date>2025-11-26T13:01:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32N55 XSPI timeout during ReadID</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/S32N55-XSPI-timeout-during-ReadID/m-p/2250014#M30709</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250449"&gt;@waldluis&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;I understand that you are working with S32N55, since it is still in the per-production phase, it is not supported via this public community, I suggest contacting your NXP DFAE/FAE, for them to provide technical support on the issue in hand.&lt;/P&gt;
&lt;P&gt;Sorry for your inconvenience.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Nov 2025 04:05:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/S32N55-XSPI-timeout-during-ReadID/m-p/2250014#M30709</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-11-27T04:05:08Z</dc:date>
    </item>
  </channel>
</rss>