<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CLEV6630B in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/CLEV6630B/m-p/2191653#M30447</link>
    <description>&lt;P&gt;I would like the impedance-matching schematic for the CLEV6630B antenna (30×50 mm). My product only came with the schematic for the 65×65 mm antenna.&lt;/P&gt;&lt;P&gt;Thank you for the response and for the schematic. However, I noticed the resistors on the board that came with my kit differ from the schematic. I removed one resistor to confirm: the schematic shows 1.6 kΩ, while my board has two 2.2 kΩ in parallel. Which one is incorrect—my schematic or the board that shipped with the kit?&lt;/P&gt;&lt;P&gt;Attached is a photo of the antenna.&lt;/P&gt;&lt;P&gt;Thank you in advance for the quick turnaround on my inquiry.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 23 Oct 2025 15:21:57 GMT</pubDate>
    <dc:creator>mrmorais</dc:creator>
    <dc:date>2025-10-23T15:21:57Z</dc:date>
    <item>
      <title>CLEV6630B</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CLEV6630B/m-p/2191653#M30447</link>
      <description>&lt;P&gt;I would like the impedance-matching schematic for the CLEV6630B antenna (30×50 mm). My product only came with the schematic for the 65×65 mm antenna.&lt;/P&gt;&lt;P&gt;Thank you for the response and for the schematic. However, I noticed the resistors on the board that came with my kit differ from the schematic. I removed one resistor to confirm: the schematic shows 1.6 kΩ, while my board has two 2.2 kΩ in parallel. Which one is incorrect—my schematic or the board that shipped with the kit?&lt;/P&gt;&lt;P&gt;Attached is a photo of the antenna.&lt;/P&gt;&lt;P&gt;Thank you in advance for the quick turnaround on my inquiry.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Oct 2025 15:21:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CLEV6630B/m-p/2191653#M30447</guid>
      <dc:creator>mrmorais</dc:creator>
      <dc:date>2025-10-23T15:21:57Z</dc:date>
    </item>
    <item>
      <title>Re: CLEV6630B</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CLEV6630B/m-p/2195959#M30504</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256100"&gt;@mrmorais&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;The antennas included in that kit are already matched to work with the CLEV6630B board. If you are planning to use a custom antenna, it is necessary to perform proper matching and tuning according to &lt;A href="https://www.nxp.com/docs/en/application-note/AN11019.pdf" target="_blank"&gt;AN11019 CLRC663 Antenna Design&lt;/A&gt;; or if you want to implement the antenna on a different reader, please refer to the corresponding antenna design and matching guide.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 15:51:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CLEV6630B/m-p/2195959#M30504</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2025-10-30T15:51:19Z</dc:date>
    </item>
  </channel>
</rss>