<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: Ghostscript recipe Yocto Build Error</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Ghostscript-recipe-Yocto-Build-Error/m-p/2190307#M30427</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I would like to confirm if you have set all packages needed?&lt;BR /&gt;By this I do not mean that the host have the packages, but if yocto has fetch and configured all pakcages, since you are running using -k option.&lt;BR /&gt;&lt;BR /&gt;I will try on my side to double check but I would recommend to try to bitbake again without the -k option and see if the same error is shown.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Wed, 22 Oct 2025 00:21:07 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2025-10-22T00:21:07Z</dc:date>
    <item>
      <title>Ghostscript recipe Yocto Build Error</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Ghostscript-recipe-Yocto-Build-Error/m-p/2189251#M30421</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am doing Yocto Build for FRDM-IMX8MPLUS development board and I did bitbake with following commands.&lt;BR /&gt;&lt;BR /&gt;bitbake -k imx-image-full&lt;/P&gt;&lt;P&gt;Result: bitbake failed and recipe name: ghostscript&lt;/P&gt;&lt;P&gt;bitbake -k ghostscript&lt;/P&gt;&lt;P&gt;then I received following error.&lt;/P&gt;&lt;P&gt;I think something wrong with gcc library. Please advise me.&lt;/P&gt;&lt;P&gt;| /usr/src/debug/gcc/13.3.0/gcc/range.cc:42:(.text+0x9c): undefined reference to `build_zero_cst(tree_node*)'&lt;BR /&gt;| /home/compulab/imx-yocto-bsp/frdm-imx8mp/tmp/work/armv8a-poky-linux/gcc/13.3.0/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.3.0/ld: /usr/src/debug/gcc/13.3.0/gcc/range.cc:42:(.text+0xa8): undefined reference to `build_zero_cst(tree_node*)'&lt;BR /&gt;| /home/compulab/imx-yocto-bsp/frdm-imx8mp/tmp/work/armv8a-poky-linux/gcc/13.3.0/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.3.0/ld: range.o: in function `int_range&amp;lt;1u, false&amp;gt;::int_range(tree_node*, tree_node*, value_range_kind)':&lt;BR /&gt;| /usr/src/debug/gcc/13.3.0/gcc/value-range.h:941:(.text+0xe4): undefined reference to `irange::set(tree_node*, tree_node*, value_range_kind)'&lt;BR /&gt;| /home/compulab/imx-yocto-bsp/frdm-imx8mp/tmp/work/armv8a-poky-linux/gcc/13.3.0/recipe-sysroot-native/usr/bin/aarch64-poky-linux/../../libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/13.3.0/ld: range.o: in function `int_range&amp;lt;1u, false&amp;gt;::operator=(int_range&amp;lt;1u, false&amp;gt; const&amp;amp;)':&lt;BR /&gt;| /usr/src/debug/gcc/13.3.0/gcc/value-range.h:972:(.text+0x264): undefined reference to `irange::operator=(irange const&amp;amp;)'&lt;BR /&gt;| collect2: error: ld returned 1 exit status&lt;BR /&gt;| make[1]: *** [../../../../../../../work-shared/gcc-13.3.0-r0/gcc-13.3.0/gcc/lto/Make-lang.in:102: lto-dump] Error 1&lt;BR /&gt;| make[1]: Leaving directory '/home/compulab/imx-yocto-bsp/frdm-imx8mp/tmp/work/armv8a-poky-linux/gcc/13.3.0/gcc-13.3.0/build.aarch64-poky-linux.aarch64-poky-linux/gcc'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;| make: *** [Makefile:4627: all-gcc] Error 2&lt;BR /&gt;| ERROR: oe_runmake failed&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;ERROR: Task (/home/compulab/imx-yocto-bsp/sources/poky/meta/recipes-devtools/gcc/gcc_13.3.bb:do_compile) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 4587 tasks of which 3788 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt;/home/compulab/imx-yocto-bsp/sources/poky/meta/recipes-devtools/gcc/gcc_13.3.bb:do_compile&lt;BR /&gt;Summary: There were 2 ERROR messages, returning a non-zero exit code.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Oct 2025 14:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Ghostscript-recipe-Yocto-Build-Error/m-p/2189251#M30421</guid>
      <dc:creator>mikie_mikie</dc:creator>
      <dc:date>2025-10-20T14:40:27Z</dc:date>
    </item>
    <item>
      <title>Re: Ghostscript recipe Yocto Build Error</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Ghostscript-recipe-Yocto-Build-Error/m-p/2190307#M30427</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I would like to confirm if you have set all packages needed?&lt;BR /&gt;By this I do not mean that the host have the packages, but if yocto has fetch and configured all pakcages, since you are running using -k option.&lt;BR /&gt;&lt;BR /&gt;I will try on my side to double check but I would recommend to try to bitbake again without the -k option and see if the same error is shown.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Oct 2025 00:21:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Ghostscript-recipe-Yocto-Build-Error/m-p/2190307#M30427</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-10-22T00:21:07Z</dc:date>
    </item>
    <item>
      <title>Re: Ghostscript recipe Yocto Build Error</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Ghostscript-recipe-Yocto-Build-Error/m-p/2190322#M30428</link>
      <description>&lt;P&gt;Hello NXP Tech Support,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;After I deleted &lt;STRONG&gt;tmp&lt;/STRONG&gt; folder then I was able to do bitbake -k successfully.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;mikie&lt;/P&gt;</description>
      <pubDate>Wed, 22 Oct 2025 01:17:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Ghostscript-recipe-Yocto-Build-Error/m-p/2190322#M30428</guid>
      <dc:creator>mikie_mikie</dc:creator>
      <dc:date>2025-10-22T01:17:49Z</dc:date>
    </item>
  </channel>
</rss>