<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: PTN3222CUK-EVB使用咨询</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PTN3222CUK-EVB%E4%BD%BF%E7%94%A8%E5%92%A8%E8%AF%A2/m-p/2186564#M30380</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It does not “auto‑sense” the role. The role is chosen by the application, either by I²C register configuration or by the eUSB2 Port Configuration command. The EVB makes this easy via its I²C header. By default after reset, the device comes up in Peripheral role and can transition under control of the state machine.&lt;/P&gt;
&lt;P&gt;Yes. That is a recommended step (even though the EVB’s factory default is peripheral). Also configure SI settings as needed.&lt;/P&gt;
&lt;P&gt;Yes, conceptually correct. In practice, there is the usual USB2 attach → reset → (optional) HS chirp negotiation → enumeration → SOF sequence and PTN3222 simply level‑shifts/conditions signals both ways throughout.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
    <pubDate>Wed, 15 Oct 2025 10:24:19 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2025-10-15T10:24:19Z</dc:date>
    <item>
      <title>PTN3222CUK-EVB使用咨询</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PTN3222CUK-EVB%E4%BD%BF%E7%94%A8%E5%92%A8%E8%AF%A2/m-p/2186463#M30379</link>
      <description>&lt;P&gt;您好：&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 我想了解一下PTN3222CUK-EVB的功能。我现在有一个eUSB设备，希望通过PTN3222CUK-EVB将eUSB信号转为USB2.0与PC通信。但我不了解PTN3222CUK-EVB是应该如何使用。比如PTN3222CUK-EVB是怎么知道自己是host repeater还是peripheral repeater的？&lt;BR /&gt;我的应用框图如下：&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhirongRao_0-1760515819679.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/360860iCC7D1130D4C8FC13/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhirongRao_0-1760515819679.png" alt="ZhirongRao_0-1760515819679.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;若想要PTN3222正常工作，流程是否如下所示：&lt;/P&gt;&lt;P&gt;1、在进行eUSB通信之前，需要MCU(eUSB设备端)通过I2C给PTN3222下命令，让PTN3222进入peripheral repeater；&lt;/P&gt;&lt;P&gt;2、PTN3222的USB2.0接口插入电脑；PC USB2.0 发起sof包，PTN3222将SOF包转为eUSB信号发送给MCU(eUSB设备)，同时MCU(eUSB设备)识别到此信号，并回PTN3222对应的波形；&lt;/P&gt;&lt;P&gt;期待您的回复，祝您生活愉快！&lt;/P&gt;</description>
      <pubDate>Wed, 15 Oct 2025 08:35:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PTN3222CUK-EVB%E4%BD%BF%E7%94%A8%E5%92%A8%E8%AF%A2/m-p/2186463#M30379</guid>
      <dc:creator>ZhirongRao</dc:creator>
      <dc:date>2025-10-15T08:35:52Z</dc:date>
    </item>
    <item>
      <title>Re: PTN3222CUK-EVB使用咨询</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PTN3222CUK-EVB%E4%BD%BF%E7%94%A8%E5%92%A8%E8%AF%A2/m-p/2186564#M30380</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It does not “auto‑sense” the role. The role is chosen by the application, either by I²C register configuration or by the eUSB2 Port Configuration command. The EVB makes this easy via its I²C header. By default after reset, the device comes up in Peripheral role and can transition under control of the state machine.&lt;/P&gt;
&lt;P&gt;Yes. That is a recommended step (even though the EVB’s factory default is peripheral). Also configure SI settings as needed.&lt;/P&gt;
&lt;P&gt;Yes, conceptually correct. In practice, there is the usual USB2 attach → reset → (optional) HS chirp negotiation → enumeration → SOF sequence and PTN3222 simply level‑shifts/conditions signals both ways throughout.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Wed, 15 Oct 2025 10:24:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PTN3222CUK-EVB%E4%BD%BF%E7%94%A8%E5%92%A8%E8%AF%A2/m-p/2186564#M30380</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-10-15T10:24:19Z</dc:date>
    </item>
  </channel>
</rss>