<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックiMX93 FRDM UART</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/iMX93-FRDM-UART/m-p/2182729#M30303</link>
    <description>&lt;P&gt;I am using the iMX93 FRDM board with the base image. I want to use the UART3 pins of the board i.e. P11 pin 8 (&lt;SPAN&gt;UART3_TX&lt;/SPAN&gt;), P11 pin 10 (&lt;SPAN&gt;UART3_RX&lt;/SPAN&gt;). But in base image it is not enabled. So how can i enable it ?&lt;/P&gt;</description>
    <pubDate>Thu, 09 Oct 2025 06:02:32 GMT</pubDate>
    <dc:creator>mrunal3008</dc:creator>
    <dc:date>2025-10-09T06:02:32Z</dc:date>
    <item>
      <title>iMX93 FRDM UART</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX93-FRDM-UART/m-p/2182729#M30303</link>
      <description>&lt;P&gt;I am using the iMX93 FRDM board with the base image. I want to use the UART3 pins of the board i.e. P11 pin 8 (&lt;SPAN&gt;UART3_TX&lt;/SPAN&gt;), P11 pin 10 (&lt;SPAN&gt;UART3_RX&lt;/SPAN&gt;). But in base image it is not enabled. So how can i enable it ?&lt;/P&gt;</description>
      <pubDate>Thu, 09 Oct 2025 06:02:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX93-FRDM-UART/m-p/2182729#M30303</guid>
      <dc:creator>mrunal3008</dc:creator>
      <dc:date>2025-10-09T06:02:32Z</dc:date>
    </item>
    <item>
      <title>Re: iMX93 FRDM UART</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX93-FRDM-UART/m-p/2184503#M30344</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;1. Please refer instructions here to build yocto sdk,&lt;/P&gt;
&lt;P&gt;&lt;A href="https://docs.nxp.com/bundle/UG10195/page/topics/image_build_01.html" target="_blank"&gt;https://docs.nxp.com/bundle/UG10195/page/topics/image_build_01.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2. Then referring&amp;nbsp;How to build U-Boot and kernel in a standalone environment here, need to modify imx93-frdm dts file to support uart3.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://docs.nxp.com/bundle/UG10195/page/topics/customization.html" target="_blank"&gt;https://docs.nxp.com/bundle/UG10195/page/topics/customization.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Mon, 13 Oct 2025 05:23:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX93-FRDM-UART/m-p/2184503#M30344</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-10-13T05:23:37Z</dc:date>
    </item>
  </channel>
</rss>