<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MFRC522 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MFRC522/m-p/2182713#M30299</link>
    <description>&lt;P&gt;&lt;STRONG&gt;Hello everyone,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am using the MFRC522 reader to read RFID cards and perform a block decrement operation. Recently, I purchased some readers from online shops that turned out to be cloned versions. When I perform the decrement operation, it fails — the command returns a timeout error.&lt;/P&gt;&lt;P&gt;After that, when I read the same block (configured as a value block through the access bits), I find that the entire block data is corrupted — all 16 bytes are 0xFF.&lt;/P&gt;&lt;P&gt;Could a cloned RFID reader be the reason for this corruption of the value block?&lt;/P&gt;</description>
    <pubDate>Thu, 09 Oct 2025 05:43:43 GMT</pubDate>
    <dc:creator>RajPadmani</dc:creator>
    <dc:date>2025-10-09T05:43:43Z</dc:date>
    <item>
      <title>MFRC522</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MFRC522/m-p/2182713#M30299</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Hello everyone,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am using the MFRC522 reader to read RFID cards and perform a block decrement operation. Recently, I purchased some readers from online shops that turned out to be cloned versions. When I perform the decrement operation, it fails — the command returns a timeout error.&lt;/P&gt;&lt;P&gt;After that, when I read the same block (configured as a value block through the access bits), I find that the entire block data is corrupted — all 16 bytes are 0xFF.&lt;/P&gt;&lt;P&gt;Could a cloned RFID reader be the reason for this corruption of the value block?&lt;/P&gt;</description>
      <pubDate>Thu, 09 Oct 2025 05:43:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MFRC522/m-p/2182713#M30299</guid>
      <dc:creator>RajPadmani</dc:creator>
      <dc:date>2025-10-09T05:43:43Z</dc:date>
    </item>
    <item>
      <title>Re: MFRC522</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MFRC522/m-p/2185505#M30370</link>
      <description>&lt;P&gt;If the cloned reader has incorrect timing, incomplete command support, or poor signal integrity, it may fail during the&amp;nbsp;decrement operation.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Oct 2025 08:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MFRC522/m-p/2185505#M30370</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2025-10-14T08:28:17Z</dc:date>
    </item>
  </channel>
</rss>