<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SC16IS752 IRQ Pull-Up Resistor value in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752-IRQ-Pull-Up-Resistor-value/m-p/2180503#M30259</link>
    <description>&lt;P&gt;In the data sheet for&amp;nbsp;SC16IS752 (and even SC16IS750) the IRQ Pull-Up Resistor value is recommended 1 kOhm for 3.3 V supply. What is the cause ? What will occur with a pullup as high as 33 kOhm ? There is no value given for the leakage current (for GPIO it's 1 µA, for SPI it's 10 µA).&lt;/P&gt;&lt;P&gt;We design a low power circuit with a quite long interrupt response time and would not spend 3.3 mA over several seconds when the rest of the circuit runs on 2 mA.&lt;/P&gt;</description>
    <pubDate>Mon, 06 Oct 2025 10:48:42 GMT</pubDate>
    <dc:creator>timbeyer</dc:creator>
    <dc:date>2025-10-06T10:48:42Z</dc:date>
    <item>
      <title>SC16IS752 IRQ Pull-Up Resistor value</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752-IRQ-Pull-Up-Resistor-value/m-p/2180503#M30259</link>
      <description>&lt;P&gt;In the data sheet for&amp;nbsp;SC16IS752 (and even SC16IS750) the IRQ Pull-Up Resistor value is recommended 1 kOhm for 3.3 V supply. What is the cause ? What will occur with a pullup as high as 33 kOhm ? There is no value given for the leakage current (for GPIO it's 1 µA, for SPI it's 10 µA).&lt;/P&gt;&lt;P&gt;We design a low power circuit with a quite long interrupt response time and would not spend 3.3 mA over several seconds when the rest of the circuit runs on 2 mA.&lt;/P&gt;</description>
      <pubDate>Mon, 06 Oct 2025 10:48:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752-IRQ-Pull-Up-Resistor-value/m-p/2180503#M30259</guid>
      <dc:creator>timbeyer</dc:creator>
      <dc:date>2025-10-06T10:48:42Z</dc:date>
    </item>
    <item>
      <title>Re: SC16IS752 IRQ Pull-Up Resistor value</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752-IRQ-Pull-Up-Resistor-value/m-p/2180531#M30261</link>
      <description>&lt;P&gt;Dear Tim,&lt;/P&gt;
&lt;H3&gt;Why 1 kΩ is recommended?&lt;/H3&gt;
&lt;OL&gt;
&lt;LI&gt;
&lt;P&gt;Fast rise time for IRQ signal&lt;BR /&gt;The IRQ pin is an open-drain output, so the pull-up resistor determines how quickly the line goes high after the device releases it.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;With 1 kΩ at 3.3 V, the current is about 3.3 mA when the pin is low, which ensures a strong pull-up and a fast transition when released.&lt;/LI&gt;
&lt;LI&gt;This is important because IRQ signals often need to meet timing specs for SPI/I²C or interrupt controllers.&lt;/LI&gt;
&lt;/UL&gt;
&lt;/LI&gt;
&lt;LI&gt;
&lt;P&gt;Noise immunity&lt;BR /&gt;A strong pull-up reduces susceptibility to noise and ensures the voltage reaches a valid logic high quickly, even with some parasitic capacitance on the line.&lt;/P&gt;
&lt;/LI&gt;
&lt;/OL&gt;
&lt;H3&gt;&lt;STRONG&gt;What happens with 33 kΩ?&lt;/STRONG&gt;&lt;/H3&gt;
&lt;UL&gt;
&lt;LI&gt;
&lt;P&gt;&lt;STRONG&gt;Rise time increases significantly&lt;/STRONG&gt; because the RC time constant grows: &lt;SPAN class="math math-inline"&gt;&lt;SPAN class="katex"&gt;&lt;SPAN class="katex-mathml"&gt;τ=R×C\tau = R \times C&lt;/SPAN&gt;&lt;SPAN class="katex-html"&gt;&lt;SPAN class="base"&gt;&lt;SPAN class="mord mathnormal"&gt;τ&lt;/SPAN&gt;&lt;SPAN class="mrel"&gt;=&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="base"&gt;&lt;SPAN class="mord mathnormal"&gt;R&lt;/SPAN&gt;&lt;SPAN class="mbin"&gt;×&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="base"&gt;&lt;SPAN class="mord mathnormal"&gt;C&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt; If the line has, say, 50 pF of capacitance:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;With 1 kΩ: &lt;SPAN class="math math-inline"&gt;&lt;SPAN class="katex"&gt;&lt;SPAN class="katex-mathml"&gt;τ=1,000×50pF=50ns\tau = 1{,}000 \times 50 \text{pF} = 50 \text{ns}&lt;/SPAN&gt;&lt;SPAN class="katex-html"&gt;&lt;SPAN class="base"&gt;&lt;SPAN class="mord mathnormal"&gt;τ&lt;/SPAN&gt;&lt;SPAN class="mrel"&gt;=&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="base"&gt;&lt;SPAN class="mord"&gt;1&lt;/SPAN&gt;&lt;SPAN class="mord"&gt;&lt;SPAN class="mpunct"&gt;,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="mord"&gt;000&lt;/SPAN&gt;&lt;SPAN class="mbin"&gt;×&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="base"&gt;&lt;SPAN class="mord"&gt;50&lt;/SPAN&gt;&lt;SPAN class="mord text"&gt;&lt;SPAN class="mord"&gt;pF&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="mrel"&gt;=&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="base"&gt;&lt;SPAN class="mord"&gt;50&lt;/SPAN&gt;&lt;SPAN class="mord text"&gt;&lt;SPAN class="mord"&gt;ns&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;With 33 kΩ: &lt;SPAN class="math math-inline"&gt;&lt;SPAN class="katex"&gt;&lt;SPAN class="katex-mathml"&gt;τ=33,000×50pF=1.65µs\tau = 33{,}000 \times 50 \text{pF} = 1.65 \text{µs}&lt;/SPAN&gt;&lt;SPAN class="katex-html"&gt;&lt;SPAN class="base"&gt;&lt;SPAN class="mord mathnormal"&gt;τ&lt;/SPAN&gt;&lt;SPAN class="mrel"&gt;=&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="base"&gt;&lt;SPAN class="mord"&gt;33&lt;/SPAN&gt;&lt;SPAN class="mord"&gt;&lt;SPAN class="mpunct"&gt;,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="mord"&gt;000&lt;/SPAN&gt;&lt;SPAN class="mbin"&gt;×&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="base"&gt;&lt;SPAN class="mord"&gt;50&lt;/SPAN&gt;&lt;SPAN class="mord text"&gt;&lt;SPAN class="mord"&gt;pF&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="mrel"&gt;=&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="base"&gt;&lt;SPAN class="mord"&gt;1.65&lt;/SPAN&gt;&lt;SPAN class="mord text"&gt;&lt;SPAN class="mord"&gt;µs&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt; That’s still fast for many systems, but if your interrupt latency is long and the MCU samples asynchronously, it might not matter much.&lt;/LI&gt;
&lt;/UL&gt;
&lt;/LI&gt;
&lt;LI&gt;
&lt;P&gt;&lt;STRONG&gt;Logic level stability&lt;/STRONG&gt;: With higher resistance, leakage currents (up to 10 µA for SPI pins) could cause noticeable voltage drop. The IRQ might only reach ~3.0 V instead of 3.3 V, which is usually okay but could be marginal in noisy environments.&lt;/P&gt;
&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;If your interrupt response time is in milliseconds and you can tolerate slower rise times, 33 kΩ is likely fine.&lt;/LI&gt;
&lt;LI&gt;Just ensure:
&lt;UL&gt;
&lt;LI&gt;Total bus capacitance isn’t huge.&lt;/LI&gt;
&lt;LI&gt;Leakage currents don’t pull the line below VIH (usually &amp;gt;2 V for 3.3 V logic).&lt;/LI&gt;
&lt;/UL&gt;
&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Oct 2025 11:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752-IRQ-Pull-Up-Resistor-value/m-p/2180531#M30261</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2025-10-06T11:47:54Z</dc:date>
    </item>
  </channel>
</rss>