<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx93 FRDM mac address randomisation in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/imx93-FRDM-mac-address-randomisation/m-p/2179816#M30250</link>
    <description>&lt;P&gt;I have a follow-up question regarding the MAC address for the i.MX93 FRDM board.&lt;/P&gt;&lt;P&gt;From the i.MX93 FRDM datasheet (screenshot attached below), it is mentioned that:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sakshi123_2-1759483198532.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/359436iE88B77F1D95B0C47/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sakshi123_2-1759483198532.png" alt="sakshi123_2-1759483198532.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Question is :&amp;nbsp;Is there any physical setup on the i.MX93 board to configure or set a static MAC address for every bootup, or is the MAC address always fused and fixed inside the i.MX93 processor?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 03 Oct 2025 09:22:27 GMT</pubDate>
    <dc:creator>sakshi123</dc:creator>
    <dc:date>2025-10-03T09:22:27Z</dc:date>
    <item>
      <title>imx93 FRDM mac address randomisation</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/imx93-FRDM-mac-address-randomisation/m-p/2178674#M30239</link>
      <description>&lt;P&gt;I am working with an i.MX93 FRDM board running the base image provided by NXP (link: "&lt;A href="https://github.com/nxp-imx/meta-imx" target="_blank"&gt;https://github.com/nxp-imx/meta-imx&lt;/A&gt;"). The issue I’m facing is that the MAC address changes every time the board is powered on. Is there an image available in which the MAC address remains fixed across reboots and does not change?&lt;/P&gt;&lt;P&gt;Currently, because the MAC address keeps changing on each reboot, the pool of allowed MAC addresses gets exhausted, preventing other devices from connecting to the network.&lt;/P&gt;&lt;P&gt;We are specifically looking for a solution at the image level, not through any additional service or workaround&lt;/P&gt;</description>
      <pubDate>Wed, 01 Oct 2025 08:36:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/imx93-FRDM-mac-address-randomisation/m-p/2178674#M30239</guid>
      <dc:creator>sakshi123</dc:creator>
      <dc:date>2025-10-01T08:36:42Z</dc:date>
    </item>
    <item>
      <title>Re: imx93 FRDM mac address randomisation</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/imx93-FRDM-mac-address-randomisation/m-p/2178710#M30240</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/255353"&gt;@sakshi123&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I would suggest you configure a MAC address using ifconfig.&amp;nbsp; you can use the following command:&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;!--ScriptorStartFragment--&gt;ifconfig &amp;lt;interface&amp;gt; hw ether &amp;lt;MAC-address&amp;gt;&lt;!--ScriptorEndFragment--&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For example:&amp;nbsp;&amp;nbsp;&lt;!--ScriptorStartFragment--&gt;ifconfig eth0 hw ether 00:11:22:33:44:55&lt;!--ScriptorEndFragment--&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Daniel&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Oct 2025 10:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/imx93-FRDM-mac-address-randomisation/m-p/2178710#M30240</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2025-10-01T10:27:01Z</dc:date>
    </item>
    <item>
      <title>Re: imx93 FRDM mac address randomisation</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/imx93-FRDM-mac-address-randomisation/m-p/2179816#M30250</link>
      <description>&lt;P&gt;I have a follow-up question regarding the MAC address for the i.MX93 FRDM board.&lt;/P&gt;&lt;P&gt;From the i.MX93 FRDM datasheet (screenshot attached below), it is mentioned that:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sakshi123_2-1759483198532.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/359436iE88B77F1D95B0C47/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sakshi123_2-1759483198532.png" alt="sakshi123_2-1759483198532.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Question is :&amp;nbsp;Is there any physical setup on the i.MX93 board to configure or set a static MAC address for every bootup, or is the MAC address always fused and fixed inside the i.MX93 processor?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Oct 2025 09:22:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/imx93-FRDM-mac-address-randomisation/m-p/2179816#M30250</guid>
      <dc:creator>sakshi123</dc:creator>
      <dc:date>2025-10-03T09:22:27Z</dc:date>
    </item>
    <item>
      <title>Re: imx93 FRDM mac address randomisation</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/imx93-FRDM-mac-address-randomisation/m-p/2181725#M30286</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to below link to write MAC address.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX91-fusemap-spreadsheet-needed-to-write-MAC-addresses-into/m-p/2150691" target="_blank"&gt;Solved: i.MX91 fusemap spreadsheet needed to write MAC addresses into OTP - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 08 Oct 2025 08:49:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/imx93-FRDM-mac-address-randomisation/m-p/2181725#M30286</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2025-10-08T08:49:10Z</dc:date>
    </item>
  </channel>
</rss>