<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RW612: Using external NOR Flash on the PSRAM-QSPI lines in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/RW612-Using-external-NOR-Flash-on-the-PSRAM-QSPI-lines/m-p/2172736#M30118</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a custom board based on the &lt;STRONG&gt;RW612&lt;/STRONG&gt; module.&lt;BR /&gt;The module provides two QSPI/FlexSPI interfaces:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Port A1 → connected to the boot flash.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Port B1 → normally intended for an external PSRAM.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Since I do not use PSRAM, I would like to connect an &lt;STRONG&gt;external NOR Flash (Micron MT25QL01GBBB, 1 Gbit)&lt;/STRONG&gt; on Port B1 instead.&lt;/P&gt;&lt;P&gt;My questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Is it generally possible to use the “PSRAM port” (FlexSPI Port B1) for an additional NOR Flash device?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;What changes are required in the SDK examples to make this work?&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Do I only need to configure the pin-mux for Port B1 to route to the NOR Flash pins?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is it sufficient to set devicePort = kFLEXSPI_PortB1 and deviceType = kSerialNorCfgOption_DeviceType_ReadSFDP_SDR in flexspi_mem_config_t?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Can I rely on FLEXSPI_NOR_GenerateConfigBlockUsingSFDP to automatically configure the Micron flash device correctly?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;The current &lt;STRONG&gt;NOR Flash SDK examples&lt;/STRONG&gt;&amp;nbsp; doesn't work when I switch the parameters to Port B1. Is there an official way or example to use a &lt;STRONG&gt;second external NOR Flash&lt;/STRONG&gt; on Port B1?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;My goal is to use the NOR Flash as additional storage (erase/program/read), not as a boot device.&lt;/P&gt;&lt;P&gt;Any guidance or examples would be greatly appreciated!&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
    <pubDate>Fri, 19 Sep 2025 10:31:32 GMT</pubDate>
    <dc:creator>rkapoor</dc:creator>
    <dc:date>2025-09-19T10:31:32Z</dc:date>
    <item>
      <title>RW612: Using external NOR Flash on the PSRAM-QSPI lines</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/RW612-Using-external-NOR-Flash-on-the-PSRAM-QSPI-lines/m-p/2172736#M30118</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a custom board based on the &lt;STRONG&gt;RW612&lt;/STRONG&gt; module.&lt;BR /&gt;The module provides two QSPI/FlexSPI interfaces:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Port A1 → connected to the boot flash.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Port B1 → normally intended for an external PSRAM.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Since I do not use PSRAM, I would like to connect an &lt;STRONG&gt;external NOR Flash (Micron MT25QL01GBBB, 1 Gbit)&lt;/STRONG&gt; on Port B1 instead.&lt;/P&gt;&lt;P&gt;My questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Is it generally possible to use the “PSRAM port” (FlexSPI Port B1) for an additional NOR Flash device?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;What changes are required in the SDK examples to make this work?&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Do I only need to configure the pin-mux for Port B1 to route to the NOR Flash pins?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is it sufficient to set devicePort = kFLEXSPI_PortB1 and deviceType = kSerialNorCfgOption_DeviceType_ReadSFDP_SDR in flexspi_mem_config_t?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Can I rely on FLEXSPI_NOR_GenerateConfigBlockUsingSFDP to automatically configure the Micron flash device correctly?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;The current &lt;STRONG&gt;NOR Flash SDK examples&lt;/STRONG&gt;&amp;nbsp; doesn't work when I switch the parameters to Port B1. Is there an official way or example to use a &lt;STRONG&gt;second external NOR Flash&lt;/STRONG&gt; on Port B1?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;My goal is to use the NOR Flash as additional storage (erase/program/read), not as a boot device.&lt;/P&gt;&lt;P&gt;Any guidance or examples would be greatly appreciated!&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Fri, 19 Sep 2025 10:31:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/RW612-Using-external-NOR-Flash-on-the-PSRAM-QSPI-lines/m-p/2172736#M30118</guid>
      <dc:creator>rkapoor</dc:creator>
      <dc:date>2025-09-19T10:31:32Z</dc:date>
    </item>
  </channel>
</rss>