<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Productsのトピックmrf101</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/mrf101/m-p/2166612#M29975</link>
    <description>&lt;P&gt;I designed an amplifier that uses a single MRF101AN operating between 0-50 MHz. Using a 100 mA bias current, I get 53W output power with a 1W SSB-FM input power and a LPF in between. I consume 1.8 amps of power at 48 V. The transistor body and the heatsink are not overheated. Do I need to increase the bias current to 200 mA for a little more power?&lt;/P&gt;</description>
    <pubDate>Wed, 10 Sep 2025 11:14:19 GMT</pubDate>
    <dc:creator>onder</dc:creator>
    <dc:date>2025-09-10T11:14:19Z</dc:date>
    <item>
      <title>mrf101</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/mrf101/m-p/2166612#M29975</link>
      <description>&lt;P&gt;I designed an amplifier that uses a single MRF101AN operating between 0-50 MHz. Using a 100 mA bias current, I get 53W output power with a 1W SSB-FM input power and a LPF in between. I consume 1.8 amps of power at 48 V. The transistor body and the heatsink are not overheated. Do I need to increase the bias current to 200 mA for a little more power?&lt;/P&gt;</description>
      <pubDate>Wed, 10 Sep 2025 11:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/mrf101/m-p/2166612#M29975</guid>
      <dc:creator>onder</dc:creator>
      <dc:date>2025-09-10T11:14:19Z</dc:date>
    </item>
    <item>
      <title>Re: mrf101</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/mrf101/m-p/2168038#M30004</link>
      <description>&lt;P&gt;Hello Onder&lt;/P&gt;
&lt;P&gt;Good Day!&lt;/P&gt;
&lt;P&gt;Yes, you can increase the current up to 300mA, I just recommend that you do this process step by step, like 20mA-50mA, the first time to verify that the signal doesn't start to fluctuate.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RafaR_0-1757614160971.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356553iE188B206E8428392/image-size/medium?v=v2&amp;amp;px=400" role="button" title="RafaR_0-1757614160971.png" alt="RafaR_0-1757614160971.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;RafaR_0-1757614160971.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this information has helped you, please let me know if you need help with anything else.&lt;/P&gt;
&lt;P&gt;Have a great day and best of luck.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Sep 2025 18:10:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/mrf101/m-p/2168038#M30004</guid>
      <dc:creator>RafaR</dc:creator>
      <dc:date>2025-09-11T18:10:00Z</dc:date>
    </item>
  </channel>
</rss>