<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LX2160A Processor Errors in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/LX2160A-Processor-Errors/m-p/2160926#M29864</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;each interrupt ID corresponds to a cluster,&lt;/P&gt;
&lt;P&gt;the LX2160A has a Sixteen 32-bit/64-bit Arm v8 A72 CPUs arranged as clusters of two cores sharing a 1 MB L2 cache, it means if there is any error on one core the assigned cluster will trigger the corresponding interrupt, those interrupts&amp;nbsp;&lt;SPAN&gt;are ORed and connected to GIC at the mentioned ID slots, for more information about the interrupts you can refer to the ARM GIC manual.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 30 Aug 2025 04:00:17 GMT</pubDate>
    <dc:creator>Oswalag</dc:creator>
    <dc:date>2025-08-30T04:00:17Z</dc:date>
    <item>
      <title>LX2160A Processor Errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LX2160A-Processor-Errors/m-p/2159905#M29845</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;LX2160ARM.pdf specifies ORed error interrupts from processor clusters as Interrupt IDs 96...103.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where can I find a list of errors which are ORed in these interrupt?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Aug 2025 11:27:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LX2160A-Processor-Errors/m-p/2159905#M29845</guid>
      <dc:creator>bboykaz</dc:creator>
      <dc:date>2025-08-28T11:27:30Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160A Processor Errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LX2160A-Processor-Errors/m-p/2160926#M29864</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;each interrupt ID corresponds to a cluster,&lt;/P&gt;
&lt;P&gt;the LX2160A has a Sixteen 32-bit/64-bit Arm v8 A72 CPUs arranged as clusters of two cores sharing a 1 MB L2 cache, it means if there is any error on one core the assigned cluster will trigger the corresponding interrupt, those interrupts&amp;nbsp;&lt;SPAN&gt;are ORed and connected to GIC at the mentioned ID slots, for more information about the interrupts you can refer to the ARM GIC manual.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 30 Aug 2025 04:00:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LX2160A-Processor-Errors/m-p/2160926#M29864</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2025-08-30T04:00:17Z</dc:date>
    </item>
  </channel>
</rss>