<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Rotary Encoder Interfacing with PCAL9722 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Rotary-Encoder-Interfacing-with-PCAL9722/m-p/2150256#M29634</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes, the PCAL9722 supports interrupt functionality that can be configured by level or edge, and each interrupt can be cleared individually without affecting other interrupt events.&lt;/P&gt;
&lt;P&gt;For more details, please refer to Section 6.4.12 – Interrupt Edge Registers (60h to 65h) in the datasheet.&lt;/P&gt;
&lt;P&gt;Hope this helps!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 11 Aug 2025 17:45:05 GMT</pubDate>
    <dc:creator>ErikaC</dc:creator>
    <dc:date>2025-08-11T17:45:05Z</dc:date>
    <item>
      <title>Rotary Encoder Interfacing with PCAL9722</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Rotary-Encoder-Interfacing-with-PCAL9722/m-p/2149164#M29590</link>
      <description>&lt;P&gt;We are going to use Rotary incremental Encoder (&lt;STRONG&gt;Quadrature output&lt;/STRONG&gt;) via SPI to IO Expander.&lt;/P&gt;&lt;P&gt;As Rotary Encoder requires Interrupt pin to interface, can you please Confirm whether it is possible to interface Rotary Encoder with&amp;nbsp;&lt;STRONG&gt;PCAL9722 &lt;/STRONG&gt;I/O Expander?&lt;/P&gt;&lt;P&gt;Does&amp;nbsp;PCAL9722 supports interrupt on Rising as well as falling edge?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Fri, 08 Aug 2025 11:09:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Rotary-Encoder-Interfacing-with-PCAL9722/m-p/2149164#M29590</guid>
      <dc:creator>mk031</dc:creator>
      <dc:date>2025-08-08T11:09:40Z</dc:date>
    </item>
    <item>
      <title>Re: Rotary Encoder Interfacing with PCAL9722</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Rotary-Encoder-Interfacing-with-PCAL9722/m-p/2150256#M29634</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes, the PCAL9722 supports interrupt functionality that can be configured by level or edge, and each interrupt can be cleared individually without affecting other interrupt events.&lt;/P&gt;
&lt;P&gt;For more details, please refer to Section 6.4.12 – Interrupt Edge Registers (60h to 65h) in the datasheet.&lt;/P&gt;
&lt;P&gt;Hope this helps!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Aug 2025 17:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Rotary-Encoder-Interfacing-with-PCAL9722/m-p/2150256#M29634</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2025-08-11T17:45:05Z</dc:date>
    </item>
  </channel>
</rss>