<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックPE Micro Debugger Mulitlink is not working</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PE-Micro-Debugger-Mulitlink-is-not-working/m-p/2146225#M29522</link>
    <description>&lt;P&gt;Hi, I am using PE Micro Multilink LC Debug Probe when i connect the Multilink to Laptop the Driver its not showing in the Laptop - Device Manager. The Blue light is glowing in the device also when i connect the Debugger to the working board even Orange light is glowing.&lt;/P&gt;&lt;P&gt;But the device is not turned up which means&lt;BR /&gt;The message popping up says that&lt;BR /&gt;Erro in service launch sequence . The GDB server was not able to establish a connection to the target processor. Please check your connections and power. Verify that the launch setting in the Debug configuration are accurate. To run simultaneous debug sessions, please specify unique Server port and GDBMI Port in the Debug Configuration for Each Project.&lt;/P&gt;&lt;P&gt;So the above message is getting popped out&lt;BR /&gt;so whether the issue with the driver ?? or whether The device gets Bricked up or something. How to resolve this issue&lt;BR /&gt;when i connect Power supply LED is glowing but the device is not getting recognised. How to overcome this issue&lt;/P&gt;</description>
    <pubDate>Mon, 04 Aug 2025 13:36:15 GMT</pubDate>
    <dc:creator>Atkinson</dc:creator>
    <dc:date>2025-08-04T13:36:15Z</dc:date>
    <item>
      <title>PE Micro Debugger Mulitlink is not working</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PE-Micro-Debugger-Mulitlink-is-not-working/m-p/2146225#M29522</link>
      <description>&lt;P&gt;Hi, I am using PE Micro Multilink LC Debug Probe when i connect the Multilink to Laptop the Driver its not showing in the Laptop - Device Manager. The Blue light is glowing in the device also when i connect the Debugger to the working board even Orange light is glowing.&lt;/P&gt;&lt;P&gt;But the device is not turned up which means&lt;BR /&gt;The message popping up says that&lt;BR /&gt;Erro in service launch sequence . The GDB server was not able to establish a connection to the target processor. Please check your connections and power. Verify that the launch setting in the Debug configuration are accurate. To run simultaneous debug sessions, please specify unique Server port and GDBMI Port in the Debug Configuration for Each Project.&lt;/P&gt;&lt;P&gt;So the above message is getting popped out&lt;BR /&gt;so whether the issue with the driver ?? or whether The device gets Bricked up or something. How to resolve this issue&lt;BR /&gt;when i connect Power supply LED is glowing but the device is not getting recognised. How to overcome this issue&lt;/P&gt;</description>
      <pubDate>Mon, 04 Aug 2025 13:36:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PE-Micro-Debugger-Mulitlink-is-not-working/m-p/2146225#M29522</guid>
      <dc:creator>Atkinson</dc:creator>
      <dc:date>2025-08-04T13:36:15Z</dc:date>
    </item>
  </channel>
</rss>