<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How does P3S0210BQ determine whether the signal is I3C or I2C? in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/How-does-P3S0210BQ-determine-whether-the-signal-is-I3C-or-I2C/m-p/2115335#M28973</link>
    <description>&lt;DIV&gt;Dear Sean,&amp;nbsp;&lt;BR clear="none" /&gt;&lt;BR clear="none" /&gt;the P3S0210BQ is a protocol-aware bus switch designed by NXP that supports both I²C and I³C communication protocols. It automatically determines whether the bus is operating in I²C or I³C mode using a dynamic detection mechanism based on the characteristics of the bus traffic.&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;The P3S0210BQ's VLT uses edge-rate accelerator circuitry (for both the high-to-low and low-to-high), N-channel Pass gate transistor and a 10 kΩ pullup resistor (to provide DC-bias and drive capabilities) to meet these requirements. All of the ports (A/A1/A2 and B/B1/B2) have internal pullup resistors when enabled and the I/O status is HIGH. When I/O status is LOW or is disabled, the pullup resistors are disconnected The design is directionless and does not need direction control signal. The implementation supports both lowspeed Open-drain operation (I2C-bus) as well as high speed push-pull operation (I3C-bus or SPI-bus). The Nchannel Pass device is on only during LOW input cycle and off during HIGH input cycle.&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;For the I2C signal you will need to add external pull-up resistors in your design, to decrease the overall pull-up value depending on I2C communication speed, voltage and bus capacitance. 10k pull-up resistor values are usually too high.&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;
&lt;DIV id="tinyMceEditorJozefKozon_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_2-1749723953503.png" style="width: 485px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/342692iCDA6235CF2943C1A/image-dimensions/485x338?v=v2" width="485" height="338" role="button" title="JozefKozon_2-1749723953503.png" alt="JozefKozon_2-1749723953503.png" /&gt;&lt;/span&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;
&amp;nbsp;&lt;/DIV&gt;</description>
    <pubDate>Thu, 12 Jun 2025 10:27:10 GMT</pubDate>
    <dc:creator>JozefKozon</dc:creator>
    <dc:date>2025-06-12T10:27:10Z</dc:date>
    <item>
      <title>How does P3S0210BQ determine whether the signal is I3C or I2C?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/How-does-P3S0210BQ-determine-whether-the-signal-is-I3C-or-I2C/m-p/2115130#M28971</link>
      <description>&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;As title,&lt;/P&gt;&lt;P&gt;How does P3S0210BQ determine whether the signal is I3C or I2C?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;SeanWu&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jun 2025 07:37:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/How-does-P3S0210BQ-determine-whether-the-signal-is-I3C-or-I2C/m-p/2115130#M28971</guid>
      <dc:creator>seanwu</dc:creator>
      <dc:date>2025-06-12T07:37:43Z</dc:date>
    </item>
    <item>
      <title>Re: How does P3S0210BQ determine whether the signal is I3C or I2C?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/How-does-P3S0210BQ-determine-whether-the-signal-is-I3C-or-I2C/m-p/2115335#M28973</link>
      <description>&lt;DIV&gt;Dear Sean,&amp;nbsp;&lt;BR clear="none" /&gt;&lt;BR clear="none" /&gt;the P3S0210BQ is a protocol-aware bus switch designed by NXP that supports both I²C and I³C communication protocols. It automatically determines whether the bus is operating in I²C or I³C mode using a dynamic detection mechanism based on the characteristics of the bus traffic.&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;The P3S0210BQ's VLT uses edge-rate accelerator circuitry (for both the high-to-low and low-to-high), N-channel Pass gate transistor and a 10 kΩ pullup resistor (to provide DC-bias and drive capabilities) to meet these requirements. All of the ports (A/A1/A2 and B/B1/B2) have internal pullup resistors when enabled and the I/O status is HIGH. When I/O status is LOW or is disabled, the pullup resistors are disconnected The design is directionless and does not need direction control signal. The implementation supports both lowspeed Open-drain operation (I2C-bus) as well as high speed push-pull operation (I3C-bus or SPI-bus). The Nchannel Pass device is on only during LOW input cycle and off during HIGH input cycle.&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;For the I2C signal you will need to add external pull-up resistors in your design, to decrease the overall pull-up value depending on I2C communication speed, voltage and bus capacitance. 10k pull-up resistor values are usually too high.&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;
&lt;DIV id="tinyMceEditorJozefKozon_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_2-1749723953503.png" style="width: 485px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/342692iCDA6235CF2943C1A/image-dimensions/485x338?v=v2" width="485" height="338" role="button" title="JozefKozon_2-1749723953503.png" alt="JozefKozon_2-1749723953503.png" /&gt;&lt;/span&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;
&amp;nbsp;&lt;/DIV&gt;</description>
      <pubDate>Thu, 12 Jun 2025 10:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/How-does-P3S0210BQ-determine-whether-the-signal-is-I3C-or-I2C/m-p/2115335#M28973</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2025-06-12T10:27:10Z</dc:date>
    </item>
  </channel>
</rss>