<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: Regarding PXS30 micro controller</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Regarding-PXS30-micro-controller/m-p/278832#M2874</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The solution can be used only if entire system has the same voltage. Moreover, you have to use P and N type of the devices because you will not be able to drive upper part of the H-bridge. The N-Fet you want to use has long fall time so it could be used, I suppose, up to 10kHz. &lt;/P&gt;&lt;P&gt;If you want to use voltage and switching devices, you have decided, then the solution is driver for devices switching.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Jul 2013 08:11:17 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2013-07-18T08:11:17Z</dc:date>
    <item>
      <title>Regarding PXS30 micro controller</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Regarding-PXS30-micro-controller/m-p/278831#M2873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I am going to use PXS3020 micro controller for my application&lt;/P&gt;&lt;P&gt;In the reference manual it is said that Each sub module is capable of &lt;/P&gt;&lt;P&gt;Driving one&amp;nbsp; half H Bridge.&lt;/P&gt;&lt;P&gt;I am going to switch 6 to 8V using&amp;nbsp; 4 MOSFET to form a H bridge.Load is coil &lt;/P&gt;&lt;P&gt;which is connected in between the H Bridge which operates in&amp;nbsp; the current of &lt;/P&gt;&lt;P&gt;50 to 100mA.&lt;/P&gt;&lt;P&gt;The MOSFET part number selected is Si2314EDS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any MOSFET driving circuit required for the above application..?or &lt;/P&gt;&lt;P&gt;shall I connect PXS3020 micro controller output directly to the 4 MOSFET.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2013 05:12:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Regarding-PXS30-micro-controller/m-p/278831#M2873</guid>
      <dc:creator>rajvelm</dc:creator>
      <dc:date>2013-07-18T05:12:32Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding PXS30 micro controller</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Regarding-PXS30-micro-controller/m-p/278832#M2874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The solution can be used only if entire system has the same voltage. Moreover, you have to use P and N type of the devices because you will not be able to drive upper part of the H-bridge. The N-Fet you want to use has long fall time so it could be used, I suppose, up to 10kHz. &lt;/P&gt;&lt;P&gt;If you want to use voltage and switching devices, you have decided, then the solution is driver for devices switching.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2013 08:11:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Regarding-PXS30-micro-controller/m-p/278832#M2874</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2013-07-18T08:11:17Z</dc:date>
    </item>
  </channel>
</rss>