<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX93 M33 add LPSPI3 initialize code in ethosu_app_rpmsg in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/IMX93-M33-add-LPSPI3-initialize-code-in-ethosu-app-rpmsg/m-p/2087154#M28436</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using both M33 and A55 (imx93). I want to drive a lcd screen from MCU ( LPSPI3) in project ethosu_app_rpmsg.&lt;/P&gt;&lt;P&gt;When i compile this project and move the output elf file to A55(imx93) to execute, unexcepted error occurred:&lt;/P&gt;&lt;P&gt;INFO: [ 267.292524] remoteproc remoteproc0: powering up imx-rproc&lt;BR /&gt;Ethosu delegate: [ 267.298756] remoteproc remoteproc0: Booting fw image ethosu_firmware, size 244976&lt;BR /&gt;device_name set to /dev/ethosu0.&lt;BR /&gt;INFO: Ethosu delegate: cache_file_path set to .&lt;BR /&gt;INFO: Ethosu delegate: timeout[ 267.316902] imx-rproc imx93-cm33: Translation failed: da = 0xffed550 len = 0x12c20&lt;BR /&gt;set to 60000000000.&lt;BR /&gt;INFO: Ethos[ 267.327253] remoteproc remoteproc0: bad phdr da 0xffed550 mem 0x12c20&lt;BR /&gt;u delegate: enable_cycle_counter[ 267.336496] remoteproc remoteproc0: Failed to load program segments: -22&lt;BR /&gt;set to 0.&lt;BR /&gt;INFO:[ 267.344747] ethosu ethosu: could not boot a remote processor&lt;BR /&gt;Ethosu delegate: enable_profiling set to 0.&lt;BR /&gt;INFO: Ethosu delegate: profiling_buffer_size set to 2048.&lt;BR /&gt;INFO: Ethosu delegate: pmu_event0 set t[ 267.361698] Unable to handle kernel paging request at virtual address ffff80000af9802c&lt;BR /&gt;o 0.&lt;BR /&gt;INFO: Ethos[ 267.371056] Mem abort info:&lt;BR /&gt;u delegate: pmu_e[ 267.375858] ESR = 0x0000000096000047&lt;BR /&gt;vent1 set to 0.&lt;BR /&gt;[ 267.380844] EC = 0x25: DABT (current EL), IL = 32 bits&lt;BR /&gt;INFO: Ethosu delegate: pmu_event[ 267.389144] SET = 0, FnV = 0&lt;BR /&gt;2 set to 0.&lt;BR /&gt;INFO[ 267.393652] EA = 0, S1PTW = 0&lt;BR /&gt;: Ethosu delegate: pmu_event3 set to 0.&lt;BR /&gt;[ 267.403537] FSC = 0x07: level 3 translation fault&lt;BR /&gt;[ 267.408497] Data abort info:&lt;BR /&gt;[ 267.411368] ISV = 0, ISS = 0x00000047&lt;BR /&gt;[ 267.415973] CM = 0, WnR = 1&lt;BR /&gt;[ 267.418943] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000081bd0000&lt;BR /&gt;[ 267.426297] [ffff80000af9802c] pgd=10000000bffff003, p4d=10000000bffff003, pud=10000000bfffe003, pmd=10000000849d3003, pte=0000000000000000&lt;BR /&gt;[ 267.439240] Internal error: Oops: 0000000096000047 [#1] PREEMPT SMP&lt;BR /&gt;[ 267.445497] Modules linked in: rpmsg_ctrl rpmsg_char crct10dif_ce polyval_ce polyval_generic flexcan layerscape_edac_mod soc_imx9 nvmem_imx_ocotp_fsb_s400 can_dev imx8_media_dev(Ce&lt;BR /&gt;[ 267.462009] CPU: 1 PID: 575 Comm: imx93_app Tainted: G C 6.1.55 #2&lt;BR /&gt;[ 267.469564] Hardware name: ATK-DLIMX93 Development board (DT)&lt;BR /&gt;[ 267.475294] pstate: 40400009 (nZcv daif +PAN -UAO -TCO -DIT -SSBS BTYPE=--)&lt;BR /&gt;[ 267.482243] pc : virtqueue_add_split+0x168/0x550&lt;BR /&gt;[ 267.486854] lr : virtqueue_add_split+0x144/0x550&lt;BR /&gt;[ 267.491456] sp : ffff80000ad73b70&lt;BR /&gt;[ 267.494757] x29: ffff80000ad73b70 x28: 0000000000000000 x27: 0000000000000400&lt;BR /&gt;[ 267.501882] x26: ffff80000ad73c40 x25: 0000000000000001 x24: 0000000000000001&lt;BR /&gt;[ 267.509006] x23: 0000000000000000 x22: ffff80000af98000 x21: 0000000000000002&lt;BR /&gt;[ 267.516130] x20: 0000000000000002 x19: ffff000005907000 x18: 0000000000000000&lt;BR /&gt;[ 267.523254] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000&lt;BR /&gt;[ 267.530378] x14: 0000000000000000 x13: 0000000000000000 x12: 0000000000000000&lt;BR /&gt;[ 267.537501] x11: 0000000000000000 x10: 0000000000000000 x9 : 0000000000000000&lt;BR /&gt;[ 267.544626] x8 : ffff80000ad73c60 x7 : ffff00000579a000 x6 : 0000000000000000&lt;BR /&gt;[ 267.551750] x5 : 000000000000001c x4 : 0000000000000001 x3 : 0000000000000020&lt;BR /&gt;[ 267.558874] x2 : ffff80000af98020 x1 : fffffc0000a03800 x0 : 00000000a80e0800&lt;BR /&gt;[ 267.565998] Call trace:&lt;BR /&gt;[ 267.568434] virtqueue_add_split+0x168/0x550&lt;BR /&gt;[ 267.572697] virtqueue_add_outbuf+0x48/0x5c&lt;BR /&gt;[ 267.576874] rpmsg_send_offchannel_raw+0x2c4/0x3a0&lt;BR /&gt;[ 267.581658] virtio_rpmsg_send+0x28/0x34&lt;BR /&gt;[ 267.585567] rpmsg_send+0x20/0x40&lt;BR /&gt;[ 267.588877] ethosu_rpmsg_version_request+0x4c/0xa0&lt;BR /&gt;[ 267.593748] ethosu_ioctl+0x140/0x2a0&lt;BR /&gt;[ 267.597397] __arm64_sys_ioctl+0xac/0xf0&lt;BR /&gt;[ 267.601314] invoke_syscall+0x48/0x114&lt;BR /&gt;[ 267.605058] el0_svc_common.constprop.0+0x44/0xec&lt;BR /&gt;[ 267.609747] do_el0_svc+0x2c/0xd0&lt;BR /&gt;[ 267.613049] el0_svc+0x2c/0x84&lt;BR /&gt;[ 267.616099] el0t_64_sync_handler+0xf4/0x120&lt;BR /&gt;[ 267.620355] el0t_64_sync+0x18c/0x190&lt;BR /&gt;[ 267.624007] Code: d37c7ea3 b9400f45 8b0302c2 f9404a67 (79001858)&lt;BR /&gt;[ 267.630080] ---[ end trace 0000000000000000 ]---&lt;/P&gt;&lt;P&gt;Message from syslogd@atk-imx93 at Thu Mar 9 10:25:37 2023 ...&lt;BR /&gt;kernel: Code: d37c7ea3 b9400f45 8b0302c2 f9404a67 (79001858)&lt;/P&gt;&lt;P&gt;Message from syslogd@atk-imx93 at Thu Mar 9 10:25:37 2023 ...&lt;BR /&gt;kernel: Internal error: Oops: 0000000096000047 [#1] PREEMPT SMP&lt;BR /&gt;Segmentation fault&lt;/P&gt;&lt;P&gt;If you can help !&lt;/P&gt;</description>
    <pubDate>Fri, 25 Apr 2025 08:02:07 GMT</pubDate>
    <dc:creator>lzxxxx</dc:creator>
    <dc:date>2025-04-25T08:02:07Z</dc:date>
    <item>
      <title>IMX93 M33 add LPSPI3 initialize code in ethosu_app_rpmsg</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IMX93-M33-add-LPSPI3-initialize-code-in-ethosu-app-rpmsg/m-p/2087154#M28436</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using both M33 and A55 (imx93). I want to drive a lcd screen from MCU ( LPSPI3) in project ethosu_app_rpmsg.&lt;/P&gt;&lt;P&gt;When i compile this project and move the output elf file to A55(imx93) to execute, unexcepted error occurred:&lt;/P&gt;&lt;P&gt;INFO: [ 267.292524] remoteproc remoteproc0: powering up imx-rproc&lt;BR /&gt;Ethosu delegate: [ 267.298756] remoteproc remoteproc0: Booting fw image ethosu_firmware, size 244976&lt;BR /&gt;device_name set to /dev/ethosu0.&lt;BR /&gt;INFO: Ethosu delegate: cache_file_path set to .&lt;BR /&gt;INFO: Ethosu delegate: timeout[ 267.316902] imx-rproc imx93-cm33: Translation failed: da = 0xffed550 len = 0x12c20&lt;BR /&gt;set to 60000000000.&lt;BR /&gt;INFO: Ethos[ 267.327253] remoteproc remoteproc0: bad phdr da 0xffed550 mem 0x12c20&lt;BR /&gt;u delegate: enable_cycle_counter[ 267.336496] remoteproc remoteproc0: Failed to load program segments: -22&lt;BR /&gt;set to 0.&lt;BR /&gt;INFO:[ 267.344747] ethosu ethosu: could not boot a remote processor&lt;BR /&gt;Ethosu delegate: enable_profiling set to 0.&lt;BR /&gt;INFO: Ethosu delegate: profiling_buffer_size set to 2048.&lt;BR /&gt;INFO: Ethosu delegate: pmu_event0 set t[ 267.361698] Unable to handle kernel paging request at virtual address ffff80000af9802c&lt;BR /&gt;o 0.&lt;BR /&gt;INFO: Ethos[ 267.371056] Mem abort info:&lt;BR /&gt;u delegate: pmu_e[ 267.375858] ESR = 0x0000000096000047&lt;BR /&gt;vent1 set to 0.&lt;BR /&gt;[ 267.380844] EC = 0x25: DABT (current EL), IL = 32 bits&lt;BR /&gt;INFO: Ethosu delegate: pmu_event[ 267.389144] SET = 0, FnV = 0&lt;BR /&gt;2 set to 0.&lt;BR /&gt;INFO[ 267.393652] EA = 0, S1PTW = 0&lt;BR /&gt;: Ethosu delegate: pmu_event3 set to 0.&lt;BR /&gt;[ 267.403537] FSC = 0x07: level 3 translation fault&lt;BR /&gt;[ 267.408497] Data abort info:&lt;BR /&gt;[ 267.411368] ISV = 0, ISS = 0x00000047&lt;BR /&gt;[ 267.415973] CM = 0, WnR = 1&lt;BR /&gt;[ 267.418943] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000081bd0000&lt;BR /&gt;[ 267.426297] [ffff80000af9802c] pgd=10000000bffff003, p4d=10000000bffff003, pud=10000000bfffe003, pmd=10000000849d3003, pte=0000000000000000&lt;BR /&gt;[ 267.439240] Internal error: Oops: 0000000096000047 [#1] PREEMPT SMP&lt;BR /&gt;[ 267.445497] Modules linked in: rpmsg_ctrl rpmsg_char crct10dif_ce polyval_ce polyval_generic flexcan layerscape_edac_mod soc_imx9 nvmem_imx_ocotp_fsb_s400 can_dev imx8_media_dev(Ce&lt;BR /&gt;[ 267.462009] CPU: 1 PID: 575 Comm: imx93_app Tainted: G C 6.1.55 #2&lt;BR /&gt;[ 267.469564] Hardware name: ATK-DLIMX93 Development board (DT)&lt;BR /&gt;[ 267.475294] pstate: 40400009 (nZcv daif +PAN -UAO -TCO -DIT -SSBS BTYPE=--)&lt;BR /&gt;[ 267.482243] pc : virtqueue_add_split+0x168/0x550&lt;BR /&gt;[ 267.486854] lr : virtqueue_add_split+0x144/0x550&lt;BR /&gt;[ 267.491456] sp : ffff80000ad73b70&lt;BR /&gt;[ 267.494757] x29: ffff80000ad73b70 x28: 0000000000000000 x27: 0000000000000400&lt;BR /&gt;[ 267.501882] x26: ffff80000ad73c40 x25: 0000000000000001 x24: 0000000000000001&lt;BR /&gt;[ 267.509006] x23: 0000000000000000 x22: ffff80000af98000 x21: 0000000000000002&lt;BR /&gt;[ 267.516130] x20: 0000000000000002 x19: ffff000005907000 x18: 0000000000000000&lt;BR /&gt;[ 267.523254] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000&lt;BR /&gt;[ 267.530378] x14: 0000000000000000 x13: 0000000000000000 x12: 0000000000000000&lt;BR /&gt;[ 267.537501] x11: 0000000000000000 x10: 0000000000000000 x9 : 0000000000000000&lt;BR /&gt;[ 267.544626] x8 : ffff80000ad73c60 x7 : ffff00000579a000 x6 : 0000000000000000&lt;BR /&gt;[ 267.551750] x5 : 000000000000001c x4 : 0000000000000001 x3 : 0000000000000020&lt;BR /&gt;[ 267.558874] x2 : ffff80000af98020 x1 : fffffc0000a03800 x0 : 00000000a80e0800&lt;BR /&gt;[ 267.565998] Call trace:&lt;BR /&gt;[ 267.568434] virtqueue_add_split+0x168/0x550&lt;BR /&gt;[ 267.572697] virtqueue_add_outbuf+0x48/0x5c&lt;BR /&gt;[ 267.576874] rpmsg_send_offchannel_raw+0x2c4/0x3a0&lt;BR /&gt;[ 267.581658] virtio_rpmsg_send+0x28/0x34&lt;BR /&gt;[ 267.585567] rpmsg_send+0x20/0x40&lt;BR /&gt;[ 267.588877] ethosu_rpmsg_version_request+0x4c/0xa0&lt;BR /&gt;[ 267.593748] ethosu_ioctl+0x140/0x2a0&lt;BR /&gt;[ 267.597397] __arm64_sys_ioctl+0xac/0xf0&lt;BR /&gt;[ 267.601314] invoke_syscall+0x48/0x114&lt;BR /&gt;[ 267.605058] el0_svc_common.constprop.0+0x44/0xec&lt;BR /&gt;[ 267.609747] do_el0_svc+0x2c/0xd0&lt;BR /&gt;[ 267.613049] el0_svc+0x2c/0x84&lt;BR /&gt;[ 267.616099] el0t_64_sync_handler+0xf4/0x120&lt;BR /&gt;[ 267.620355] el0t_64_sync+0x18c/0x190&lt;BR /&gt;[ 267.624007] Code: d37c7ea3 b9400f45 8b0302c2 f9404a67 (79001858)&lt;BR /&gt;[ 267.630080] ---[ end trace 0000000000000000 ]---&lt;/P&gt;&lt;P&gt;Message from syslogd@atk-imx93 at Thu Mar 9 10:25:37 2023 ...&lt;BR /&gt;kernel: Code: d37c7ea3 b9400f45 8b0302c2 f9404a67 (79001858)&lt;/P&gt;&lt;P&gt;Message from syslogd@atk-imx93 at Thu Mar 9 10:25:37 2023 ...&lt;BR /&gt;kernel: Internal error: Oops: 0000000096000047 [#1] PREEMPT SMP&lt;BR /&gt;Segmentation fault&lt;/P&gt;&lt;P&gt;If you can help !&lt;/P&gt;</description>
      <pubDate>Fri, 25 Apr 2025 08:02:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IMX93-M33-add-LPSPI3-initialize-code-in-ethosu-app-rpmsg/m-p/2087154#M28436</guid>
      <dc:creator>lzxxxx</dc:creator>
      <dc:date>2025-04-25T08:02:07Z</dc:date>
    </item>
    <item>
      <title>Re: IMX93 M33 add LPSPI3 initialize code in ethosu_app_rpmsg</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IMX93-M33-add-LPSPI3-initialize-code-in-ethosu-app-rpmsg/m-p/2087372#M28448</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Please check:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX93-RPMsg-intercore-communications-question/td-p/1832545?profile.language=en" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/i-MX93-RPMsg-intercore-communications-question/td-p/1832545?profile.language=en&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Fri, 25 Apr 2025 14:44:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IMX93-M33-add-LPSPI3-initialize-code-in-ethosu-app-rpmsg/m-p/2087372#M28448</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-04-25T14:44:41Z</dc:date>
    </item>
  </channel>
</rss>