<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: RCP Timeout and Crash Under High Command Load (Flooding) with Framing Errors</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/RCP-Timeout-and-Crash-Under-High-Command-Load-Flooding-with/m-p/2086007#M28422</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Are you following an application note for doing the test?&lt;/P&gt;
&lt;P&gt;I notice that you are using a different link for OpenThread,&amp;nbsp; Could you please try with this Github by NXP&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/NXP/ot-nxp/blob/release/v1.4.0/src/k32w0/jn5189/README.md" target="_blank"&gt;https://github.com/NXP/ot-nxp/blob/release/v1.4.0/src/k32w0/jn5189/README.md&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 23 Apr 2025 22:30:44 GMT</pubDate>
    <dc:creator>luis_maravilla</dc:creator>
    <dc:date>2025-04-23T22:30:44Z</dc:date>
    <item>
      <title>RCP Timeout and Crash Under High Command Load (Flooding) with Framing Errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/RCP-Timeout-and-Crash-Under-High-Command-Load-Flooding-with/m-p/2084614#M28400</link>
      <description>&lt;P&gt;Issue Description&lt;BR /&gt;When flooding control commands (e.g., repeated On/Off cluster commands) from the ChipTool APK to a Thread end device (Nanoleaf), the otbr-agent crashes due to an RCP timeout and framing errors in the RCP communication layer.&lt;/P&gt;&lt;P&gt;Tested with Below Configurations&lt;BR /&gt;Baud 115200 and 460800&lt;BR /&gt;NCP_TX_BUFFER - 1024 and 4096&lt;/P&gt;&lt;P&gt;Environment&lt;BR /&gt;OTBR - otbr-posix (OpenThread Border Router)&lt;BR /&gt;Repository:&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://github.com/openthread/ot-br-posix.git" target="_blank" rel="noopener"&gt;https://github.com/openthread/ot-br-posix.git&lt;/A&gt;&lt;BR /&gt;Branch: main&lt;BR /&gt;Commit: 6112f9802f32c41b15ble331bf391c2c0f86bbc5&lt;/P&gt;&lt;P&gt;RCP Hardware: NXP JN5189&lt;BR /&gt;RCP Firmware - Repository:&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://github.com/openthread/ot-nxp.git" target="_blank" rel="noopener"&gt;https://github.com/openthread/ot-nxp.git&lt;/A&gt;&lt;BR /&gt;Branch: main&lt;BR /&gt;Commit:&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://github.com/openthread/ot-nxp/commit/70a5b2dd33ff30e938aac7556a84804a84ce05a9" target="_blank" rel="noopener"&gt;openthread/ot-nxp@70a5b2d&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Host OS: Linux (OpenWRT)&lt;BR /&gt;Thread version: 1.4.0&lt;/P&gt;&lt;P&gt;Commissioner: ChipTool APK (Android)&lt;/P&gt;&lt;P&gt;End Device: Nanoleaf Thread Device&lt;/P&gt;&lt;P&gt;Reproduction Steps&lt;BR /&gt;Commission the Nanoleaf device onto the Thread network via OTBR.&lt;BR /&gt;Use ChipTool APK to send rapid commands (e.g., toggle command in a loop with minimal delay).&lt;BR /&gt;Observe otbr-agent logs for framing errors and eventual timeout crash.&lt;/P&gt;&lt;P&gt;I've&amp;nbsp; attached OTBR Agent Log and&amp;nbsp;For Compilation Purpose I've applied the below patches on top of the vanilla ot-nxp repo&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Apr 2025 12:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/RCP-Timeout-and-Crash-Under-High-Command-Load-Flooding-with/m-p/2084614#M28400</guid>
      <dc:creator>Vvg1997</dc:creator>
      <dc:date>2025-04-22T12:04:02Z</dc:date>
    </item>
    <item>
      <title>Re: RCP Timeout and Crash Under High Command Load (Flooding) with Framing Errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/RCP-Timeout-and-Crash-Under-High-Command-Load-Flooding-with/m-p/2086007#M28422</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Are you following an application note for doing the test?&lt;/P&gt;
&lt;P&gt;I notice that you are using a different link for OpenThread,&amp;nbsp; Could you please try with this Github by NXP&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/NXP/ot-nxp/blob/release/v1.4.0/src/k32w0/jn5189/README.md" target="_blank"&gt;https://github.com/NXP/ot-nxp/blob/release/v1.4.0/src/k32w0/jn5189/README.md&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Apr 2025 22:30:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/RCP-Timeout-and-Crash-Under-High-Command-Load-Flooding-with/m-p/2086007#M28422</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-04-23T22:30:44Z</dc:date>
    </item>
    <item>
      <title>Re: RCP Timeout and Crash Under High Command Load (Flooding) with Framing Errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/RCP-Timeout-and-Crash-Under-High-Command-Load-Flooding-with/m-p/2086566#M28430</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for pointing that out.&lt;/P&gt;&lt;P&gt;To clarify, I wasn’t following any specific application note for this test. The OpenThread repo I referenced is, to the best of my knowledge, the official OT-NXP repository. The one you've shared appears to be a user-forked version rather than the mainline maintained by NXP.&lt;/P&gt;&lt;P&gt;I did give the repo you linked a try.&lt;BR /&gt;1) However, when building with the SDK version specified in the README (SDK_6_3), I ran into build errors (find it in the attached log files). On the other hand, using SDK_6_16, I was able to successfully compile without issues.&lt;BR /&gt;2) There's no such folder as "mr3_fixes" inside "third_party/jn5189_sdk" as specified in the README file for applying patch (patch_jn5189_mr3_sdk.sh). I proceeded with the build without applying them&lt;BR /&gt;&lt;BR /&gt;After building successfully i flashed the RCP binary and once again tried to test, But still facing the same issue.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Apr 2025 11:20:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/RCP-Timeout-and-Crash-Under-High-Command-Load-Flooding-with/m-p/2086566#M28430</guid>
      <dc:creator>Vvg1997</dc:creator>
      <dc:date>2025-04-24T11:20:09Z</dc:date>
    </item>
    <item>
      <title>Re: RCP Timeout and Crash Under High Command Load (Flooding) with Framing Errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/RCP-Timeout-and-Crash-Under-High-Command-Load-Flooding-with/m-p/2102857#M28726</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;NXP is currently migrating information to update the Open Thread GitHub repository. Both repositories are official NXP repositories. The one I shared will be the primary github for future support by NXP as will get more updates later.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I would recommend checking on NXP examples for Open Thread Border Router for future I.MX reference&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/meta-nxp-connectivity/tree/imx_matter_2024_q4?tab=readme-ov-file#how-to-setup-openthread-border-router-and-openther-deamon-on-the-target" target="_blank"&gt;GitHub - nxp-imx/meta-nxp-connectivity at imx_matter_2024_q4&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;</description>
      <pubDate>Thu, 22 May 2025 16:20:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/RCP-Timeout-and-Crash-Under-High-Command-Load-Flooding-with/m-p/2102857#M28726</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-05-22T16:20:34Z</dc:date>
    </item>
  </channel>
</rss>