<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GD3162 gate driver in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/GD3162-gate-driver/m-p/2056135#M27708</link>
    <description>&lt;P&gt;Hi Akshat,&lt;/P&gt;
&lt;P&gt;DESAT_LEB (Leading Edge Blanking Time) -&amp;nbsp;This is the initial delay after the gate driver turns ON the power device, during which DESAT detection is ignored to prevent false triggering from transient spikes. The purpose is,&amp;nbsp;when an IGBT or SiC MOSFET turns ON, there is a natural transient period where VCE/VDS momentarily spikes due to switching dynamics. DESAT_LEB prevents the gate driver from falsely detecting a desaturation event during this period.&amp;nbsp;Think of DESAT_LEB as a "safe startup window" where DESAT protection is temporarily disabled to avoid false faults.&lt;/P&gt;
&lt;P&gt;DESAT Filter Time -&amp;nbsp;This is the additional delay after DESAT_LEB before a DESAT fault is actually triggered.&amp;nbsp;Even after DESAT_LEB ends, noise or transient overshoots may cause momentary high VCE/VDS readings. The DESAT filter time ensures that only sustained high VCE/VDS triggers a DESAT fault.&amp;nbsp;Think of DESAT filter time as a "confirmation delay" to ensure only real desaturation events trigger a fault.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
    <pubDate>Wed, 05 Mar 2025 09:11:30 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2025-03-05T09:11:30Z</dc:date>
    <item>
      <title>GD3162 gate driver</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/GD3162-gate-driver/m-p/2056013#M27702</link>
      <description>&lt;P&gt;Hi NXP,&lt;BR /&gt;Please clarify the difference between DESAT_LED (Leading edge blanking time and DESAT filter time). Is it so that the DESA_LEB refers to the programmable time after which Vds will be on?&lt;/P&gt;</description>
      <pubDate>Wed, 05 Mar 2025 06:30:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/GD3162-gate-driver/m-p/2056013#M27702</guid>
      <dc:creator>Akshat_VE02376</dc:creator>
      <dc:date>2025-03-05T06:30:04Z</dc:date>
    </item>
    <item>
      <title>Re: GD3162 gate driver</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/GD3162-gate-driver/m-p/2056135#M27708</link>
      <description>&lt;P&gt;Hi Akshat,&lt;/P&gt;
&lt;P&gt;DESAT_LEB (Leading Edge Blanking Time) -&amp;nbsp;This is the initial delay after the gate driver turns ON the power device, during which DESAT detection is ignored to prevent false triggering from transient spikes. The purpose is,&amp;nbsp;when an IGBT or SiC MOSFET turns ON, there is a natural transient period where VCE/VDS momentarily spikes due to switching dynamics. DESAT_LEB prevents the gate driver from falsely detecting a desaturation event during this period.&amp;nbsp;Think of DESAT_LEB as a "safe startup window" where DESAT protection is temporarily disabled to avoid false faults.&lt;/P&gt;
&lt;P&gt;DESAT Filter Time -&amp;nbsp;This is the additional delay after DESAT_LEB before a DESAT fault is actually triggered.&amp;nbsp;Even after DESAT_LEB ends, noise or transient overshoots may cause momentary high VCE/VDS readings. The DESAT filter time ensures that only sustained high VCE/VDS triggers a DESAT fault.&amp;nbsp;Think of DESAT filter time as a "confirmation delay" to ensure only real desaturation events trigger a fault.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Wed, 05 Mar 2025 09:11:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/GD3162-gate-driver/m-p/2056135#M27708</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-03-05T09:11:30Z</dc:date>
    </item>
  </channel>
</rss>