<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックAutomatic Power-On Behavior for i.MX8MP with overtemperature</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Automatic-Power-On-Behavior-for-i-MX8MP-with-overtemperature/m-p/2034471#M27301</link>
    <description>&lt;P&gt;I am using a congatec SMARC module with a imx8mp processor.&lt;/P&gt;&lt;P&gt;To clarify our requirements:&lt;/P&gt;&lt;P&gt;When the temperature sensor on the SMARC module reaches 105°C, the system powers off.&lt;/P&gt;&lt;P&gt;Currently, the system requires a manual power cycle to restart.&lt;/P&gt;&lt;P&gt;I would like to modify this behaviour so that the system automatically powers back on when the temperature falls below the trigger threshold.&lt;/P&gt;&lt;P&gt;We found references suggesting that this behaviour could be modified in the SCFW (System Controller Firmware). However, the SCFW firmware is not used for the i.MX8MP processor.&lt;/P&gt;&lt;P&gt;The boot sequence for the i.MX8MP is as follows:&lt;/P&gt;&lt;P&gt;BootROM → SPL → BL31 (ATF - ARM Trusted Firmware) → OP-TEE (Optional) → BL33 (U-Boot) → Linux kernel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Based on our understanding, potential areas to address this behaviour include:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;a) Modifying BL31 (ATF).&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Adjusting settings within the SNVS (Secure Non-Volatile Storage).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;b) Configuring the PMIC PCA9450C present on the SMARC module to enable auto-power-on.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the PMIC configuration is the correct path, could you provide documentation or details on configuring the PCA9450C for automatic power-on?&lt;/P&gt;&lt;P&gt;Or, do you have a better solution?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 27 Jan 2025 10:12:24 GMT</pubDate>
    <dc:creator>Marco_Savo</dc:creator>
    <dc:date>2025-01-27T10:12:24Z</dc:date>
    <item>
      <title>Automatic Power-On Behavior for i.MX8MP with overtemperature</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Automatic-Power-On-Behavior-for-i-MX8MP-with-overtemperature/m-p/2034471#M27301</link>
      <description>&lt;P&gt;I am using a congatec SMARC module with a imx8mp processor.&lt;/P&gt;&lt;P&gt;To clarify our requirements:&lt;/P&gt;&lt;P&gt;When the temperature sensor on the SMARC module reaches 105°C, the system powers off.&lt;/P&gt;&lt;P&gt;Currently, the system requires a manual power cycle to restart.&lt;/P&gt;&lt;P&gt;I would like to modify this behaviour so that the system automatically powers back on when the temperature falls below the trigger threshold.&lt;/P&gt;&lt;P&gt;We found references suggesting that this behaviour could be modified in the SCFW (System Controller Firmware). However, the SCFW firmware is not used for the i.MX8MP processor.&lt;/P&gt;&lt;P&gt;The boot sequence for the i.MX8MP is as follows:&lt;/P&gt;&lt;P&gt;BootROM → SPL → BL31 (ATF - ARM Trusted Firmware) → OP-TEE (Optional) → BL33 (U-Boot) → Linux kernel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Based on our understanding, potential areas to address this behaviour include:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;a) Modifying BL31 (ATF).&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Adjusting settings within the SNVS (Secure Non-Volatile Storage).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;b) Configuring the PMIC PCA9450C present on the SMARC module to enable auto-power-on.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the PMIC configuration is the correct path, could you provide documentation or details on configuring the PCA9450C for automatic power-on?&lt;/P&gt;&lt;P&gt;Or, do you have a better solution?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jan 2025 10:12:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Automatic-Power-On-Behavior-for-i-MX8MP-with-overtemperature/m-p/2034471#M27301</guid>
      <dc:creator>Marco_Savo</dc:creator>
      <dc:date>2025-01-27T10:12:24Z</dc:date>
    </item>
    <item>
      <title>Re: Automatic Power-On Behavior for i.MX8MP with overtemperature</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Automatic-Power-On-Behavior-for-i-MX8MP-with-overtemperature/m-p/2037368#M27363</link>
      <description>dear Marco_Savo,&lt;BR /&gt;to modify the BL31 is not an option.&lt;BR /&gt;your second option is not posible due you have to assert the  PMIC_ON_REQ in order to start the power-on sequence it hasn't an auto power-on.&lt;BR /&gt;You could use a FPGA to assert the PMIC_ON_REQ signal.</description>
      <pubDate>Mon, 03 Feb 2025 18:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Automatic-Power-On-Behavior-for-i-MX8MP-with-overtemperature/m-p/2037368#M27363</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2025-02-03T18:32:33Z</dc:date>
    </item>
    <item>
      <title>Re: Automatic Power-On Behavior for i.MX8MP with overtemperature</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Automatic-Power-On-Behavior-for-i-MX8MP-with-overtemperature/m-p/2037566#M27367</link>
      <description>&lt;P&gt;I ended up setting a wake up alarm, and adding a service to set it up just before the shutdown. So each time the system would be triggered a power off etc. the alarm will be triggered. Better than nothing.&lt;/P&gt;&lt;TABLE border="1" width="100%"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="100%"&gt;&lt;P&gt;&lt;SPAN class=""&gt;echo +120 &amp;gt; /sys/class/rtc/rtc1/wakealarm&lt;/SPAN&gt;&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Feb 2025 07:56:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Automatic-Power-On-Behavior-for-i-MX8MP-with-overtemperature/m-p/2037566#M27367</guid>
      <dc:creator>Marco_Savo</dc:creator>
      <dc:date>2025-02-04T07:56:29Z</dc:date>
    </item>
  </channel>
</rss>