<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: NTP5332- HOW TO PROGRAM?</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/NTP5332-HOW-TO-PROGRAM/m-p/2029428#M27182</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In the I2C master mode it is said that the NTAG 5 needs to be powered by VCC. But I do not want to use a battery. I want to power the whole circuit using the power harvested from NFC. In that case, will I not be able to use the NTAG 5 to power the whole circuit via power harvesting as well as act as the I2C master at the same time?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a workaround?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 17 Jan 2025 02:54:19 GMT</pubDate>
    <dc:creator>samiha1234</dc:creator>
    <dc:date>2025-01-17T02:54:19Z</dc:date>
    <item>
      <title>NTP5332- HOW TO PROGRAM?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NTP5332-HOW-TO-PROGRAM/m-p/2028522#M27159</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am making a custom board with the&amp;nbsp;NTP5332 IC and the A7341 Color sensor IC which communicates via I2C.&lt;/P&gt;&lt;P&gt;As advertised in the NXP website, the&amp;nbsp;NTP5332 IC can receive sensor data via I2C without the need for a microcontroller. I am not considering using a microcontroller since I will be using power harvesting mode of NTP5332 and I don't know if it would be enough to power up a microcontroller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So my questions are:&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. How to configure the NTP5332 so that it knows the I2C address of my sensor?&lt;/P&gt;&lt;P&gt;2. And will the IC be able to transfer this data and show it in the NDEF format in a phone? How do I do that?&lt;/P&gt;&lt;P&gt;I have heard that there are android applications by NXP to control the NTAG 5 LINK, but will that work with a bare NTP5332 chip?&amp;nbsp;&lt;/P&gt;&lt;P&gt;It would be great if you could provide detailed answers since I am very new to this.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="NTAG5-LINK" id="NTAG5-LINK"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jan 2025 21:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NTP5332-HOW-TO-PROGRAM/m-p/2028522#M27159</guid>
      <dc:creator>samiha1234</dc:creator>
      <dc:date>2025-01-15T21:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: NTP5332- HOW TO PROGRAM?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NTP5332-HOW-TO-PROGRAM/m-p/2029414#M27181</link>
      <description>&lt;P&gt;FYI.&lt;A href="https://www.nxp.com/docs/en/application-note/AN12368.pdf" target="_blank"&gt;&amp;nbsp;NTAG 5 link - I2C master mode&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;and the RM00221 :&amp;nbsp;&lt;A href="https://www.nxp.com/search?keyword=rm00221&amp;amp;start=0" target="_blank"&gt;Search | NXP Semiconductors&lt;/A&gt;.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jan 2025 02:37:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NTP5332-HOW-TO-PROGRAM/m-p/2029414#M27181</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2025-01-17T02:37:55Z</dc:date>
    </item>
    <item>
      <title>Re: NTP5332- HOW TO PROGRAM?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NTP5332-HOW-TO-PROGRAM/m-p/2029428#M27182</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In the I2C master mode it is said that the NTAG 5 needs to be powered by VCC. But I do not want to use a battery. I want to power the whole circuit using the power harvested from NFC. In that case, will I not be able to use the NTAG 5 to power the whole circuit via power harvesting as well as act as the I2C master at the same time?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a workaround?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jan 2025 02:54:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NTP5332-HOW-TO-PROGRAM/m-p/2029428#M27182</guid>
      <dc:creator>samiha1234</dc:creator>
      <dc:date>2025-01-17T02:54:19Z</dc:date>
    </item>
    <item>
      <title>Re: NTP5332- HOW TO PROGRAM?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NTP5332-HOW-TO-PROGRAM/m-p/2031303#M27233</link>
      <description>&lt;P&gt;Do you see the example 5 in&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12368.pdf" target="_blank"&gt;NTAG 5 link - I2C master mode&lt;/A&gt;? Is it meet your requirement?&lt;/P&gt;
&lt;P&gt;And the Application Note NTAG 5 - How to use energy harvesting&amp;nbsp; is here.&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12365.pdf" target="_blank"&gt;NTAG 5 - How to use energy harvesting&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jan 2025 08:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NTP5332-HOW-TO-PROGRAM/m-p/2031303#M27233</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2025-01-21T08:46:52Z</dc:date>
    </item>
  </channel>
</rss>