<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Problem with the ROM Version (CME-555)</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-the-ROM-Version-CME-555/m-p/238736#M2711</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community!&lt;/P&gt;&lt;P&gt;I have a problem with my CME555 board and the codewarrior v8.7.&lt;/P&gt;&lt;P&gt;At the codewarrior Settings I can choose between the debug and the rom version. When I use the debug version everything is okay and I can the run my program. When I choose the ROM Version I get an error (see attachment) and I don’t know why? Because the error happens in the __start.c file and I use the same file for the debug and in the rom version. In the linker settings I choose for both Versions the same settings:&lt;/P&gt;&lt;P&gt;-__start&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; as entrypoint&lt;/P&gt;&lt;P&gt;-0x3f9800&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; as codeaddress(int. RAM)&lt;/P&gt;&lt;P&gt;-0xcf0000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; as stackaddress (ext. RAM)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I power up my board and run the rom version there is the described error. But when I power up the board and first run the debug version and after a SW-reset the rom version, both versions are okay. So it seems to me that in the rom version not everything is initialized.&lt;/P&gt;&lt;P&gt;Have you an Idea how to fix this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Jun 2013 13:05:41 GMT</pubDate>
    <dc:creator>Schobie</dc:creator>
    <dc:date>2013-06-25T13:05:41Z</dc:date>
    <item>
      <title>Problem with the ROM Version (CME-555)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-the-ROM-Version-CME-555/m-p/238736#M2711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community!&lt;/P&gt;&lt;P&gt;I have a problem with my CME555 board and the codewarrior v8.7.&lt;/P&gt;&lt;P&gt;At the codewarrior Settings I can choose between the debug and the rom version. When I use the debug version everything is okay and I can the run my program. When I choose the ROM Version I get an error (see attachment) and I don’t know why? Because the error happens in the __start.c file and I use the same file for the debug and in the rom version. In the linker settings I choose for both Versions the same settings:&lt;/P&gt;&lt;P&gt;-__start&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; as entrypoint&lt;/P&gt;&lt;P&gt;-0x3f9800&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; as codeaddress(int. RAM)&lt;/P&gt;&lt;P&gt;-0xcf0000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; as stackaddress (ext. RAM)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I power up my board and run the rom version there is the described error. But when I power up the board and first run the debug version and after a SW-reset the rom version, both versions are okay. So it seems to me that in the rom version not everything is initialized.&lt;/P&gt;&lt;P&gt;Have you an Idea how to fix this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jun 2013 13:05:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-the-ROM-Version-CME-555/m-p/238736#M2711</guid>
      <dc:creator>Schobie</dc:creator>
      <dc:date>2013-06-25T13:05:41Z</dc:date>
    </item>
  </channel>
</rss>