<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GD3160-Isolation failure in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/GD3160-Isolation-failure/m-p/2024480#M27050</link>
    <description>&lt;P&gt;I am using GD310 IC in one of the projects. The voltage on the LV side is 12V and the HV side is nearly 16 V.&lt;/P&gt;&lt;P&gt;What will be the impact if the isolation fails and is there any mechanism that can be implemented in traction inverter level to detect this ?&lt;/P&gt;</description>
    <pubDate>Thu, 09 Jan 2025 05:08:00 GMT</pubDate>
    <dc:creator>irbaz7</dc:creator>
    <dc:date>2025-01-09T05:08:00Z</dc:date>
    <item>
      <title>GD3160-Isolation failure</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/GD3160-Isolation-failure/m-p/2024480#M27050</link>
      <description>&lt;P&gt;I am using GD310 IC in one of the projects. The voltage on the LV side is 12V and the HV side is nearly 16 V.&lt;/P&gt;&lt;P&gt;What will be the impact if the isolation fails and is there any mechanism that can be implemented in traction inverter level to detect this ?&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 05:08:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/GD3160-Isolation-failure/m-p/2024480#M27050</guid>
      <dc:creator>irbaz7</dc:creator>
      <dc:date>2025-01-09T05:08:00Z</dc:date>
    </item>
    <item>
      <title>Re: GD3160-Isolation failure</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/GD3160-Isolation-failure/m-p/2024736#M27057</link>
      <description>&lt;P&gt;Hello Irbaz,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;In any typical system which is fully isolated between HV and LV domains, a single point failure of the GD isolation will not create a functional issue (apart from high noise coupling). But this isolation failure would be a breach of the safety concept for human electrocution prevention.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xavier_b_0-1736414374909.png" style="width: 368px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/318786iC3A1AB5D29DAC76D/image-dimensions/368x276?v=v2" width="368" height="276" role="button" title="xavier_b_0-1736414374909.png" alt="xavier_b_0-1736414374909.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;In practice, at GD level, most isolation failures will also result in other GD failures which will be detectable. However, as recommended in the safety manual, another means of ensuring the galvanic isolation integrity must be provided at system level. This is typically handled on the battery side, with dedicated leakage measurement circuitry, to ensure the maximum allowable leakage is not exceeded. (both polarities).&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BRs, Tomas&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 09:54:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/GD3160-Isolation-failure/m-p/2024736#M27057</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-01-09T09:54:08Z</dc:date>
    </item>
  </channel>
</rss>