<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 SC18IS606 datasheet incorrect about GPIO?</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IS606-datasheet-incorrect-about-GPIO/m-p/2024472#M27049</link>
    <description>&lt;P&gt;I am using GPIO functionality for GPIO0/SS0# and GPIO2/SS2#; I am using SS1# as a slave select. &lt;LI-PRODUCT title="SC18IS606" id="SC18IS606"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have attempted to write F7 11 to set GPIO0 and GPIO2 as push-pull (function F7: GPIO configuration).&amp;nbsp; However, this makes the SS1# stop working.&lt;/P&gt;&lt;P&gt;It looks like I have to write F7 15 to make SS1# still be push-pull; however this contradicts the datasheet which seems to indicate that F7 should only be used to configure GPIOs. "GPIO Configuration - Function ID F7h: The pins defined as GPIO may be configured by software to one of three types on a pin-by-pin basis."&lt;/P&gt;&lt;P&gt;Is this correct?&amp;nbsp; Do I need to explicitly set SS1# to push-pull using function F7?&lt;/P&gt;&lt;P&gt;My part's version string is "SC18IS606 1.0.2"&lt;/P&gt;</description>
    <pubDate>Thu, 09 Jan 2025 04:24:03 GMT</pubDate>
    <dc:creator>mlyle</dc:creator>
    <dc:date>2025-01-09T04:24:03Z</dc:date>
    <item>
      <title>SC18IS606 datasheet incorrect about GPIO?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IS606-datasheet-incorrect-about-GPIO/m-p/2024472#M27049</link>
      <description>&lt;P&gt;I am using GPIO functionality for GPIO0/SS0# and GPIO2/SS2#; I am using SS1# as a slave select. &lt;LI-PRODUCT title="SC18IS606" id="SC18IS606"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have attempted to write F7 11 to set GPIO0 and GPIO2 as push-pull (function F7: GPIO configuration).&amp;nbsp; However, this makes the SS1# stop working.&lt;/P&gt;&lt;P&gt;It looks like I have to write F7 15 to make SS1# still be push-pull; however this contradicts the datasheet which seems to indicate that F7 should only be used to configure GPIOs. "GPIO Configuration - Function ID F7h: The pins defined as GPIO may be configured by software to one of three types on a pin-by-pin basis."&lt;/P&gt;&lt;P&gt;Is this correct?&amp;nbsp; Do I need to explicitly set SS1# to push-pull using function F7?&lt;/P&gt;&lt;P&gt;My part's version string is "SC18IS606 1.0.2"&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 04:24:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC18IS606-datasheet-incorrect-about-GPIO/m-p/2024472#M27049</guid>
      <dc:creator>mlyle</dc:creator>
      <dc:date>2025-01-09T04:24:03Z</dc:date>
    </item>
    <item>
      <title>Re: SC18IS606 datasheet incorrect about GPIO?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IS606-datasheet-incorrect-about-GPIO/m-p/2024807#M27060</link>
      <description>&lt;P&gt;Dear Michael,&lt;/P&gt;
&lt;P&gt;another customer reported same issue. The solution was to set all the SSx pin to push-pull. Setting the 0xF7 register to 0x55. Please try the same.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;DESCRIPTION&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;SPAN&gt;thanks for the answer. This is now working with command 0xF7 following 0x55. I have to send 0x55 to set ALL pins (GPIO) to push-pull.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1736421511893.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/318806i55D2E0FA33C146E2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1736421511893.png" alt="JozefKozon_0-1736421511893.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 11:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC18IS606-datasheet-incorrect-about-GPIO/m-p/2024807#M27060</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2025-01-09T11:19:09Z</dc:date>
    </item>
  </channel>
</rss>