<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: io in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2011659#M26752</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244031"&gt;@syedhashmiraza&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If your&amp;nbsp;USART RX pin is&amp;nbsp;PIO0_29.&lt;/P&gt;
&lt;P&gt;You can refer to the LPC55S1x/LPC551x&amp;nbsp;Product data sheet.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1733899348345.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/315275i7321A2F789C8C8DF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1733899348345.png" alt="Harry_Zhang_0-1733899348345.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Harry_Zhang_0-1733899348345.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You can change function of&amp;nbsp;PIO0_29 to 0 function.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
    <pubDate>Wed, 11 Dec 2024 06:43:49 GMT</pubDate>
    <dc:creator>Harry_Zhang</dc:creator>
    <dc:date>2024-12-11T06:43:49Z</dc:date>
    <item>
      <title>io</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2011565#M26748</link>
      <description>&lt;P&gt;hello iam using lpc55s16&amp;nbsp;"How can I use the USART RX pin as an IO pin?"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Dec 2024 05:07:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2011565#M26748</guid>
      <dc:creator>syedhashmiraza</dc:creator>
      <dc:date>2024-12-11T05:07:44Z</dc:date>
    </item>
    <item>
      <title>Re: io</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2011659#M26752</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244031"&gt;@syedhashmiraza&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If your&amp;nbsp;USART RX pin is&amp;nbsp;PIO0_29.&lt;/P&gt;
&lt;P&gt;You can refer to the LPC55S1x/LPC551x&amp;nbsp;Product data sheet.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1733899348345.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/315275i7321A2F789C8C8DF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1733899348345.png" alt="Harry_Zhang_0-1733899348345.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Harry_Zhang_0-1733899348345.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You can change function of&amp;nbsp;PIO0_29 to 0 function.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Wed, 11 Dec 2024 06:43:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2011659#M26752</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-12-11T06:43:49Z</dc:date>
    </item>
    <item>
      <title>Re: io</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2011788#M26753</link>
      <description>&lt;P&gt;how can i use this pin as io pin&lt;/P&gt;</description>
      <pubDate>Wed, 11 Dec 2024 08:35:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2011788#M26753</guid>
      <dc:creator>syedhashmiraza</dc:creator>
      <dc:date>2024-12-11T08:35:25Z</dc:date>
    </item>
    <item>
      <title>Re: io</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2012566#M26769</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244031"&gt;@syedhashmiraza&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As I mentioned in my previous post, you need to&amp;nbsp;change function of PIO0_29 to 0 function.&lt;/P&gt;
&lt;P&gt;0 function is the IO function.&lt;/P&gt;
&lt;P&gt;You can import the USRAT example form LPC55s16 SDK.&lt;/P&gt;
&lt;P&gt;In pin_mux.c, you can change the code&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1733983859555.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/315538i80279D849C2A8DD7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1733983859555.png" alt="Harry_Zhang_0-1733983859555.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Harry_Zhang_0-1733983859555.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Thu, 12 Dec 2024 06:11:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2012566#M26769</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-12-12T06:11:12Z</dc:date>
    </item>
    <item>
      <title>Re: io</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2012589#M26770</link>
      <description>&lt;P&gt;iam asking you ISO7816 IO pin how i can&amp;nbsp; use in this ? i know lpc55s16 is not support iso7816 but in this how i can use io pin ?&lt;/P&gt;</description>
      <pubDate>Thu, 12 Dec 2024 06:48:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2012589#M26770</guid>
      <dc:creator>syedhashmiraza</dc:creator>
      <dc:date>2024-12-12T06:48:48Z</dc:date>
    </item>
    <item>
      <title>Re: io</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2014346#M26807</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244031"&gt;@syedhashmiraza&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The LPC55S16 does not natively support ISO/IEC 7816 as it lacks a dedicated hardware module for this protocol. But&amp;nbsp;&lt;SPAN data-teams="true"&gt;you can implement ISO7816 functionality using general-purpose IO pins and peripherals like UART with additional software logic to comply with the protocol’s requirements.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;I checked and it requires the following steps.&lt;/P&gt;
&lt;P&gt;1. IO Pin Setup:&lt;BR /&gt;• Assign a GPIO or UART TX/RX pin for the IO line.&lt;BR /&gt;• Control direction using software logic.&lt;BR /&gt;2. UART Configuration:&lt;BR /&gt;• Set up UART for 8 data bits, even parity, and 1 stop bit (8E1).&lt;BR /&gt;• Configure the baud rate to match the required ETU.&lt;BR /&gt;3. GPIO for RST and CLK:&lt;BR /&gt;• Use GPIO pins to toggle the reset and clock lines as per the smart card’s ATR (Answer to Reset) process.&lt;BR /&gt;4. Transmit/Receive Logic:&lt;BR /&gt;• Implement logic to send and receive data frames, ensuring the proper protocol format (start bit, data bits, parity, stop bit).&lt;BR /&gt;5. Clock and Timing Management:&lt;BR /&gt;• Use a timer peripheral to generate accurate delays and ensure timing compliance with ISO7816.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Mon, 16 Dec 2024 09:26:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/io/m-p/2014346#M26807</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-12-16T09:26:25Z</dc:date>
    </item>
  </channel>
</rss>