<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: TJA1043 - Normal Mode - Using for only Bus Diagnostic</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1043-Normal-Mode-Using-for-only-Bus-Diagnostic/m-p/2008087#M26686</link>
    <description>&lt;P&gt;Hello Sam,&lt;/P&gt;
&lt;P&gt;You are correct that the TJA1043’s bus failure diagnostic is only active in Normal mode (STB_N = EN = 1). The ERRN pin will be pulled low when a bus error is detected. Keep in mind the current rating of the ERR_N pin as shown in table 8 of the datasheet. For more information, please refer to the &lt;A href="https://www.nxp.com/docs/en/supporting-information/AH1014.pdf" target="_self"&gt;AH1014&lt;/A&gt;, chapter 6.6 - Bus failure diagnosis.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 05 Dec 2024 10:11:46 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2024-12-05T10:11:46Z</dc:date>
    <item>
      <title>TJA1043 - Normal Mode - Using for only Bus Diagnostic</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1043-Normal-Mode-Using-for-only-Bus-Diagnostic/m-p/2007922#M26680</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I want to detect if there is a problem in CAN Bus. At first, I thought that I can do it in listen only mode. As I understand from datasheet, bus diagnostic functions are only active when in normal mode. If so, what should I do to TXD pin? Should I connect it to ground or something else? Can I use TJA 1043 to only detect bus failures? I will not use a microcontroller. I want to show if there is an error with led with using ERRN pin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Dec 2024 08:10:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1043-Normal-Mode-Using-for-only-Bus-Diagnostic/m-p/2007922#M26680</guid>
      <dc:creator>samfisher</dc:creator>
      <dc:date>2024-12-05T08:10:37Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1043 - Normal Mode - Using for only Bus Diagnostic</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1043-Normal-Mode-Using-for-only-Bus-Diagnostic/m-p/2008087#M26686</link>
      <description>&lt;P&gt;Hello Sam,&lt;/P&gt;
&lt;P&gt;You are correct that the TJA1043’s bus failure diagnostic is only active in Normal mode (STB_N = EN = 1). The ERRN pin will be pulled low when a bus error is detected. Keep in mind the current rating of the ERR_N pin as shown in table 8 of the datasheet. For more information, please refer to the &lt;A href="https://www.nxp.com/docs/en/supporting-information/AH1014.pdf" target="_self"&gt;AH1014&lt;/A&gt;, chapter 6.6 - Bus failure diagnosis.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Dec 2024 10:11:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1043-Normal-Mode-Using-for-only-Bus-Diagnostic/m-p/2008087#M26686</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-12-05T10:11:46Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1043 - Normal Mode - Using for only Bus Diagnostic</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1043-Normal-Mode-Using-for-only-Bus-Diagnostic/m-p/2010704#M26728</link>
      <description>&lt;P&gt;Thank you for the reply, Thomas,&lt;/P&gt;&lt;P&gt;I will keep in mind about current rating. What about the TXD pin? Should it be connected to GND or 5V or something else to not to interfere the bus?&lt;/P&gt;&lt;P&gt;Sam&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 05:30:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1043-Normal-Mode-Using-for-only-Bus-Diagnostic/m-p/2010704#M26728</guid>
      <dc:creator>samfisher</dc:creator>
      <dc:date>2024-12-10T05:30:40Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1043 - Normal Mode - Using for only Bus Diagnostic</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1043-Normal-Mode-Using-for-only-Bus-Diagnostic/m-p/2010817#M26732</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello Sam,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I think the TXD pin can be left unconnected as it is internally pulled up to VIO.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BRs, Tomas&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 08:01:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1043-Normal-Mode-Using-for-only-Bus-Diagnostic/m-p/2010817#M26732</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-12-10T08:01:05Z</dc:date>
    </item>
  </channel>
</rss>