<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックWrite error issue -MC13224</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Write-error-issue-MC13224/m-p/223043#M2641</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using free-scale controller MC12334&amp;nbsp; in our application, initially few baords&amp;nbsp; we manually assembled and tested . it was working fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But as a first of mass production we assembled 200 board&amp;nbsp; we used Pick plcae .but after the assembly majority of boards are failing to program the controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we trying JTAG&amp;nbsp; it showing "Write error" when we contacted with assebly house they says they have prepacked with 120 degree for 7 hours(Controller and Bare PCB).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reflow temperature profile&amp;nbsp; also same as recommended by freeescale.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please answer few my doubts&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Write error meaning controller internal flash corrupted or it can be JTAG contact issue with JTAG connector?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Prebaking 7 hours at 120 degree is recommended?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;chandra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Feb 2014 06:13:23 GMT</pubDate>
    <dc:creator>chandrashekarp</dc:creator>
    <dc:date>2014-02-11T06:13:23Z</dc:date>
    <item>
      <title>Write error issue -MC13224</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Write-error-issue-MC13224/m-p/223043#M2641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using free-scale controller MC12334&amp;nbsp; in our application, initially few baords&amp;nbsp; we manually assembled and tested . it was working fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But as a first of mass production we assembled 200 board&amp;nbsp; we used Pick plcae .but after the assembly majority of boards are failing to program the controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we trying JTAG&amp;nbsp; it showing "Write error" when we contacted with assebly house they says they have prepacked with 120 degree for 7 hours(Controller and Bare PCB).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reflow temperature profile&amp;nbsp; also same as recommended by freeescale.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please answer few my doubts&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Write error meaning controller internal flash corrupted or it can be JTAG contact issue with JTAG connector?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Prebaking 7 hours at 120 degree is recommended?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;chandra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2014 06:13:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Write-error-issue-MC13224/m-p/223043#M2641</guid>
      <dc:creator>chandrashekarp</dc:creator>
      <dc:date>2014-02-11T06:13:23Z</dc:date>
    </item>
  </channel>
</rss>