<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: iMX8M plus BOOT priority / order</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/iMX8M-plus-BOOT-priority-order/m-p/1992971#M26365</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It is possible to do it using manufacturing mode, please take a look in reference manual.&lt;/P&gt;
&lt;P&gt;Manufacture mode is intended to allow a system to boot from a SD/MMC card on a board with unprogrammed boot media or to upgrade the image on a boot device. For manufacture mode, the boot ROM assumes if there is a SD/MMC card present indicated by the uSDHC card detect (CD) signal pulled low, then there is a valid image on the card.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Tue, 12 Nov 2024 17:06:19 GMT</pubDate>
    <dc:creator>JorgeCas</dc:creator>
    <dc:date>2024-11-12T17:06:19Z</dc:date>
    <item>
      <title>iMX8M plus BOOT priority / order</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX8M-plus-BOOT-priority-order/m-p/1992714#M26358</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In my application I would like to boot from uSD in the initial production phase, and then boot from eMMC. I would like to avoid burning eFuses, because in certain situations it is required to go back to uSD boot.&lt;/P&gt;&lt;P&gt;The iMX6 has a BOOT priority / order feature, which allows booting from eMMC, but if there is no UBoot in eMMC, then the iMX6 falls back to boot from uSD - without any hardware intervention on the BOOT or BOOT CFG pins.&lt;/P&gt;&lt;P&gt;Does this feature exist in the iMX8M Plus? If so, please direct me to more information.&lt;/P&gt;&lt;P&gt;If the above feature does not exist, what solution do you recommend?&lt;/P&gt;&lt;P&gt;Should the HW tie the BOOT pins for uSD? If so, how would the CPU fall back to uSD when the eMMC does not contain the UBoot?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Tue, 12 Nov 2024 09:16:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX8M-plus-BOOT-priority-order/m-p/1992714#M26358</guid>
      <dc:creator>Username_AH</dc:creator>
      <dc:date>2024-11-12T09:16:14Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M plus BOOT priority / order</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX8M-plus-BOOT-priority-order/m-p/1992971#M26365</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It is possible to do it using manufacturing mode, please take a look in reference manual.&lt;/P&gt;
&lt;P&gt;Manufacture mode is intended to allow a system to boot from a SD/MMC card on a board with unprogrammed boot media or to upgrade the image on a boot device. For manufacture mode, the boot ROM assumes if there is a SD/MMC card present indicated by the uSDHC card detect (CD) signal pulled low, then there is a valid image on the card.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Nov 2024 17:06:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX8M-plus-BOOT-priority-order/m-p/1992971#M26365</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2024-11-12T17:06:19Z</dc:date>
    </item>
  </channel>
</rss>