<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SJA1110 SPI_AP interface in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988670#M26260</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Thank you very much, I am now clearly understand the SPI_AP and boot process.&lt;/P&gt;&lt;P&gt;At last, I am not sure about the SWITCH_CONTROL_INTERNAL and SWITH_CONTROL_SPI mode in SDK,&amp;nbsp; do I need to config it to&amp;nbsp;SWITH_CONTROL_SPI if I want to work on SPI_AP access, I see it set to&amp;nbsp;SWITCH_CONTROL_INTERNAL as default in SDK.&lt;/P&gt;</description>
    <pubDate>Wed, 06 Nov 2024 08:53:26 GMT</pubDate>
    <dc:creator>yangjinzhuang</dc:creator>
    <dc:date>2024-11-06T08:53:26Z</dc:date>
    <item>
      <title>SJA1110 SPI_AP interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1987814#M26234</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I see that SJA1110 supports SPI_HOST and SPI_AP access point in the UM11107 software UM for SJA1110.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;My hardware is GLDBOX, it's design is S32G274A---SPI---SJA1110&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I am not sure if I want to use SPI_AP interface, first I select the&amp;nbsp;Pins SPI_HAP_SSx_N to&amp;nbsp;SPI_HAP_SS0; second if I should connect the external controller's SPI_PER to sja1110's SPI_HAP?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;If I use SPI_AP, does SJA1110 can't boot and download image itself? so the external controller must be another SJA1110 and can't be S32J274A, even they have SPI connect? Is my understand right?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Thank you very much!&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Nov 2024 08:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1987814#M26234</guid>
      <dc:creator>yangjinzhuang</dc:creator>
      <dc:date>2024-11-05T08:38:24Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1110 SPI_AP interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1987978#M26242</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210110"&gt;@yangjinzhuang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;SJA1110 supports NVM boot from external SPI flash or SDL boot from the host controller,&amp;nbsp; independently to usage of SPI_AP. Set DIP switch on your board accordingly to AN13185 chapter 3.2.1. You may also refer to&amp;nbsp;UM11107 Software user manual for SJA1110 for more details. Both documents require Sign in.&lt;/P&gt;
&lt;P&gt;You need to use&amp;nbsp;SPI_HAP_SS0_N to access all internal registers/settings by SPI_AP.&lt;/P&gt;
&lt;P&gt;SJA1110's SPI_PER is mostly used for cascading two SJA1110s.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Tue, 05 Nov 2024 13:34:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1987978#M26242</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2024-11-05T13:34:19Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1110 SPI_AP interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988357#M26249</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Thanks for your reply, from um549820-UM11107 software UM, I got that SPI_HOST and SPI_AP are multiplexed, because SPI_HOST&amp;nbsp;is used to control the processor boot, then if I set SPI_AP and switch is controlled by external microcontroller, so I understand that SPI_AP has&lt;SPAN&gt;&amp;nbsp;an impact on boot step, maybe my understand is not right, so I need your help to confirm.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;1、I see my hardware, the dip switch&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;SW12[1] is on and SW12[2] is off in default, it's boot mode is NVM boot and boot from SPI flash. If I use SPI_AP, then the boot mode as default can also boot success, it will not boot fail because of not SPI_HOST?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;2、About SPI_AP, I can get form UM111107 that two SJA1110, one SJA1110 is controlled by another SJA1110, but I am not sure that: can I use S32G274A&amp;nbsp;as an external microcontroller to control SJA1110 through SPI_AP？In this case NVM boot can still boot success from SPI flash？&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 01:57:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988357#M26249</guid>
      <dc:creator>yangjinzhuang</dc:creator>
      <dc:date>2024-11-06T01:57:57Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1110 SPI_AP interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988379#M26250</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I still has some question about the SPI_AP:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;1、Does external microcontroller not must be another SJA1110, S32G274A has SPI access also can be the external microcontroller?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; 2、On SPI_AP, boot step also load image from SPI flash, run over the init and static config process, etc.&amp;nbsp; as same as the SPI_HOST mode, then what will the external microcontroller do about the ethernet switch?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;3、In my understand that the boot and load image will controlled by external microcontroller, SJA1110 only provides ethernet switch to external microcontroller as hardwares&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 02:16:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988379#M26250</guid>
      <dc:creator>yangjinzhuang</dc:creator>
      <dc:date>2024-11-06T02:16:38Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1110 SPI_AP interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988639#M26258</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210110"&gt;@yangjinzhuang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;ad 1. External controller can be anyone. I use my laptop &amp;amp; FTDI driver to access my SJA1110 EVM board.&lt;/P&gt;
&lt;P&gt;ad 2. Once you load image from SPI FLASH, the external microcontroller is not necessary at all. SJA1110 can work fully autonomously. External microcontroller could monitor traffic, diagnostic registers, ...&amp;nbsp;&lt;/P&gt;
&lt;P&gt;ad 3. SDL boot is also supported option.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 08:33:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988639#M26258</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2024-11-06T08:33:15Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1110 SPI_AP interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988651#M26259</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210110"&gt;@yangjinzhuang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Usage of SPI_AP does NOT affect boot from SPI FLASH.&lt;/P&gt;
&lt;P&gt;ad 1. After reset, the SJA110 reads pin strapping options and boots from SPI FLASH. Then you can access SPI_AP at your will - reading registers, dynamically changing configuration, ...&lt;/P&gt;
&lt;P&gt;ad 2. You can use&amp;nbsp;&lt;SPAN&gt;32G274A&amp;nbsp;as an external microcontroller to control SJA1110 through SPI_AP. Yes, the NVM boot will still succeeded.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 08:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988651#M26259</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2024-11-06T08:39:47Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1110 SPI_AP interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988670#M26260</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Thank you very much, I am now clearly understand the SPI_AP and boot process.&lt;/P&gt;&lt;P&gt;At last, I am not sure about the SWITCH_CONTROL_INTERNAL and SWITH_CONTROL_SPI mode in SDK,&amp;nbsp; do I need to config it to&amp;nbsp;SWITH_CONTROL_SPI if I want to work on SPI_AP access, I see it set to&amp;nbsp;SWITCH_CONTROL_INTERNAL as default in SDK.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 08:53:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988670#M26260</guid>
      <dc:creator>yangjinzhuang</dc:creator>
      <dc:date>2024-11-06T08:53:26Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1110 SPI_AP interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988711#M26261</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210110"&gt;@yangjinzhuang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;you need to say to SDK, how the switchcore can be accessed.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PavelL_0-1730884199563.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/308891i47A550E653846724/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PavelL_0-1730884199563.png" alt="PavelL_0-1730884199563.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Then internal routines (like SWITCH_DRV_Read) take care of that automatically.&lt;/P&gt;
&lt;P&gt;If you are developing firmware for SJA1110's internal M7,&amp;nbsp;&lt;SPAN&gt;SWITCH_CONTROL_INTERNAL shall be set.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you are developing firmware for SJA1110's internal M7 to access external switchcore (cascaded SJA1110),&amp;nbsp;SWITH_CONTROL_SPI&amp;nbsp;shall be used:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PavelL_1-1730884833620.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/308899i36CC577DF236A728/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PavelL_1-1730884833620.png" alt="PavelL_1-1730884833620.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I guess it will be about the same if you are developing firmware for S32G to control SJA1110 over SPI. I need to double check it. You have created another thread on that, so I will answer there. Thank you for your patience.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 09:22:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1988711#M26261</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2024-11-06T09:22:32Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1110 SPI_AP interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1989589#M26279</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Thank you for your reply, yes, I have asked in another topic "SJA1110 SDK for the hardware GLDBOX". Maybe we can discuss there.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Nov 2024 01:11:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1110-SPI-AP-interface/m-p/1989589#M26279</guid>
      <dc:creator>yangjinzhuang</dc:creator>
      <dc:date>2024-11-07T01:11:13Z</dc:date>
    </item>
  </channel>
</rss>