<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCF2131 losing seconds. in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1988617#M26257</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The PCF2131 should operate reliably down to a specified minimum voltage, typically 1.2V. If the voltage drops below this, the oscillator supply also fails and a reset occurs. See section 7.6 of the datasheet for more information.&lt;/P&gt;
&lt;P&gt;At 2.8V, the supercap should indeed be sufficient for the PCF2131.&lt;/P&gt;
&lt;P&gt;Voltage transients on the supercap when switching from main power could potentially impact the oscillator. Consider placing a small decoupling capacitor close to the RTC’s VDD pin to help smooth any voltage fluctuations from the supercap during switchover.&lt;/P&gt;
&lt;P&gt;Is the PCF2131 exposed&amp;nbsp;to large temperature variations? Is the TC_DIS bit = 0?&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
    <pubDate>Wed, 06 Nov 2024 08:17:26 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2024-11-06T08:17:26Z</dc:date>
    <item>
      <title>PCF2131 losing seconds.</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1987936#M26239</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a custom PCB board with a PCF2131 RTC.&lt;/P&gt;&lt;P&gt;it is supplied by a main power of 3.3V and a supercap of 12F when main power supplies cut off.&lt;/P&gt;&lt;P&gt;I have disabled the WD and tried multiple Aging Offset but it keeps losing up to -10 seconds in a week or so.&lt;/P&gt;&lt;P&gt;Right now the supercap is running at around 2.8V, which should be enough.&lt;/P&gt;&lt;P&gt;Out of curiosity: Does RTC drift time, or reset time, when voltage drops below 1.8 for few milliseconds?&lt;/P&gt;&lt;P&gt;Don't really understand what could cause this.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Nov 2024 11:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1987936#M26239</guid>
      <dc:creator>PepeTheSkrilla</dc:creator>
      <dc:date>2024-11-05T11:41:18Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2131 losing seconds.</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1988617#M26257</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The PCF2131 should operate reliably down to a specified minimum voltage, typically 1.2V. If the voltage drops below this, the oscillator supply also fails and a reset occurs. See section 7.6 of the datasheet for more information.&lt;/P&gt;
&lt;P&gt;At 2.8V, the supercap should indeed be sufficient for the PCF2131.&lt;/P&gt;
&lt;P&gt;Voltage transients on the supercap when switching from main power could potentially impact the oscillator. Consider placing a small decoupling capacitor close to the RTC’s VDD pin to help smooth any voltage fluctuations from the supercap during switchover.&lt;/P&gt;
&lt;P&gt;Is the PCF2131 exposed&amp;nbsp;to large temperature variations? Is the TC_DIS bit = 0?&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 08:17:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1988617#M26257</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-11-06T08:17:26Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2131 losing seconds.</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1988845#M26268</link>
      <description>&lt;P&gt;Hi Tomas, Thanks for the answer.&lt;/P&gt;&lt;P&gt;i will check for TC_DIS, but I think it will be 1.&lt;/P&gt;&lt;P&gt;if TS1, TS2, TS3 and TS4 are connected to 3V3 in series with a 4KOhm Resistor, can it cause any sort of problem of drifting?&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 11:57:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1988845#M26268</guid>
      <dc:creator>PepeTheSkrilla</dc:creator>
      <dc:date>2024-11-06T11:57:40Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2131 losing seconds.</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1988954#M26273</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Connecting the&amp;nbsp; timestamp inputs to 3.3V with pull-up resistors should not affect the RTC timekeeping accuracy.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 15:13:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1988954#M26273</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-11-06T15:13:09Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2131 losing seconds.</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1990235#M26290</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We connected the oscilloscope to the CLKOUT pin and we retrieved this guassian distribution of the frequency of the oscillator (around 90hz) at ambient temperature. (See image)&lt;/P&gt;&lt;P&gt;Could be this the cause of the drift?&lt;/P&gt;</description>
      <pubDate>Thu, 07 Nov 2024 13:49:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1990235#M26290</guid>
      <dc:creator>PepeTheSkrilla</dc:creator>
      <dc:date>2024-11-07T13:49:47Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2131 losing seconds.</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1991810#M26333</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This is likely&amp;nbsp;a primary contributor to your time drift issue. I see you created a support case, so please follow up on this internally with my colleague.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 11 Nov 2024 08:19:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2131-losing-seconds/m-p/1991810#M26333</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-11-11T08:19:54Z</dc:date>
    </item>
  </channel>
</rss>