<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCF85263 RTC I2C Communication Issue - All Registers Returning 0x00 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCF85263-RTC-I2C-Communication-Issue-All-Registers-Returning/m-p/1983666#M26117</link>
    <description>Thank you, forgot to answer... Got a logic analyzer and looking at the addresses I found out that I had to use the 0x51 address as is. Our other sensors required the R/W bit included in the address so I thought this one also needed.</description>
    <pubDate>Tue, 29 Oct 2024 09:08:35 GMT</pubDate>
    <dc:creator>ohck</dc:creator>
    <dc:date>2024-10-29T09:08:35Z</dc:date>
    <item>
      <title>PCF85263 RTC I2C Communication Issue - All Registers Returning 0x00</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF85263-RTC-I2C-Communication-Issue-All-Registers-Returning/m-p/1978175#M25993</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm configuring the PCF85263 RTC and encountering an issue where all registers return 0x00 when I attempt to read them via I2C. Here’s my setup and the steps I’ve followed:&lt;/P&gt;&lt;P&gt;HW setup:&lt;/P&gt;&lt;P&gt;- PCF85263 rtc connected to a Quectel BG95-m3 module.&lt;/P&gt;&lt;P&gt;- pull-up resistors are present&lt;/P&gt;&lt;P&gt;Issue:&lt;/P&gt;&lt;P&gt;- I have tried to write different commands to different registers but when verifying the registers state they all return as 0x00&lt;/P&gt;&lt;P&gt;Steps I have taken:&lt;/P&gt;&lt;P&gt;- I have confirmed that the rtc gets 1.8v on VDD, SDA and SCL using a multimeter.&lt;/P&gt;&lt;P&gt;- Tested on two separate devices.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My code is in the attached file(set_alarm function gets called).&lt;/P&gt;&lt;P&gt;Is there some step I'm missing in the configuration?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Mon, 21 Oct 2024 10:49:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF85263-RTC-I2C-Communication-Issue-All-Registers-Returning/m-p/1978175#M25993</guid>
      <dc:creator>ohck</dc:creator>
      <dc:date>2024-10-21T10:49:46Z</dc:date>
    </item>
    <item>
      <title>Re: PCF85263 RTC I2C Communication Issue - All Registers Returning 0x00</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF85263-RTC-I2C-Communication-Issue-All-Registers-Returning/m-p/1978313#M26000</link>
      <description>&lt;P&gt;Hi Oscar,&lt;/P&gt;
&lt;P&gt;If you have a logic analyzer or an oscilloscope, could you please share some screenshots to check what is going on the bus?&lt;/P&gt;
&lt;P&gt;It should also help us to verify each I2C operation's acknowledgment. If a command is not acknowledged, subsequent operations could fail.&lt;/P&gt;
&lt;P&gt;Looking at your code,&amp;nbsp;the I2C device address being used is correct. Just verify&amp;nbsp;if the I2C library expects this 7-bit address (0x51) and automatically handles the read/write bit.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Oct 2024 14:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF85263-RTC-I2C-Communication-Issue-All-Registers-Returning/m-p/1978313#M26000</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-10-21T14:13:14Z</dc:date>
    </item>
    <item>
      <title>Re: PCF85263 RTC I2C Communication Issue - All Registers Returning 0x00</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF85263-RTC-I2C-Communication-Issue-All-Registers-Returning/m-p/1983666#M26117</link>
      <description>Thank you, forgot to answer... Got a logic analyzer and looking at the addresses I found out that I had to use the 0x51 address as is. Our other sensors required the R/W bit included in the address so I thought this one also needed.</description>
      <pubDate>Tue, 29 Oct 2024 09:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF85263-RTC-I2C-Communication-Issue-All-Registers-Returning/m-p/1983666#M26117</guid>
      <dc:creator>ohck</dc:creator>
      <dc:date>2024-10-29T09:08:35Z</dc:date>
    </item>
  </channel>
</rss>