<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: iMX-31 Camera interface</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/iMX-31-Camera-interface/m-p/217802#M2605</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Camera should be connected to J10 only, not J13.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I never saw the rotating issue to happen on the MX31ADS.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;In your log message that are several I2C transfer error. Maybe it is because your kernel is configured for a certain camera module and you are using other.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;By default, rel6 selects OV2640 driver. Please make sure you are using this model or change it in the kernel config.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Fabio Estevam&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Feb 2009 23:16:46 GMT</pubDate>
    <dc:creator>fabio_estevam</dc:creator>
    <dc:date>2009-02-10T23:16:46Z</dc:date>
    <item>
      <title>iMX-31 Camera interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX-31-Camera-interface/m-p/217800#M2603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;We have connected the camera which came along with the board to both J10 and J13 for testing purpose.&lt;BR /&gt;We followed the document IPU.htm provided in help/software/device_drivers/ipu directory in the imx31_ads_20080722-rel6-ltib.iso image.&lt;BR /&gt;We configured the kernel accordingly and tried to execute some test applications&amp;nbsp;from root file system.&lt;BR /&gt;It happened to see that there is rotating device present on the daughter board MC13783 (ATLAS BOARD).&lt;BR /&gt;It starts rotating when the test application is executed, which makes the entire board vibrate. Will this create any damage to the board ?&lt;BR /&gt;The test application is crashing after list of errors which we have logged to the file Error.log and attached to this mail.&lt;BR /&gt;FYI, All the test application related to camera produces the same output.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Prem&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jan 2009 20:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX-31-Camera-interface/m-p/217800#M2603</guid>
      <dc:creator>kpremendra</dc:creator>
      <dc:date>2009-01-21T20:00:11Z</dc:date>
    </item>
    <item>
      <title>Re: iMX-31 Camera interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX-31-Camera-interface/m-p/217801#M2604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The vibrator included in the Atlas board in ADS can be activated by using SPI. This seems a little bit odd to me since IPU and SPI are not related at all.&lt;BR /&gt;&lt;BR /&gt;Having the vibrator active while running an application will cause no harm, however; this should not be happening. I would recommend to recheck the configuration you are using in your OS to ensure you are only configuring the required information for the camera.&lt;BR /&gt;&lt;BR /&gt;I wish I could provide more insight on the Linux side, however; I am just HW &lt;SPAN&gt;&lt;IMG alt=":smileytongue:" class="emoticon emoticon-smileytongue" id="smileytongue" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-tongue.gif" title="Smiley Tongue" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2009 04:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX-31-Camera-interface/m-p/217801#M2604</guid>
      <dc:creator>JorgeRivera</dc:creator>
      <dc:date>2009-02-03T04:27:10Z</dc:date>
    </item>
    <item>
      <title>Re: iMX-31 Camera interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX-31-Camera-interface/m-p/217802#M2605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Camera should be connected to J10 only, not J13.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I never saw the rotating issue to happen on the MX31ADS.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;In your log message that are several I2C transfer error. Maybe it is because your kernel is configured for a certain camera module and you are using other.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;By default, rel6 selects OV2640 driver. Please make sure you are using this model or change it in the kernel config.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Fabio Estevam&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Feb 2009 23:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX-31-Camera-interface/m-p/217802#M2605</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2009-02-10T23:16:46Z</dc:date>
    </item>
    <item>
      <title>Re: iMX-31 Camera interface</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX-31-Camera-interface/m-p/217803#M2606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi prem,&lt;/P&gt;&lt;P&gt;1. &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; To stop the vibrator remove the jumper 2 (JMP2) in ASSY 700-20540 board&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; To test the camera ov2640 in imx31 ads board, make sure that the configuration of gpio levels (reset and power down are done properly).&lt;/P&gt;&lt;P&gt;(MX31_PIN_GPIO3_1 -LOW, MX31_PIN_GPIO3_0 -LOW).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;&lt;P&gt;Ananthapadmanaban&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2009 13:44:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX-31-Camera-interface/m-p/217803#M2606</guid>
      <dc:creator>Ananth</dc:creator>
      <dc:date>2009-04-14T13:44:49Z</dc:date>
    </item>
  </channel>
</rss>