<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Dual boot setup in imx8mplus in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Dual-boot-setup-in-imx8mplus/m-p/1964964#M25772</link>
    <description>&lt;P&gt;Hi Bio_TICFSL,&lt;/P&gt;&lt;P&gt;What I'm looking for is emmc of the board should have 2 images and the board should be able to boot from both images. I'm also looking it as solution for adding image upgrade feature.&amp;nbsp;Jailhouse is generally used for running isolated applications or OS instances, not directly for performing image upgrades.&lt;/P&gt;</description>
    <pubDate>Tue, 01 Oct 2024 06:20:34 GMT</pubDate>
    <dc:creator>sanum19</dc:creator>
    <dc:date>2024-10-01T06:20:34Z</dc:date>
    <item>
      <title>Dual boot setup in imx8mplus</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Dual-boot-setup-in-imx8mplus/m-p/1964264#M25736</link>
      <description>&lt;P&gt;After successfully building and flashing the image into the &lt;EM&gt;&lt;STRONG&gt;imx8mplus&lt;/STRONG&gt;&lt;/EM&gt; board. 2partitions are formed boot &amp;amp; root.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Boot= contains devicetree, kernel(Image)&lt;/P&gt;&lt;P&gt;Root= root file system&lt;/P&gt;&lt;P&gt;1.I would like to know how u-boot binary is integrated into the image?&lt;/P&gt;&lt;P&gt;My motive is to maually setup a dualcopy image in imx8mplus. ie The board will be having 2 boot partition and 2 root partitions (for booting 2 respective images ).&lt;/P&gt;&lt;P&gt;mmcblk p1,p2(imageA)&amp;nbsp; ,p3,p4(imageB)&lt;/P&gt;&lt;P&gt;I have updated bootargs and other paths from u-boot shell to choose the current image to load.&amp;nbsp;When i boot the board a bashshell is coming up instead of loading proper rootfs.&lt;/P&gt;&lt;P&gt;2.So can anyone helpme out with how to correctly do the partition to make dual copy image booting.&lt;/P&gt;</description>
      <pubDate>Mon, 30 Sep 2024 07:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Dual-boot-setup-in-imx8mplus/m-p/1964264#M25736</guid>
      <dc:creator>sanum19</dc:creator>
      <dc:date>2024-09-30T07:31:00Z</dc:date>
    </item>
    <item>
      <title>Re: Dual boot setup in imx8mplus</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Dual-boot-setup-in-imx8mplus/m-p/1964518#M25767</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Uboot need to boot 1st device and the other device boot the second device, you may need read the jailhouse mode:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/IMX-8M-Quad-Eval-board-Jailhouse-Demo-instructions/td-p/1530559" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/IMX-8M-Quad-Eval-board-Jailhouse-Demo-instructions/td-p/1530559&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://variwiki.com/index.php?title=Jailhouse_Guide" target="_blank"&gt;https://variwiki.com/index.php?title=Jailhouse_Guide&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 30 Sep 2024 14:02:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Dual-boot-setup-in-imx8mplus/m-p/1964518#M25767</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-09-30T14:02:03Z</dc:date>
    </item>
    <item>
      <title>Re: Dual boot setup in imx8mplus</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Dual-boot-setup-in-imx8mplus/m-p/1964964#M25772</link>
      <description>&lt;P&gt;Hi Bio_TICFSL,&lt;/P&gt;&lt;P&gt;What I'm looking for is emmc of the board should have 2 images and the board should be able to boot from both images. I'm also looking it as solution for adding image upgrade feature.&amp;nbsp;Jailhouse is generally used for running isolated applications or OS instances, not directly for performing image upgrades.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Oct 2024 06:20:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Dual-boot-setup-in-imx8mplus/m-p/1964964#M25772</guid>
      <dc:creator>sanum19</dc:creator>
      <dc:date>2024-10-01T06:20:34Z</dc:date>
    </item>
  </channel>
</rss>