<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: linux login not available in debug terminal in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/linux-login-not-available-in-debug-terminal/m-p/1949045#M25395</link>
    <description>&lt;P&gt;thanks for the reply,&lt;/P&gt;&lt;P&gt;i've booted the imx8 with the os and connected it to the gtk terminal.&lt;/P&gt;&lt;P&gt;i get debug updates upto the login but not the login option.&lt;/P&gt;&lt;P&gt;then it shows the updates while being powered down&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 06 Sep 2024 12:11:44 GMT</pubDate>
    <dc:creator>donjacobvellathottam</dc:creator>
    <dc:date>2024-09-06T12:11:44Z</dc:date>
    <item>
      <title>linux login not available in debug terminal</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/linux-login-not-available-in-debug-terminal/m-p/1948139#M25367</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've built a linux image for imx8 board using yocto.&lt;/P&gt;&lt;P&gt;the linux works without any issues in the hardware. But I am not able to login to the system with a debug terminal from my linux pc using gtk terminal.&lt;/P&gt;&lt;P&gt;all other debug information up to boot and from shutdown to poweroff are coming in the gtk terminal, but the login prompt is not shown.&lt;/P&gt;&lt;P&gt;any suggestions as to why this is happening or how can i solve this ?&lt;/P&gt;&lt;P&gt;TIA&lt;/P&gt;</description>
      <pubDate>Thu, 05 Sep 2024 10:05:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/linux-login-not-available-in-debug-terminal/m-p/1948139#M25367</guid>
      <dc:creator>donjacobvellathottam</dc:creator>
      <dc:date>2024-09-05T10:05:32Z</dc:date>
    </item>
    <item>
      <title>Re: linux login not available in debug terminal</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/linux-login-not-available-in-debug-terminal/m-p/1948311#M25371</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Connect your mx8 to the terminal and see if this works since we running console by default.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 05 Sep 2024 13:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/linux-login-not-available-in-debug-terminal/m-p/1948311#M25371</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-09-05T13:56:55Z</dc:date>
    </item>
    <item>
      <title>Re: linux login not available in debug terminal</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/linux-login-not-available-in-debug-terminal/m-p/1949045#M25395</link>
      <description>&lt;P&gt;thanks for the reply,&lt;/P&gt;&lt;P&gt;i've booted the imx8 with the os and connected it to the gtk terminal.&lt;/P&gt;&lt;P&gt;i get debug updates upto the login but not the login option.&lt;/P&gt;&lt;P&gt;then it shows the updates while being powered down&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Sep 2024 12:11:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/linux-login-not-available-in-debug-terminal/m-p/1949045#M25395</guid>
      <dc:creator>donjacobvellathottam</dc:creator>
      <dc:date>2024-09-06T12:11:44Z</dc:date>
    </item>
  </channel>
</rss>