<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic uboot show BootOrder not defined after Kernel size changed from 30M to 50M in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/uboot-show-BootOrder-not-defined-after-Kernel-size-changed-from/m-p/1948860#M25390</link>
    <description>&lt;P&gt;U-Boot 2022.04&lt;BR /&gt;Kernel:5.15.71&lt;BR /&gt;I want to implement boot animation in the kernel. 100 pictures are linked in the kernel, resulting in the kernel changing from 30M to 50M. When booting, it was found that the uboot was stuck, indicating that the uboot could not be found&lt;/P&gt;&lt;P&gt;No EFI system partition&lt;BR /&gt;BootOrder not defined&lt;BR /&gt;EFI boot manager: Cannot load any image&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;Scanning mmc 2:1...&lt;BR /&gt;62250 bytes read in 2 ms (29.7 MiB/s)&lt;BR /&gt;BootOrder not defined&lt;BR /&gt;EFI boot manager: Cannot load any image&lt;/P&gt;</description>
    <pubDate>Fri, 06 Sep 2024 07:46:03 GMT</pubDate>
    <dc:creator>wei_wang_semight</dc:creator>
    <dc:date>2024-09-06T07:46:03Z</dc:date>
    <item>
      <title>uboot show BootOrder not defined after Kernel size changed from 30M to 50M</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/uboot-show-BootOrder-not-defined-after-Kernel-size-changed-from/m-p/1948860#M25390</link>
      <description>&lt;P&gt;U-Boot 2022.04&lt;BR /&gt;Kernel:5.15.71&lt;BR /&gt;I want to implement boot animation in the kernel. 100 pictures are linked in the kernel, resulting in the kernel changing from 30M to 50M. When booting, it was found that the uboot was stuck, indicating that the uboot could not be found&lt;/P&gt;&lt;P&gt;No EFI system partition&lt;BR /&gt;BootOrder not defined&lt;BR /&gt;EFI boot manager: Cannot load any image&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;Scanning mmc 2:1...&lt;BR /&gt;62250 bytes read in 2 ms (29.7 MiB/s)&lt;BR /&gt;BootOrder not defined&lt;BR /&gt;EFI boot manager: Cannot load any image&lt;/P&gt;</description>
      <pubDate>Fri, 06 Sep 2024 07:46:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/uboot-show-BootOrder-not-defined-after-Kernel-size-changed-from/m-p/1948860#M25390</guid>
      <dc:creator>wei_wang_semight</dc:creator>
      <dc:date>2024-09-06T07:46:03Z</dc:date>
    </item>
    <item>
      <title>Re: uboot show BootOrder not defined after Kernel size changed from 30M to 50M</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/uboot-show-BootOrder-not-defined-after-Kernel-size-changed-from/m-p/1949127#M25396</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;In this case you will have to change the address in uboot and the cma memory.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 06 Sep 2024 14:31:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/uboot-show-BootOrder-not-defined-after-Kernel-size-changed-from/m-p/1949127#M25396</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-09-06T14:31:34Z</dc:date>
    </item>
  </channel>
</rss>