<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックDSPAUDIOEVM with DSP56371 How to control via RS232</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/DSPAUDIOEVM-with-DSP56371-How-to-control-via-RS232/m-p/141006#M253</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;I'm working with a EVM motherboard and a 371 daugtherboard.&lt;BR /&gt;It's the intention to work without the framework. And I'm currently running a passthrough application&lt;BR /&gt;debugging is done via Parallel port.&lt;BR /&gt;&lt;BR /&gt;I now want to implement the a 10BandEquilizer like in document DSP56311_Implementing10BandsEqualizer.pdf&lt;BR /&gt;&lt;BR /&gt;Problem is to change settings.&lt;BR /&gt;Is it possible to control the application via RS232 ?&lt;BR /&gt;RS232 is connected via the DEBUG MPU to SHI of the DSP. But I canot change the code of the MPU.&lt;BR /&gt;&lt;BR /&gt;Another question: is the 56371 allready supported by codewarrior? And does it bring a contribution?&lt;BR /&gt;&lt;BR /&gt;Thanks in advance&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jul 2007 20:39:03 GMT</pubDate>
    <dc:creator>rvdv2001</dc:creator>
    <dc:date>2007-07-24T20:39:03Z</dc:date>
    <item>
      <title>DSPAUDIOEVM with DSP56371 How to control via RS232</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/DSPAUDIOEVM-with-DSP56371-How-to-control-via-RS232/m-p/141006#M253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;I'm working with a EVM motherboard and a 371 daugtherboard.&lt;BR /&gt;It's the intention to work without the framework. And I'm currently running a passthrough application&lt;BR /&gt;debugging is done via Parallel port.&lt;BR /&gt;&lt;BR /&gt;I now want to implement the a 10BandEquilizer like in document DSP56311_Implementing10BandsEqualizer.pdf&lt;BR /&gt;&lt;BR /&gt;Problem is to change settings.&lt;BR /&gt;Is it possible to control the application via RS232 ?&lt;BR /&gt;RS232 is connected via the DEBUG MPU to SHI of the DSP. But I canot change the code of the MPU.&lt;BR /&gt;&lt;BR /&gt;Another question: is the 56371 allready supported by codewarrior? And does it bring a contribution?&lt;BR /&gt;&lt;BR /&gt;Thanks in advance&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2007 20:39:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/DSPAUDIOEVM-with-DSP56371-How-to-control-via-RS232/m-p/141006#M253</guid>
      <dc:creator>rvdv2001</dc:creator>
      <dc:date>2007-07-24T20:39:03Z</dc:date>
    </item>
    <item>
      <title>Re: DSPAUDIOEVM with DSP56371 How to control via RS232</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/DSPAUDIOEVM-with-DSP56371-How-to-control-via-RS232/m-p/141007#M254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The RS232 port on the DSPAUDIOEVMMB1 is connected to a microcontroller, not directly to the DSP.&amp;nbsp; It serves as an asynchronous to synchronous serial translation device for use with the Symphony Debugger (SDI).&amp;nbsp; The communication protocol has not been made public, since the protocol is largely connected to the internal operating system in the ROM.&amp;nbsp; The best bet to achieve serial communication between a host PC and the DSP is to use a USB or RS232 to SPI or I2C adapter, connecting that directly to the SHI port on the 56371.&lt;BR /&gt;&lt;BR /&gt;There is no CodeWarrior support for the 563xx family of 24-bit DSPs.&amp;nbsp; The only tool suite currently available is Suite56.&amp;nbsp; There is a new tool suite based on Eclipse that is coming out later this year.&amp;nbsp; It offers USB debugging support in addition to the legacy parallel port.&amp;nbsp; A port of the GNU C compiler is included with eventual support for Altium's C compiler.&lt;BR /&gt;&lt;BR /&gt;As a side note, to port the 56311EVM graphic equalizer code to the 56731, you need to consider these peripheral differences between the two:&amp;nbsp; The 371 has a very different PLL and method of programming it.&amp;nbsp; The SHI is a synchronous serial peripheral only whereas the SCI on the 56311 has synchronous and asynchronous modes.&amp;nbsp; The ESAI's on the 56371 are very different from the ESSI's on the 56311.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Sep 2007 05:18:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/DSPAUDIOEVM-with-DSP56371-How-to-control-via-RS232/m-p/141007#M254</guid>
      <dc:creator>david_dicarlo</dc:creator>
      <dc:date>2007-09-01T05:18:20Z</dc:date>
    </item>
  </channel>
</rss>