<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: P3S0210BQ Oscillating in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1942881#M25233</link>
    <description>&lt;P&gt;The schematic is too large and not very useful.&amp;nbsp; &amp;nbsp;It is a Xilinx Artix FPGA driving multiple I2C/I3C buses.&amp;nbsp; At the FPGA there is a 1K pullup to the rail voltage which is adjustable.&amp;nbsp; &amp;nbsp;Currently this voltage is at 1.8V.&amp;nbsp; &amp;nbsp; &amp;nbsp;I am attaching a scope capture of the oscillation starting.&amp;nbsp; Initially, the FPGA is holding SCL and SDA LOW.&amp;nbsp; &amp;nbsp;On command, it releases them to IDLE which is both high.&amp;nbsp; &amp;nbsp; As Port 1 ramps through a transition region, it starts to oscillate.&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;If I hold the OE pin low before releasing the SCL and SDA and then release it later, it will go to a stable IDLE.&amp;nbsp; &amp;nbsp;However, the oscillation starts again when bus activity occurs.&amp;nbsp; &amp;nbsp; On the demo board, all adjustable supplies are set to 3.3V.&amp;nbsp; &amp;nbsp; &amp;nbsp;I tried with pullup options, 1K, 2.2K and internal 10K.&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I hold the OE pin low, then the FPGA can read the temperature sensor on Port 1 at 12.5MHZ.&amp;nbsp; &amp;nbsp;So, the FPGA, its connections, and the voltage rail are OK onto the demo board.&amp;nbsp; &amp;nbsp;The problem only shows up when I enable the translator.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Aug 2024 01:48:25 GMT</pubDate>
    <dc:creator>smiller2</dc:creator>
    <dc:date>2024-08-29T01:48:25Z</dc:date>
    <item>
      <title>P3S0210BQ Oscillating</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1941683#M25195</link>
      <description>&lt;P&gt;We are evaluating the P3S0210BQ for a new design.&amp;nbsp; &amp;nbsp;We need to mux together an I3C bus and a low voltage UART into a single downstream port.&amp;nbsp; &amp;nbsp; When I attempt to send I3C through the MUX it starts oscillating.&amp;nbsp; &amp;nbsp; Sinewave at about 50MHZ,&amp;nbsp; well over a volt in amplitude.&amp;nbsp; &amp;nbsp; Oscillation continues until I pull the signal lines to GND.&amp;nbsp; Both SDA and SCL will oscillate.&amp;nbsp; &amp;nbsp;I increased the series resistors, but did not help.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;If I disable with the output enable, then the I3C connected to Port 1 can read the I3C temperature sensor on that port.&amp;nbsp; &amp;nbsp; If I enable the output, then it can see neither the sensor on Port 1 or Port S.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I unplug the demo board, initialize the I3C bus to idle, and then hot plug the 5V to the demo board,&amp;nbsp; I can get both lines to a stable IDLE at 1.8V.&amp;nbsp; &amp;nbsp;However, the first I3C transaction will start up the oscillation again.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The I3C controller is inside an FPGA that is on a remote board.&amp;nbsp; &amp;nbsp;There is probably over 24 inches of etch and a couple of connectors between the FPGA and the P3S0210BQ.&amp;nbsp; &amp;nbsp; Is there a maximum trace spec on these interconnects?&amp;nbsp; &amp;nbsp; &amp;nbsp;Any app notes on choosing the series resistors or snubbers?&amp;nbsp; &amp;nbsp; Thank you.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Aug 2024 02:25:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1941683#M25195</guid>
      <dc:creator>smiller2</dc:creator>
      <dc:date>2024-08-28T02:25:22Z</dc:date>
    </item>
    <item>
      <title>Re: P3S0210BQ Oscillating</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1941956#M25200</link>
      <description>&lt;P&gt;Dear Stephen,&lt;/P&gt;
&lt;P&gt;please share your schematic with voltage levels and part values. Please share the scopes of the SDA and SCL signals.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For designing the I3C lines, please check the following documents attached. Very detailed information to the I3C and other documents can be found in this &lt;A href="https://www.mipi.org/specifications/i3c-sensor-specification" target="_self"&gt;link&lt;/A&gt;.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regads,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Wed, 28 Aug 2024 08:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1941956#M25200</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2024-08-28T08:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: P3S0210BQ Oscillating</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1942881#M25233</link>
      <description>&lt;P&gt;The schematic is too large and not very useful.&amp;nbsp; &amp;nbsp;It is a Xilinx Artix FPGA driving multiple I2C/I3C buses.&amp;nbsp; At the FPGA there is a 1K pullup to the rail voltage which is adjustable.&amp;nbsp; &amp;nbsp;Currently this voltage is at 1.8V.&amp;nbsp; &amp;nbsp; &amp;nbsp;I am attaching a scope capture of the oscillation starting.&amp;nbsp; Initially, the FPGA is holding SCL and SDA LOW.&amp;nbsp; &amp;nbsp;On command, it releases them to IDLE which is both high.&amp;nbsp; &amp;nbsp; As Port 1 ramps through a transition region, it starts to oscillate.&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;If I hold the OE pin low before releasing the SCL and SDA and then release it later, it will go to a stable IDLE.&amp;nbsp; &amp;nbsp;However, the oscillation starts again when bus activity occurs.&amp;nbsp; &amp;nbsp; On the demo board, all adjustable supplies are set to 3.3V.&amp;nbsp; &amp;nbsp; &amp;nbsp;I tried with pullup options, 1K, 2.2K and internal 10K.&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I hold the OE pin low, then the FPGA can read the temperature sensor on Port 1 at 12.5MHZ.&amp;nbsp; &amp;nbsp;So, the FPGA, its connections, and the voltage rail are OK onto the demo board.&amp;nbsp; &amp;nbsp;The problem only shows up when I enable the translator.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Aug 2024 01:48:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1942881#M25233</guid>
      <dc:creator>smiller2</dc:creator>
      <dc:date>2024-08-29T01:48:25Z</dc:date>
    </item>
    <item>
      <title>Re: P3S0210BQ Oscillating</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1942919#M25234</link>
      <description>I have a typo above. All the adjustable supplies on the demo board are set to 1.8V and not 3.3V. Right now we are trying to use the part simply as a mux. 1.8V in and 1.8V out.</description>
      <pubDate>Thu, 29 Aug 2024 02:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1942919#M25234</guid>
      <dc:creator>smiller2</dc:creator>
      <dc:date>2024-08-29T02:31:08Z</dc:date>
    </item>
    <item>
      <title>Re: P3S0210BQ Oscillating</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1943440#M25250</link>
      <description>&lt;P&gt;Dear Stephen,&lt;/P&gt;
&lt;P&gt;could you please confirm the power supply pins voltage?&lt;/P&gt;
&lt;P&gt;1. What voltages have you applied to the VCCR, VCCP1, VCCP2 and VCCS?&lt;/P&gt;
&lt;P&gt;2. Please connect the&amp;nbsp;P3S0210BQ directly to the FPGA and the sensor. Make the links as short as possible.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3. Please use 30Ohm serial resistors on the lines as in our EVB.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1724932074068.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/296066i974C6287E666118C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1724932074068.png" alt="JozefKozon_0-1724932074068.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JozefKozon_0-1724932074068.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Thu, 29 Aug 2024 11:49:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1943440#M25250</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2024-08-29T11:49:07Z</dc:date>
    </item>
    <item>
      <title>Re: P3S0210BQ Oscillating</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1943904#M25260</link>
      <description>&lt;P&gt;I took a new device and dead bugged it onto a piece of perf board.&amp;nbsp; &amp;nbsp;All power pins were connected to 1.8V.&amp;nbsp; &amp;nbsp; &amp;nbsp;Series resistors were 47 ohms and pullups were 330 ohms.&amp;nbsp; &amp;nbsp;Pullups again connected to 1.8V.&amp;nbsp; &amp;nbsp; I see the same oscillation.&amp;nbsp; &amp;nbsp;If I keep OE LOW, then I can drive I3C to the chip on Port 1 and the waveforms are clean.&amp;nbsp; &amp;nbsp;If I allow OE to be pulled to 1.8V,&amp;nbsp; then it will start oscillating on the first or second transition.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The board with the FPGA is already in the field and I cannot shorten the traces to the FPGA.&amp;nbsp; &amp;nbsp;I don't think this part is suitable for systems with significant trace lengths.&amp;nbsp; &amp;nbsp; &amp;nbsp;The FPGA is probably about 4nS time of flight from this part.&amp;nbsp; &amp;nbsp; I think the reflection back from the FPGA is causing the edge enhancement to turn this into an oscillator.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Aug 2024 01:24:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1943904#M25260</guid>
      <dc:creator>smiller2</dc:creator>
      <dc:date>2024-08-30T01:24:06Z</dc:date>
    </item>
    <item>
      <title>Re: P3S0210BQ Oscillating</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1947196#M25347</link>
      <description>&lt;P&gt;Dear Stephen,&lt;/P&gt;
&lt;P&gt;I have sent a request for an advice on this issue. As soon as they will answer me, I will definitely reply to you.&lt;/P&gt;
&lt;P&gt;Thank you for your patience.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Wed, 04 Sep 2024 11:13:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1947196#M25347</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2024-09-04T11:13:36Z</dc:date>
    </item>
    <item>
      <title>Re: P3S0210BQ Oscillating</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1951686#M25426</link>
      <description>&lt;P&gt;Dear Stephen,&lt;/P&gt;
&lt;P&gt;I apologize for a late reply. There is still no answer from the application team. I have just sent them a reminder.&amp;nbsp;&lt;SPAN&gt;As soon as they will answer me, I will definitely reply to you.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for your patience.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 05:24:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1951686#M25426</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2024-09-11T05:24:05Z</dc:date>
    </item>
    <item>
      <title>Re: P3S0210BQ Oscillating</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1953016#M25445</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear Stephen,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;please see below an answer from the application engineer. The 24in length is too much load for the P3S0210BQ.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;DESCRIPTION&lt;/P&gt;
&lt;P class="x_MsoNormal"&gt;&lt;FONT color="#0000FF"&gt;We were able to simulate a similar case on our test bench with these conditions below and saw a round trip delay for the reflections of around 19ns:&lt;/FONT&gt;&lt;/P&gt;
&lt;P class="x_MsoNormal"&gt;&lt;FONT color="#0000FF"&gt;24inch trace w/ 3pF/in and 7.5nH/in&lt;/FONT&gt;&lt;/P&gt;
&lt;P class="x_MsoNormal"&gt;&lt;FONT color="#0000FF"&gt;Rseries = 50ohm&lt;/FONT&gt;&lt;/P&gt;
&lt;P class="x_MsoNormal"&gt;&lt;FONT color="#0000FF"&gt;2 connectors added adding ~90pF&lt;/FONT&gt;&lt;/P&gt;
&lt;P class="x_MsoNormal"&gt;&lt;FONT color="#0000FF"&gt;50ohm, 10pF load&lt;/FONT&gt;&lt;/P&gt;
&lt;P class="x_MsoNormal" aria-hidden="true"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P class="x_MsoNormal"&gt;&lt;FONT color="#0000FF"&gt;19ns is too high. The on time of the one-shot block is ~10ns. If this kind of oscillations are to be avoided, the round trip delay should be less than 10ns. 24in trace already creates 8ns delay even without connectors and load.&lt;/FONT&gt;&lt;/P&gt;
&lt;P class="x_MsoNormal"&gt;&lt;FONT color="#0000FF"&gt;This type of VLT with one-shot accelerator has this kind of limitation, unfortunately. There is no good way to overcome this without reducing the trace length.&lt;/FONT&gt;&lt;/P&gt;
&lt;P class="x_MsoNormal"&gt;With Best Regards,&lt;/P&gt;
&lt;P class="x_MsoNormal"&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 04:52:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/P3S0210BQ-Oscillating/m-p/1953016#M25445</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2024-09-12T04:52:23Z</dc:date>
    </item>
  </channel>
</rss>