<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CST: Error loading pkcs11 engine: could not load the shared library in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/CST-Error-loading-pkcs11-engine-could-not-load-the-shared/m-p/1940971#M25179</link>
    <description>Hi,&lt;BR /&gt;&lt;BR /&gt;I'm also facing the same issue with CST 3.4.1; How can I update shared library path for CST instead of /opt/cst&lt;BR /&gt;&lt;BR /&gt;I have tried by exporting; LD_LIBRARY_PATH, MODULE_PATH, OPENSSL_MODULE_PATH, PKCS11_MODULE_PATH but none of them worked&lt;BR /&gt;&lt;BR /&gt;how does CST know where to find the pkcs11.so file?&lt;BR /&gt;&lt;BR /&gt;Thanks</description>
    <pubDate>Tue, 27 Aug 2024 06:45:14 GMT</pubDate>
    <dc:creator>Umair-max</dc:creator>
    <dc:date>2024-08-27T06:45:14Z</dc:date>
    <item>
      <title>CST: Error loading pkcs11 engine: could not load the shared library</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CST-Error-loading-pkcs11-engine-could-not-load-the-shared/m-p/1805185#M21094</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I get the following error when I try to run the CST to connect to AWS CloudHSM. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;./linux64/bin/cst -i u-boot.csf -o out/signed.bin -b pkcs11 --verbose&lt;BR /&gt;Install SRK&lt;BR /&gt;Authenticate data&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;[ERROR] CST: Error loading pkcs11 engine: could not load the shared library&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In the code directory I notice there is a front_end and back_end-ssl. However, there is no back_end-pkcs11. Is the back_end-pkcs11 missing from 3.4.0?&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Or am I missing a configuration somewhere?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Also, the documentation for 3.4.0 mentions an example.csf file. However, there is no such example file.&lt;/P&gt;&lt;P&gt;The following is my csf file:&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;[Header]&lt;BR /&gt;Target = AHAB&lt;BR /&gt;Version = 1.0&lt;BR /&gt;Mode = HSM&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;[Install SRK]&lt;BR /&gt;# SRK table generated by srktool&lt;BR /&gt;File = "./crts/SRK1234table.bin"&lt;BR /&gt;# Public key certificate in PEM format&lt;BR /&gt;Source = "./crts/SRK1_sha384_secp384r1_v3_ca_crt.pem"&lt;BR /&gt;# Index of the public key certificate within the SRK table (0 .. 3)&lt;BR /&gt;Source index = 0&lt;BR /&gt;# Type of SRK set (NXP or OEM)&lt;BR /&gt;Source set = OEM&lt;BR /&gt;# bitmask of the revoked SRKs&lt;BR /&gt;Revocations = 0x0&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;[Authenticate Data]&lt;BR /&gt;# Binary to be signed generated by mkimage&lt;BR /&gt;File = "flash.bin"&lt;BR /&gt;# Offsets = Container header Signature block (printed out by mkimage)&lt;BR /&gt;Offsets = 0x0 0x90&lt;/P&gt;&lt;P&gt;Please advise how to fix this issue. Also, how does CST know where to find the pkcs11.so file?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Feb 2024 01:24:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CST-Error-loading-pkcs11-engine-could-not-load-the-shared/m-p/1805185#M21094</guid>
      <dc:creator>mighty_1</dc:creator>
      <dc:date>2024-02-13T01:24:12Z</dc:date>
    </item>
    <item>
      <title>Re: CST: Error loading pkcs11 engine: could not load the shared library</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CST-Error-loading-pkcs11-engine-could-not-load-the-shared/m-p/1806720#M21137</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228262"&gt;@mighty_1&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I hope you're doing well!&lt;/P&gt;
&lt;P&gt;I'll be supporting this case directly through email in the other ticket you submitted earlier. Thank you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Hector.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Feb 2024 18:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CST-Error-loading-pkcs11-engine-could-not-load-the-shared/m-p/1806720#M21137</guid>
      <dc:creator>hector_delgado</dc:creator>
      <dc:date>2024-02-14T18:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: CST: Error loading pkcs11 engine: could not load the shared library</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CST-Error-loading-pkcs11-engine-could-not-load-the-shared/m-p/1940971#M25179</link>
      <description>Hi,&lt;BR /&gt;&lt;BR /&gt;I'm also facing the same issue with CST 3.4.1; How can I update shared library path for CST instead of /opt/cst&lt;BR /&gt;&lt;BR /&gt;I have tried by exporting; LD_LIBRARY_PATH, MODULE_PATH, OPENSSL_MODULE_PATH, PKCS11_MODULE_PATH but none of them worked&lt;BR /&gt;&lt;BR /&gt;how does CST know where to find the pkcs11.so file?&lt;BR /&gt;&lt;BR /&gt;Thanks</description>
      <pubDate>Tue, 27 Aug 2024 06:45:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CST-Error-loading-pkcs11-engine-could-not-load-the-shared/m-p/1940971#M25179</guid>
      <dc:creator>Umair-max</dc:creator>
      <dc:date>2024-08-27T06:45:14Z</dc:date>
    </item>
  </channel>
</rss>