<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 IMX8MQ camera network casting problem</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/IMX8MQ-camera-network-casting-problem/m-p/1938238#M25104</link>
    <description>&lt;P&gt;Platform: IMX8MQ&lt;BR /&gt;Kernel version: linux-4.14.98&lt;BR /&gt;System: Linux Qt system&lt;BR /&gt;Camera: USB and MIPI&lt;BR /&gt;Problem description: The customer uses a MiPI camera and then uses the GST-Launch-1.0 RTSP stream to transmit data over Ethernet. The computer uses VLC software&lt;BR /&gt;The playback camera collects network streams, but the camera captures graphics. It will only be displayed on VLC after 2 seconds, and the customer said that a delay of 2 seconds is&lt;BR /&gt;Can it be reduced. I tested it with a USB camera and found a similar delay effect.&lt;/P&gt;&lt;P&gt;The attachment contains detailed operations.&lt;/P&gt;</description>
    <pubDate>Thu, 22 Aug 2024 08:18:12 GMT</pubDate>
    <dc:creator>claire_chen</dc:creator>
    <dc:date>2024-08-22T08:18:12Z</dc:date>
    <item>
      <title>IMX8MQ camera network casting problem</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IMX8MQ-camera-network-casting-problem/m-p/1938238#M25104</link>
      <description>&lt;P&gt;Platform: IMX8MQ&lt;BR /&gt;Kernel version: linux-4.14.98&lt;BR /&gt;System: Linux Qt system&lt;BR /&gt;Camera: USB and MIPI&lt;BR /&gt;Problem description: The customer uses a MiPI camera and then uses the GST-Launch-1.0 RTSP stream to transmit data over Ethernet. The computer uses VLC software&lt;BR /&gt;The playback camera collects network streams, but the camera captures graphics. It will only be displayed on VLC after 2 seconds, and the customer said that a delay of 2 seconds is&lt;BR /&gt;Can it be reduced. I tested it with a USB camera and found a similar delay effect.&lt;/P&gt;&lt;P&gt;The attachment contains detailed operations.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Aug 2024 08:18:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IMX8MQ-camera-network-casting-problem/m-p/1938238#M25104</guid>
      <dc:creator>claire_chen</dc:creator>
      <dc:date>2024-08-22T08:18:12Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ camera network casting problem</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IMX8MQ-camera-network-casting-problem/m-p/1939191#M25140</link>
      <description>&lt;P&gt;一般这种跟码流本身关系很大，你们可以在跑gstreamer命令之前加一个debug参数看看具体得延迟、export GST_DEBUG=v4l2bufferpool:6， 然后看下buffer queue 和dequeue之间的时间，还有就是4.14.98真的太老了，如果可以尽量更新到新版本&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 23 Aug 2024 10:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IMX8MQ-camera-network-casting-problem/m-p/1939191#M25140</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-08-23T10:16:18Z</dc:date>
    </item>
  </channel>
</rss>