<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: Preparing U-Boot to support AHAB secure boot features</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Preparing-U-Boot-to-support-AHAB-secure-boot-features/m-p/1936477#M25056</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The App note for the secure boot using AHAB for the i.MX8X is available at the following link:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12312.pdf" target="_blank" rel="nofollow noopener noreferrer"&gt;https://www.nxp.com/docs/en/application-note/AN12312.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;And you can refer to the security reference manual after request in the following link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=IMX8QXPSRM&amp;amp;appType=moderatedWithoutFAE&amp;amp;_gl=1*14s6i6i*_ga*MzYxNTg3MTA2LjE3MjQwOTE1NDI.*_ga_WM5LE0KMSH*MTcyNDE2MjMwMy45LjEuMTcyNDE2Mjk3My4wLjAuMA." target="_blank"&gt;https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=IMX8QXPSRM&amp;amp;appType=moderatedWithoutFAE&amp;amp;_gl=1*14s6i6i*_ga*MzYxNTg3MTA2LjE3MjQwOTE1NDI.*_ga_WM5LE0KMSH*MTcyNDE2MjMwMy45LjEuMTcyNDE2Mjk3My4wLjAuMA.&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;All the information applies as well for iMX95.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
    <pubDate>Tue, 20 Aug 2024 14:09:57 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-08-20T14:09:57Z</dc:date>
    <item>
      <title>Preparing U-Boot to support AHAB secure boot features</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Preparing-U-Boot-to-support-AHAB-secure-boot-features/m-p/1935886#M25047</link>
      <description>&lt;UL&gt;&lt;LI&gt;Preparing U-Boot to support AHAB secure boot features:&lt;/LI&gt;&lt;LI&gt;How to enable the AHAB config in the GM CHM code base ?&lt;/LI&gt;&lt;LI&gt;After enable the configuration file how to boot&amp;nbsp; up the board and check the boot logs with our modification reflected or not:&lt;/LI&gt;&lt;LI&gt;I refer the like mentioned below message.&lt;/LI&gt;&lt;LI&gt;&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf-6.1.22-2.0.0/doc/imx/ahab/guides/mx8ulp_9x_secure_boot.txt" target="_blank"&gt;uboot-imx/doc/imx/ahab/guides/mx8ulp_9x_secure_boot.txt at lf-6.1.22-2.0.0 · nxp-imx/uboot-imx · GitHub&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;IMX95 Processor&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;Explain about the below screen shots&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="shanthini_1306_0-1724134776493.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/294040i123ECFBB4BF29308/image-size/medium?v=v2&amp;amp;px=400" role="button" title="shanthini_1306_0-1724134776493.png" alt="shanthini_1306_0-1724134776493.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;IMX95 NXP Processor need Cortex-A core image and Cortex-M&amp;nbsp; core image&lt;BR /&gt;Explain breif about the Building an image supporting secure boot&lt;/P&gt;&lt;P&gt;For our processor need both&amp;nbsp;Cortex-A core image and Cortex-M&amp;nbsp; core image or only&amp;nbsp;Cortex-A core image ?&lt;/P&gt;&lt;P&gt;Currently i executed successfully only&amp;nbsp;Cortex-A core image?&lt;/P&gt;&lt;P&gt;If your answer is Yes both we need to use ?&lt;/P&gt;&lt;P&gt;How to use and how to do the secure boot using hW and how to flash and check the boot up logs ?&lt;/P&gt;&lt;P&gt;Thank you :).&lt;/P&gt;</description>
      <pubDate>Tue, 20 Aug 2024 06:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Preparing-U-Boot-to-support-AHAB-secure-boot-features/m-p/1935886#M25047</guid>
      <dc:creator>shanthini_1306</dc:creator>
      <dc:date>2024-08-20T06:25:50Z</dc:date>
    </item>
    <item>
      <title>Re: Preparing U-Boot to support AHAB secure boot features</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Preparing-U-Boot-to-support-AHAB-secure-boot-features/m-p/1936477#M25056</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The App note for the secure boot using AHAB for the i.MX8X is available at the following link:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12312.pdf" target="_blank" rel="nofollow noopener noreferrer"&gt;https://www.nxp.com/docs/en/application-note/AN12312.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;And you can refer to the security reference manual after request in the following link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=IMX8QXPSRM&amp;amp;appType=moderatedWithoutFAE&amp;amp;_gl=1*14s6i6i*_ga*MzYxNTg3MTA2LjE3MjQwOTE1NDI.*_ga_WM5LE0KMSH*MTcyNDE2MjMwMy45LjEuMTcyNDE2Mjk3My4wLjAuMA." target="_blank"&gt;https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=IMX8QXPSRM&amp;amp;appType=moderatedWithoutFAE&amp;amp;_gl=1*14s6i6i*_ga*MzYxNTg3MTA2LjE3MjQwOTE1NDI.*_ga_WM5LE0KMSH*MTcyNDE2MjMwMy45LjEuMTcyNDE2Mjk3My4wLjAuMA.&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;All the information applies as well for iMX95.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Tue, 20 Aug 2024 14:09:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Preparing-U-Boot-to-support-AHAB-secure-boot-features/m-p/1936477#M25056</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-08-20T14:09:57Z</dc:date>
    </item>
  </channel>
</rss>