<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックBoot using DDR on MSC8156AMC board</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Boot-using-DDR-on-MSC8156AMC-board/m-p/214909#M2489</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to boot my MSC8156AMC board with a program where some data are mapped in the DDR memory.&lt;/P&gt;&lt;P&gt;I know to do this I need to use a boot patch to initialize the DDR memory controllers, so I adapted the the ADS boot patch for the AMC&amp;nbsp; board using the values contains in the MSC8156AMC_Init.cfg file (Initialization do by JTAG).&lt;/P&gt;&lt;P&gt;But even if with the boot patch the DSP can't access to the DDR memory during the boot.&lt;/P&gt;&lt;P&gt;I also tried on a MSC8156ADS to boot a program with data mapped in DDR memory on a MSC8156ADS board using the boot patch for ADS and this time it works.&lt;/P&gt;&lt;P&gt;I don't understand why it work on the ADS board and not on the AMC board, because the only difference is the DDR memory type (DDR2 to DDR3), and I use the JTAG initialization values for the AMC board.&lt;/P&gt;&lt;P&gt;In the attachments there is the DDR AMC boot patch ASM file and the .txt file that I burn in the EEPROM memory.&lt;/P&gt;&lt;P&gt;Is there someone have the solution or a clue to solve this problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jimmy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jun 2011 18:44:59 GMT</pubDate>
    <dc:creator>Jim95</dc:creator>
    <dc:date>2011-06-14T18:44:59Z</dc:date>
    <item>
      <title>Boot using DDR on MSC8156AMC board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Boot-using-DDR-on-MSC8156AMC-board/m-p/214909#M2489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to boot my MSC8156AMC board with a program where some data are mapped in the DDR memory.&lt;/P&gt;&lt;P&gt;I know to do this I need to use a boot patch to initialize the DDR memory controllers, so I adapted the the ADS boot patch for the AMC&amp;nbsp; board using the values contains in the MSC8156AMC_Init.cfg file (Initialization do by JTAG).&lt;/P&gt;&lt;P&gt;But even if with the boot patch the DSP can't access to the DDR memory during the boot.&lt;/P&gt;&lt;P&gt;I also tried on a MSC8156ADS to boot a program with data mapped in DDR memory on a MSC8156ADS board using the boot patch for ADS and this time it works.&lt;/P&gt;&lt;P&gt;I don't understand why it work on the ADS board and not on the AMC board, because the only difference is the DDR memory type (DDR2 to DDR3), and I use the JTAG initialization values for the AMC board.&lt;/P&gt;&lt;P&gt;In the attachments there is the DDR AMC boot patch ASM file and the .txt file that I burn in the EEPROM memory.&lt;/P&gt;&lt;P&gt;Is there someone have the solution or a clue to solve this problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jimmy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jun 2011 18:44:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Boot-using-DDR-on-MSC8156AMC-board/m-p/214909#M2489</guid>
      <dc:creator>Jim95</dc:creator>
      <dc:date>2011-06-14T18:44:59Z</dc:date>
    </item>
    <item>
      <title>Re: Boot using DDR on MSC8156AMC board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Boot-using-DDR-on-MSC8156AMC-board/m-p/214910#M2490</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem it solves, it cames from the PLL, it was not qtable during the DDR initialization.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jun 2011 16:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Boot-using-DDR-on-MSC8156AMC-board/m-p/214910#M2490</guid>
      <dc:creator>Jim95</dc:creator>
      <dc:date>2011-06-27T16:34:33Z</dc:date>
    </item>
  </channel>
</rss>