<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PTN5150 Cold Plug State in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PTN5150-Cold-Plug-State/m-p/1931201#M24876</link>
    <description>&lt;P&gt;I want to do something similar in my system.&lt;/P&gt;&lt;P&gt;Could you check that the CC pin doesn't work properly when VDD is unpowered because:&lt;/P&gt;&lt;P&gt;1) This UFP use case is covered in the demo board.&lt;/P&gt;&lt;P&gt;2) When I connect 5V through a 10K resistor to CCx on an unpowered PTN5150A, I read 1.27V on the CCx pin.&lt;/P&gt;&lt;P&gt;It looks like the PTN5150A is implementing the +/- 20% voltage clamp from table 4-25 of the USB Type-C spec before it is powered.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Gavin&lt;/P&gt;</description>
    <pubDate>Tue, 13 Aug 2024 14:55:30 GMT</pubDate>
    <dc:creator>gavin5342</dc:creator>
    <dc:date>2024-08-13T14:55:30Z</dc:date>
    <item>
      <title>PTN5150 Cold Plug State</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PTN5150-Cold-Plug-State/m-p/1435783#M13586</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a device that I'd like to run in two modes with the PTN5150:&lt;/P&gt;&lt;P&gt;1. When battery is present, use USB-C DRP mode.&lt;/P&gt;&lt;P&gt;2. When battery is not present, use USB-C UFP mode.&lt;/P&gt;&lt;P&gt;I know the PTN5150 would work well for the first mode, but I am unsure about the second. In the second mode, the PTN5150 will have no supply voltage and from my understanding, VBUS is not connected to a UFP until CC detection is complete. Will UFP CC detection work if the PTN5150 has no power or do I have to find another solution?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;</description>
      <pubDate>Wed, 30 Mar 2022 00:57:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PTN5150-Cold-Plug-State/m-p/1435783#M13586</guid>
      <dc:creator>lucavald</dc:creator>
      <dc:date>2022-03-30T00:57:03Z</dc:date>
    </item>
    <item>
      <title>Re: PTN5150 Cold Plug State</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PTN5150-Cold-Plug-State/m-p/1436643#M13604</link>
      <description>&lt;P&gt;CC pins connected to VDD internally of IC, if VDD no power,CC pin can't work normally.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Mar 2022 03:05:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PTN5150-Cold-Plug-State/m-p/1436643#M13604</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-03-31T03:05:41Z</dc:date>
    </item>
    <item>
      <title>Re: PTN5150 Cold Plug State</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PTN5150-Cold-Plug-State/m-p/1931201#M24876</link>
      <description>&lt;P&gt;I want to do something similar in my system.&lt;/P&gt;&lt;P&gt;Could you check that the CC pin doesn't work properly when VDD is unpowered because:&lt;/P&gt;&lt;P&gt;1) This UFP use case is covered in the demo board.&lt;/P&gt;&lt;P&gt;2) When I connect 5V through a 10K resistor to CCx on an unpowered PTN5150A, I read 1.27V on the CCx pin.&lt;/P&gt;&lt;P&gt;It looks like the PTN5150A is implementing the +/- 20% voltage clamp from table 4-25 of the USB Type-C spec before it is powered.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Tue, 13 Aug 2024 14:55:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PTN5150-Cold-Plug-State/m-p/1931201#M24876</guid>
      <dc:creator>gavin5342</dc:creator>
      <dc:date>2024-08-13T14:55:30Z</dc:date>
    </item>
  </channel>
</rss>