<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MACHINE CHECK PARITY ERROR in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MACHINE-CHECK-PARITY-ERROR/m-p/1917908#M24395</link>
    <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;For the clock attached, it not only the frequency but also the PPJ and phase noise, and so on.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;Please confirm follow all the SPEC.&lt;/P&gt;</description>
    <pubDate>Fri, 26 Jul 2024 07:34:58 GMT</pubDate>
    <dc:creator>June_Lu</dc:creator>
    <dc:date>2024-07-26T07:34:58Z</dc:date>
    <item>
      <title>MACHINE CHECK PARITY ERROR</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MACHINE-CHECK-PARITY-ERROR/m-p/1901992#M23547</link>
      <description>&lt;P&gt;HI All.&lt;/P&gt;&lt;P&gt;We are using T1040 in one of Switch/Router. We did Booting by using Code Warrior Tools. While loading Linux we are facing the Issue. Those logs are as follows :&amp;nbsp;&lt;/P&gt;&lt;P&gt;Machine check in kernel mode.&lt;BR /&gt;Machine check in kernel mode.&lt;BR /&gt;Caused by (from MCSR=400c0000): Instruction Cache Parity Error&lt;BR /&gt;Machine Check Effective Address: 0xc000000000314004&lt;BR /&gt;Machine check in kernel mode.&lt;BR /&gt;Caused by (from MCSR=400d0000): Instruction Cache Parity Error&lt;BR /&gt;Machine Check Effective Address: 0xc00000000004b404&lt;BR /&gt;Machine check in kernel mode.&lt;BR /&gt;Caused by (from MCSR=400d0000): Instruction Cache Parity Error&lt;BR /&gt;Machine Check Effective Address: 0xc00000000013f600&lt;BR /&gt;Machine check in kernel mode.&lt;BR /&gt;Caused by (from MCSR=400d0000): Instruction Cache Parity Error&lt;BR /&gt;Machine Check Effective Address: 0xc00000000004b404&lt;BR /&gt;Unable to handle kernel paging request for data at address 0x00000061&lt;BR /&gt;Faulting instruction address: 0xc00000000013f604&lt;BR /&gt;Oops: Kernel access of bad area, sig: 11 [#1]&lt;BR /&gt;SMP NR_CPUS=4 CoreNet Generic&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It need to give us Linux Prompt. But we are facing issue related to Machine Check Parity Error. Pls try to reply if&amp;nbsp; you have any suggestion regarding this.&lt;BR /&gt;&lt;BR /&gt;Thank You.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jul 2024 09:08:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MACHINE-CHECK-PARITY-ERROR/m-p/1901992#M23547</guid>
      <dc:creator>A_Maruthi</dc:creator>
      <dc:date>2024-07-08T09:08:10Z</dc:date>
    </item>
    <item>
      <title>Re: MACHINE CHECK PARITY ERROR</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MACHINE-CHECK-PARITY-ERROR/m-p/1906938#M23784</link>
      <description>&lt;P&gt;&lt;SPAN&gt;P&lt;/SPAN&gt;&lt;SPAN&gt;roblems start with a cache parity&lt;/SPAN&gt; &lt;SPAN&gt;error. Most likely, this has to&lt;/SPAN&gt; &lt;SPAN&gt;do with overclocking, noisy, unstable or inappropriate voltage power,&lt;/SPAN&gt; &lt;SPAN&gt;external conditions like high level of radiation or overheating. The only way the&lt;/SPAN&gt; &lt;SPAN&gt;software can directly create this condition is described in E&lt;/SPAN&gt;&lt;SPAN&gt;5&lt;/SPAN&gt;&lt;SPAN&gt;500RM,&lt;/SPAN&gt; &lt;SPAN&gt;Section 5.4.5. I do not think Linux has any code for cache error&lt;/SPAN&gt; &lt;SPAN&gt;injection&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;suggestions below are&lt;/SPAN&gt; &lt;SPAN&gt;actually sanity checks:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Check if it violate the errata.&lt;/P&gt;
&lt;P&gt;Make sure no customizations have been done to u-Boot and/or Linux to switch on/off cache error protection without cache invalidation.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;Compare the problematic kernel configuration against the SDK default to make sure the build flags are correct for the CPU and no unsupported code is included in the build.&lt;/P&gt;
&lt;P&gt;Use SDK provided build tools to ensure the kernel is not miscompiled.&lt;/P&gt;
&lt;P&gt;Check general system operation conditions, make sure there is no overheating, overclocking, ESD, radiation.&lt;/P&gt;
&lt;P&gt;Check the power rails for stability and noise. The fact that the problem aggravates with more cores enabled together with the observation that the error shoots when a core leaves the normal idle routine, point to power as the most likely root cause.&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jul 2024 08:55:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MACHINE-CHECK-PARITY-ERROR/m-p/1906938#M23784</guid>
      <dc:creator>June_Lu</dc:creator>
      <dc:date>2024-07-12T08:55:59Z</dc:date>
    </item>
    <item>
      <title>Re: MACHINE CHECK PARITY ERROR</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MACHINE-CHECK-PARITY-ERROR/m-p/1908567#M23914</link>
      <description>&lt;P&gt;Thank You for Replying to Us. We have considered your suggestions and proceeded to debug. In our Cards , all the hardware and software debug options mentioned by you are in Suitable Working Condition according to our observation. We have total 30 Cards based on T1040RDB, in which 28 Cards are finished with U-boot, Linux Installation, and they are Working. We are following same procedure, but specifically in 2 Cards we are facing Machine Check Parity Error. We checked Power Supply levels (3.3V &amp;amp; 1.8V) which are within the Permissible limit. The clock input to the processor is measured to be 99.9997 MHz (Screenshot attached). Are there any other specific tests that we may do to further debug the source of the problem faced?&lt;/P&gt;&lt;P&gt;Thank You!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jul 2024 09:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MACHINE-CHECK-PARITY-ERROR/m-p/1908567#M23914</guid>
      <dc:creator>A_Maruthi</dc:creator>
      <dc:date>2024-07-15T09:30:26Z</dc:date>
    </item>
    <item>
      <title>Re: MACHINE CHECK PARITY ERROR</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MACHINE-CHECK-PARITY-ERROR/m-p/1917908#M24395</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;For the clock attached, it not only the frequency but also the PPJ and phase noise, and so on.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;Please confirm follow all the SPEC.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jul 2024 07:34:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MACHINE-CHECK-PARITY-ERROR/m-p/1917908#M24395</guid>
      <dc:creator>June_Lu</dc:creator>
      <dc:date>2024-07-26T07:34:58Z</dc:date>
    </item>
  </channel>
</rss>