<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Productsのトピックremove model from boot (change MPC8313e revision)</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/remove-model-from-boot-change-MPC8313e-revision/m-p/213210#M2422</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;Some time ago we developed a system based on MPC8313erdb REVA4 (MPC8313E rev1.0) and MPC8313E_RDB_K26_20070831-LTIB.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;Then we assembled a second batch of systems and by mistake mounted the MPC8313 rev2.1, and upon a power up sequence the bootloader gets stucked saying "CPU: rev unknown". We have reviewed the AN3545 and decided to update the ltib. This is a hard work becouse we made some changes in it.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;We adapted u-boot and it worked fine. We disabled some driver in kernel but it hang on boot, it stops after the usb module loads. We don't have USB so we have disabled in the kernel but it still boots.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;We think the USB module stop the boot,if this is right how can we remove this module from the kernel/&lt;/FONT&gt;initramfs&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;?&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;Thanks in advance.&lt;BR /&gt;Best Regards.&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Jul 2010 15:51:39 GMT</pubDate>
    <dc:creator>medina</dc:creator>
    <dc:date>2010-07-15T15:51:39Z</dc:date>
    <item>
      <title>remove model from boot (change MPC8313e revision)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/remove-model-from-boot-change-MPC8313e-revision/m-p/213210#M2422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;Some time ago we developed a system based on MPC8313erdb REVA4 (MPC8313E rev1.0) and MPC8313E_RDB_K26_20070831-LTIB.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;Then we assembled a second batch of systems and by mistake mounted the MPC8313 rev2.1, and upon a power up sequence the bootloader gets stucked saying "CPU: rev unknown". We have reviewed the AN3545 and decided to update the ltib. This is a hard work becouse we made some changes in it.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;We adapted u-boot and it worked fine. We disabled some driver in kernel but it hang on boot, it stops after the usb module loads. We don't have USB so we have disabled in the kernel but it still boots.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;We think the USB module stop the boot,if this is right how can we remove this module from the kernel/&lt;/FONT&gt;initramfs&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;?&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;Thanks in advance.&lt;BR /&gt;Best Regards.&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jul 2010 15:51:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/remove-model-from-boot-change-MPC8313e-revision/m-p/213210#M2422</guid>
      <dc:creator>medina</dc:creator>
      <dc:date>2010-07-15T15:51:39Z</dc:date>
    </item>
    <item>
      <title>Re: remove model from boot (change MPC8313e revision)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/remove-model-from-boot-change-MPC8313e-revision/m-p/213211#M2423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have found a solution. We have modifed the dts file from the older ltib. Now we are testing it but we see one problem:&lt;/P&gt;&lt;P&gt;The new uboot modifed is compatible with two revision. The kernel and rootfs don't change. We have two diferent dtb files, one per revision.&lt;/P&gt;&lt;P&gt;Can we do a dts/dtb compatible with two revisions?&lt;/P&gt;&lt;P&gt;How can we read the different revision and load the different dtb file depending of the revision read?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Best regard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jul 2010 18:50:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/remove-model-from-boot-change-MPC8313e-revision/m-p/213211#M2423</guid>
      <dc:creator>medina</dc:creator>
      <dc:date>2010-07-15T18:50:24Z</dc:date>
    </item>
  </channel>
</rss>