<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SWUpdate with quashfs on eMMC in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SWUpdate-with-quashfs-on-eMMC/m-p/1911287#M23980</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I managed to add swupdate to imx8mm-evk imx-linux system kernel 5.10.72 and use swupdate-scripts to generate the base image and update image. The images work for rootfs with ext2, ext3 and ext4. However, I need rootfs to use squashfs instead but seems like the swupdate-script does not support squashfs?&lt;/P&gt;&lt;P&gt;Would appreciate if you can provide some lights on creating the base image which rootfs is squashfs fstype for imx8mm.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 18 Jul 2024 10:40:11 GMT</pubDate>
    <dc:creator>alanlow</dc:creator>
    <dc:date>2024-07-18T10:40:11Z</dc:date>
    <item>
      <title>SWUpdate with quashfs on eMMC</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SWUpdate-with-quashfs-on-eMMC/m-p/1911287#M23980</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I managed to add swupdate to imx8mm-evk imx-linux system kernel 5.10.72 and use swupdate-scripts to generate the base image and update image. The images work for rootfs with ext2, ext3 and ext4. However, I need rootfs to use squashfs instead but seems like the swupdate-script does not support squashfs?&lt;/P&gt;&lt;P&gt;Would appreciate if you can provide some lights on creating the base image which rootfs is squashfs fstype for imx8mm.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jul 2024 10:40:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SWUpdate-with-quashfs-on-eMMC/m-p/1911287#M23980</guid>
      <dc:creator>alanlow</dc:creator>
      <dc:date>2024-07-18T10:40:11Z</dc:date>
    </item>
  </channel>
</rss>