<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCA9615 Failures in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Failures/m-p/1906160#M23773</link>
    <description>&lt;P&gt;I am also facing the same issue, can this be recovered with a power cycle? how to resolve the issue if the communication is throwing an error during the hot swapping. please clarify in detail.&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jul 2024 09:32:55 GMT</pubDate>
    <dc:creator>Satyabobbadi</dc:creator>
    <dc:date>2024-07-11T09:32:55Z</dc:date>
    <item>
      <title>PCA9615 Failures</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Failures/m-p/1302064#M11441</link>
      <description>&lt;P&gt;Hi, Forum,&lt;/P&gt;&lt;P&gt;The circuit below is used on both ends of a 10-foot cable.&amp;nbsp; The PCA9615 I.C.s catastrophically and permanently fail, sometimes at both ends of cable simultaneously.&amp;nbsp; Failed I.C.s drag down our power supply and get hot - they die. Replacing the I.C.s fixes the problem.&lt;/P&gt;&lt;P&gt;Failures may occur after hours or days of normal operation, or immediately after a disconnect/reconnect, and possible after (unauthorized) hot-swapping.&amp;nbsp; The cable carries the PCA9615 dual differential bus, ground, and +24V.&amp;nbsp; +5V and +3V are generated from +24V independently at each end of the cable.&amp;nbsp; We are not using the hot-swap logic, but have EN tied to +3.3V.&amp;nbsp; The datasheet includes no Limiting Values identified for hot-swap, and its hot-swap description mentions nothing about protecting the I.C., so I presume the hot-swap logic is intended not to protect the device from damage, but to prevent the device from corrupting data when connected to a live bus.&lt;/P&gt;&lt;P&gt;The failure can be recreated by intentionally hot-swapping under ESD-safe conditions, so failures are probably not likely cause by ESD.&lt;/P&gt;&lt;P&gt;No microcontroller is available to operate the hot-swap EN signal at one end of the cable.&lt;/P&gt;&lt;P&gt;Is hot-swapping without using the hot-swap logic known to cause device failures?&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the failure mechanism?&lt;/P&gt;&lt;P&gt;The PCA9615 is a nice, inexpensive, compact solution to extending I2C through a cable.&amp;nbsp; We'd like to keep using it, and we want to keep using it if possible.&lt;/P&gt;&lt;P&gt;Suggestions?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Staff_3-1625341932550.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/148725i5A5447057E241F62/image-dimensions/717x397?v=v2" alt="Staff_3-1625341932550.png" title="Staff_3-1625341932550.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 03 Jul 2021 20:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Failures/m-p/1302064#M11441</guid>
      <dc:creator>Staff</dc:creator>
      <dc:date>2021-07-03T20:31:33Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615 Failures</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Failures/m-p/1307295#M11501</link>
      <description>&lt;P&gt;For the unused of hot swap function, floating the EN pin because of it connect with VDDA inside of IC.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 03:21:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Failures/m-p/1307295#M11501</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-07-14T03:21:34Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615 Failures</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Failures/m-p/1402884#M13087</link>
      <description>&lt;P&gt;I am having similar issues with heat and communication failure. VDD(A) = 3.3V, VDD(B) = 5V, EN = floating, no hot-swap.&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jan 2022 21:57:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Failures/m-p/1402884#M13087</guid>
      <dc:creator>aferm</dc:creator>
      <dc:date>2022-01-20T21:57:02Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615 Failures</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Failures/m-p/1586618#M16494</link>
      <description>&lt;P&gt;I also have the same issue, VDDA = 3.3V, VDDB= 3.3V. and it all seems to be happening during hot plugging operations (also under ESD safe environment). Once the PCA9615 fails it won't recover, and the PCA9615 starts getting really hot.&lt;/P&gt;</description>
      <pubDate>Mon, 23 Jan 2023 15:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Failures/m-p/1586618#M16494</guid>
      <dc:creator>jmse</dc:creator>
      <dc:date>2023-01-23T15:45:20Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615 Failures</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Failures/m-p/1906160#M23773</link>
      <description>&lt;P&gt;I am also facing the same issue, can this be recovered with a power cycle? how to resolve the issue if the communication is throwing an error during the hot swapping. please clarify in detail.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jul 2024 09:32:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Failures/m-p/1906160#M23773</guid>
      <dc:creator>Satyabobbadi</dc:creator>
      <dc:date>2024-07-11T09:32:55Z</dc:date>
    </item>
  </channel>
</rss>