<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 TDA1572</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/TDA1572/m-p/1904136#M23675</link>
    <description>&lt;P&gt;I tried to build an AM receiver with the TDA1572 integrated circuit. The specimens found on the Asian market are marked with the Philips logo. When I feed according to the application scheme, the consumption at pin 1 is very high, the voltage at pin 1 dropping to 1V (inductance feeding at 9V). I bought from several sources, the result being the same. Then I used the TDA1072, an equivalent integrated circuit that complies with the specifications in the catalog sheet and the assembly is functional.&lt;BR /&gt;Question:&lt;BR /&gt;Does anyone have an application schematic for this possible new version of the TDA1572 circuit?&lt;BR /&gt;Any information or suggestion will be appreciated.&lt;BR /&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Tue, 09 Jul 2024 10:10:34 GMT</pubDate>
    <dc:creator>fox7878</dc:creator>
    <dc:date>2024-07-09T10:10:34Z</dc:date>
    <item>
      <title>TDA1572</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TDA1572/m-p/1904136#M23675</link>
      <description>&lt;P&gt;I tried to build an AM receiver with the TDA1572 integrated circuit. The specimens found on the Asian market are marked with the Philips logo. When I feed according to the application scheme, the consumption at pin 1 is very high, the voltage at pin 1 dropping to 1V (inductance feeding at 9V). I bought from several sources, the result being the same. Then I used the TDA1072, an equivalent integrated circuit that complies with the specifications in the catalog sheet and the assembly is functional.&lt;BR /&gt;Question:&lt;BR /&gt;Does anyone have an application schematic for this possible new version of the TDA1572 circuit?&lt;BR /&gt;Any information or suggestion will be appreciated.&lt;BR /&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jul 2024 10:10:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TDA1572/m-p/1904136#M23675</guid>
      <dc:creator>fox7878</dc:creator>
      <dc:date>2024-07-09T10:10:34Z</dc:date>
    </item>
  </channel>
</rss>