<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Use multiple PCA9552 and control LED blink same frequency in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Use-multiple-PCA9552-and-control-LED-blink-same-frequency/m-p/1892805#M23257</link>
    <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;We want to use&amp;nbsp;multiple PCA9552 to control more LED, and we think PCA9552 each have an internal clock, so can't&amp;nbsp;sync the blinking frequency between the multiple PCA9552.&lt;/P&gt;&lt;P&gt;And we see the application note "PCA9552_AN264", in the page 20 "Dimming LEDs - Alternative solution using external oscillator", should we use external oscillator to control&amp;nbsp;LED blink same frequency? Or do you have other solution?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 24 Jun 2024 10:21:13 GMT</pubDate>
    <dc:creator>James_ATLT</dc:creator>
    <dc:date>2024-06-24T10:21:13Z</dc:date>
    <item>
      <title>Use multiple PCA9552 and control LED blink same frequency</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Use-multiple-PCA9552-and-control-LED-blink-same-frequency/m-p/1892805#M23257</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;We want to use&amp;nbsp;multiple PCA9552 to control more LED, and we think PCA9552 each have an internal clock, so can't&amp;nbsp;sync the blinking frequency between the multiple PCA9552.&lt;/P&gt;&lt;P&gt;And we see the application note "PCA9552_AN264", in the page 20 "Dimming LEDs - Alternative solution using external oscillator", should we use external oscillator to control&amp;nbsp;LED blink same frequency? Or do you have other solution?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jun 2024 10:21:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Use-multiple-PCA9552-and-control-LED-blink-same-frequency/m-p/1892805#M23257</guid>
      <dc:creator>James_ATLT</dc:creator>
      <dc:date>2024-06-24T10:21:13Z</dc:date>
    </item>
    <item>
      <title>Re: Use multiple PCA9552 and control LED blink same frequency</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Use-multiple-PCA9552-and-control-LED-blink-same-frequency/m-p/1893056#M23260</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;PCA9552 has three hardware address pins on the PCA9552 allow eight devices to operate on the same bus, if you use the external oscillator solution&amp;nbsp;PCA9552 cannot be addressed.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ErikaC_0-1719254274871.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/285497i379553856987D78B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ErikaC_0-1719254274871.png" alt="ErikaC_0-1719254274871.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ErikaC_0-1719254274871.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So, how many LEDs you want to use? Please see the&amp;nbsp;FREQUENTLY ASKED QUESTIONS&lt;/P&gt;
&lt;P&gt;3. Question: Can the LED Dimmers or Blinkers be used to blink multiple LEDs?&lt;BR /&gt;Answer: Each bit is limited to 25 mA, the 8-bit device can provide up to 100 mA total and the 16-bit device can&lt;BR /&gt;provide up to 200 mA total (100 mA per 8-bit group). You can put as many LEDs on each bit and package as not to&lt;BR /&gt;exceed these limits. Normally there will be one LED on each bit and each LED can be ON, OFF or at Blink Rate 1&lt;BR /&gt;or 2. An external FET or a bipolar transistor controlled by the LED blinker output signal can be used to increase the&lt;BR /&gt;number of LEDs per output or to pull up the LED supply voltage to some voltage level higher than 6.0 V.&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jun 2024 18:39:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Use-multiple-PCA9552-and-control-LED-blink-same-frequency/m-p/1893056#M23260</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2024-06-24T18:39:13Z</dc:date>
    </item>
    <item>
      <title>Re: Use multiple PCA9552 and control LED blink same frequency</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Use-multiple-PCA9552-and-control-LED-blink-same-frequency/m-p/1893392#M23271</link>
      <description>&lt;P&gt;Hi ErikaC,&lt;/P&gt;&lt;P&gt;Thanks your reply.&lt;BR /&gt;But we use 48 pcs LEDs (3 pcs PCA9552) and if we want to control separately every LEDs, so I think&amp;nbsp;the&amp;nbsp;FREQUENTLY ASKED QUESTIONS 3. still can't solve the questions.&lt;/P&gt;&lt;P&gt;Do you have any other suggestions?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 07:18:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Use-multiple-PCA9552-and-control-LED-blink-same-frequency/m-p/1893392#M23271</guid>
      <dc:creator>James_ATLT</dc:creator>
      <dc:date>2024-06-25T07:18:33Z</dc:date>
    </item>
    <item>
      <title>Re: Use multiple PCA9552 and control LED blink same frequency</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Use-multiple-PCA9552-and-control-LED-blink-same-frequency/m-p/1893471#M23275</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi ErikaC,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Sorry, one more question, "alternative solution using external oscillator" just only for dimming LED, not for blinking, is correct?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 08:49:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Use-multiple-PCA9552-and-control-LED-blink-same-frequency/m-p/1893471#M23275</guid>
      <dc:creator>James_ATLT</dc:creator>
      <dc:date>2024-06-25T08:49:13Z</dc:date>
    </item>
  </channel>
</rss>